Post Go back to editing

What are the differences between ad725ar-reel7 and ad725arz?

Thread Summary

The user inquired about the differences between AD725AR-REEL7 and AD725ARZ, particularly regarding functionality and interchangeability. The final answer clarifies that -REEL and -REEL7 suffixes only indicate the packaging method (7-inch reel), and the base part number is AD725AR. The accompanying answers suggest reviewing the respective datasheets for detailed comparisons and provide a link to a comparison resource and a related thread discussing the AD725ARZ buffer output for composite signals.
AI Generated Content
Category: Hardware
Product Number: AD725AR

Is ad725ar-reel7 just older version of ad725arz? Do they have identical function and interchangeable? Any flaws with ad725ar-reel7? Or, any improvements for ad725arz over ad725ar-reel7?

Parents on Aug 25, 2023 9:29 AM in reply to PoornimaSubramani
+1

The -REEL and -REEL7 just specifies how the parts are shipped,  i.e.  -REEL7 mean parts are on tape on a 7 inch reel.  The base number is just AD725AR

Reply
  • FormerMember
    FormerMember
on Aug 25, 2023 9:29 AM in reply to PoornimaSubramani
+1

The -REEL and -REEL7 just specifies how the parts are shipped,  i.e.  -REEL7 mean parts are on tape on a 7 inch reel.  The base number is just AD725AR

Children
No Data