I have configured INTR1 (0x24),RX0 (0x1004),but reading CNT8 (0x40) is always 0. How ton config max96712 and I can get right packets count with CNT8 (0x40) ?
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX96717R
Recommended for New Designs
The MAX96717R GMSLâ„¢ serializer receives video on a 4-lane MIPI CSI-2 interface and outputs it on a GMSL2 serial link transceiver for transport over a...
Datasheet
MAX96717R on Analog.com
MAX96711
Production
The MAX96711 is a compact serializer with features especially suited for automotive camera applications. In high-bandwidth mode, the parallel-clock maximum...
Datasheet
MAX96711 on Analog.com
I have configured INTR1 (0x24),RX0 (0x1004),but reading CNT8 (0x40) is always 0. How ton config max96712 and I can get right packets count with CNT8 (0x40) ?
Hi,
We are not aware much about this part so could you please go through the "Packet Protocol " related section in the below suggested documents.
Thanks,
Poornima
96712 is a deserializer,my Serializer is 96705, I should config Serializer ?