Hi teams
The system architecture which I use consists of FPGA+ADV202, where the images and compressed bitstreams are transmitted using HDATA+DMA. The bitstream is uploaded to the the PC for decoding. The RGB test patterns are generated Inside the FPGA, converted to YCbCr, and then encoded by ADV202. The current test results are as follows:
(1) ADV202 is configured as 4x8-bit Single Component, 8-bit precision, and only Y Component is transmitted. The PC decoding result displays correctly.
(2) ADV202 is configured as 4x8-bit Packed YYCbCr, 8-bit precision. The RGB pattern decoded by PC displays incorrectly.
I have attached the relevant file after the question.
Thanks & Best Regards