Post Go back to editing

adv202 error during the decoding of the bitstream when uploaded to the PC.

Product Number: adv202

Hi teams

The system architecture which I use consists of FPGA+ADV202, where the images and compressed bitstreams are transmitted using HDATA+DMA. The bitstream is uploaded to the the PC for decoding. The RGB test patterns are generated Inside the FPGA, converted to YCbCr, and then encoded by ADV202. The current test results are as follows:

(1)  ADV202 is configured as 4x8-bit Single Component, 8-bit precision, and only Y Component is transmitted. The PC decoding result displays correctly.

(2) ADV202 is configured as 4x8-bit Packed YYCbCr, 8-bit precision. The RGB pattern decoded by PC displays incorrectly.

I have attached the relevant file after the question.

DOCX a1-9.bmp PDFb1-4.bmp

Thanks & Best Regards

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.