Post Go back to editing

ADV7619 can receive 1080p from HDMI generator (no EDID), but failed to receive 1080p from PC (with EDID)

Category: Software
Product Number: ADV7619

Hello,

We are using Terasic (HDMI licensee)  HDMI-FMC board and a customized FPGA board to receive 1080p. The system works well with a HDMI video pattern generator (QVS VPG-HL HDMI Video Pattern Generator). All the 1080p data is correctly received. The DE/HS/VS and data are correct (Fig. 1). 

However, when the video source is switched to a laptop's HDMI output, it doesn't work.  The PC can't detect the Terasic board, and the DE/HS/VS and Data don't make sense (the DE pulse changed every 800 pixel data, instead of whole frame; the data is always zero).  (Fig. 2)

We checked many previous posts in this forum. We think the difference (between video pattern generator and PC) is the EDID.  Following the previous post (it is for ADV7611, but we didn't find a similar one for ADV7619 -- so we assume the EDID RAM is the same), we set the EDID internal RAM as well other registers. But we still can't receive valid signals on DE/HS/VS and data lines.  Attached is the register setup for our test. We are stuck on this for a few weeks. Can anyone help ? 

Many thanks.

Charlie 

Information 1:

Fig.1  Valid DE/HS/VS and Data signal with video generator

Information 2:

Fig.2 Invalid DE/HS/VS and Data with PC HDMI output as video source

Information 3: previous post on ADV7611 EDID setup:

ez.analog.com/.../how-can-i-use-adv7611-with-an-internal-edid

Information 4:  ADV7619 register setup in our test:

ADV7619RegSet(0x98, 0xF4, 0x80); //CEC
ADV7619RegSet(0x98, 0xF5, 0x7C); //INFOFRAME
ADV7619RegSet(0x98, 0xF8, 0x4C); //DPLL
ADV7619RegSet(0x98, 0xF9, 0x64); //KSV
ADV7619RegSet(0x98, 0xFA, 0x6C); //EDID
ADV7619RegSet(0x98, 0xFB, 0x68); //HDMI
ADV7619RegSet(0x98, 0xFD, 0x44); //CP
//EDID Internal RAM
ADV7619RegSet(0X64,0X77,0X00); //Disable internal EDID
ADV7619RegSet(0X6C,0X00,0X00);
ADV7619RegSet(0X6C,0X01,0XFF);
ADV7619RegSet(0X6C,0X02,0XFF);
ADV7619RegSet(0X6C,0X03,0XFF);
ADV7619RegSet(0X6C,0X04,0XFF);
ADV7619RegSet(0X6C,0X05,0XFF);
ADV7619RegSet(0X6C,0X06,0XFF);
ADV7619RegSet(0X6C,0X07,0X00);
ADV7619RegSet(0X6C,0X08,0X06);
ADV7619RegSet(0X6C,0X09,0X8F);
ADV7619RegSet(0X6C,0X0A,0X07);
ADV7619RegSet(0X6C,0X0B,0X11);
ADV7619RegSet(0X6C,0X0C,0X01);
ADV7619RegSet(0X6C,0X0D,0X00);
ADV7619RegSet(0X6C,0X0E,0X00);
ADV7619RegSet(0X6C,0X0F,0X00);
ADV7619RegSet(0X6C,0X10,0X17);
ADV7619RegSet(0X6C,0X11,0X11);
ADV7619RegSet(0X6C,0X12,0X01);
ADV7619RegSet(0X6C,0X13,0X03);
ADV7619RegSet(0X6C,0X14,0X80);
ADV7619RegSet(0X6C,0X15,0X0C);
ADV7619RegSet(0X6C,0X16,0X09);
ADV7619RegSet(0X6C,0X17,0X78);
ADV7619RegSet(0X6C,0X18,0X0A);
ADV7619RegSet(0X6C,0X19,0X1E);
ADV7619RegSet(0X6C,0X1A,0XAC);
ADV7619RegSet(0X6C,0X1B,0X98);
ADV7619RegSet(0X6C,0X1C,0X59);
ADV7619RegSet(0X6C,0X1D,0X56);
ADV7619RegSet(0X6C,0X1E,0X85);
ADV7619RegSet(0X6C,0X1F,0X28);
ADV7619RegSet(0X6C,0X20,0X29);
ADV7619RegSet(0X6C,0X21,0X52);
ADV7619RegSet(0X6C,0X22,0X57);
ADV7619RegSet(0X6C,0X23,0X00);
ADV7619RegSet(0X6C,0X24,0X00);
ADV7619RegSet(0X6C,0X25,0X00);
ADV7619RegSet(0X6C,0X26,0X01);
ADV7619RegSet(0X6C,0X27,0X01);
ADV7619RegSet(0X6C,0X28,0X01);
ADV7619RegSet(0X6C,0X29,0X01);
ADV7619RegSet(0X6C,0X2A,0X01);
ADV7619RegSet(0X6C,0X2B,0X01);
ADV7619RegSet(0X6C,0X2C,0X01);
ADV7619RegSet(0X6C,0X2D,0X01);
ADV7619RegSet(0X6C,0X2E,0X01);
ADV7619RegSet(0X6C,0X2F,0X01);
ADV7619RegSet(0X6C,0X30,0X01);
ADV7619RegSet(0X6C,0X31,0X01);
ADV7619RegSet(0X6C,0X32,0X01);
ADV7619RegSet(0X6C,0X33,0X01);
ADV7619RegSet(0X6C,0X34,0X01);
ADV7619RegSet(0X6C,0X35,0X01);
ADV7619RegSet(0X6C,0X36,0X8C);
ADV7619RegSet(0X6C,0X37,0X0A);
ADV7619RegSet(0X6C,0X38,0XD0);
ADV7619RegSet(0X6C,0X39,0X8A);
ADV7619RegSet(0X6C,0X3A,0X20);
ADV7619RegSet(0X6C,0X3B,0XE0);
ADV7619RegSet(0X6C,0X3C,0X2D);
ADV7619RegSet(0X6C,0X3D,0X10);
ADV7619RegSet(0X6C,0X3E,0X10);
ADV7619RegSet(0X6C,0X3F,0X3E);
ADV7619RegSet(0X6C,0X40,0X96);
ADV7619RegSet(0X6C,0X41,0X00);
ADV7619RegSet(0X6C,0X42,0X81);
ADV7619RegSet(0X6C,0X43,0X60);
ADV7619RegSet(0X6C,0X44,0X00);
ADV7619RegSet(0X6C,0X45,0X00);
ADV7619RegSet(0X6C,0X46,0X00);
ADV7619RegSet(0X6C,0X47,0X18);
ADV7619RegSet(0X6C,0X48,0X01);
ADV7619RegSet(0X6C,0X49,0X1D);
ADV7619RegSet(0X6C,0X4A,0X80);
ADV7619RegSet(0X6C,0X4B,0X18);
ADV7619RegSet(0X6C,0X4C,0X71);
ADV7619RegSet(0X6C,0X4D,0X1C);
ADV7619RegSet(0X6C,0X4E,0X16);
ADV7619RegSet(0X6C,0X4F,0X20);
ADV7619RegSet(0X6C,0X50,0X58);
ADV7619RegSet(0X6C,0X51,0X2C);
ADV7619RegSet(0X6C,0X52,0X25);
ADV7619RegSet(0X6C,0X53,0X00);
ADV7619RegSet(0X6C,0X54,0X81);
ADV7619RegSet(0X6C,0X55,0X49);
ADV7619RegSet(0X6C,0X56,0X00);
ADV7619RegSet(0X6C,0X57,0X00);
ADV7619RegSet(0X6C,0X58,0X00);
ADV7619RegSet(0X6C,0X59,0X9E);
ADV7619RegSet(0X6C,0X5A,0X00);
ADV7619RegSet(0X6C,0X5B,0X00);
ADV7619RegSet(0X6C,0X5C,0X00);
ADV7619RegSet(0X6C,0X5D,0XFC);
ADV7619RegSet(0X6C,0X5E,0X00);
ADV7619RegSet(0X6C,0X5F,0X56);
ADV7619RegSet(0X6C,0X60,0X41);
ADV7619RegSet(0X6C,0X61,0X2D);
ADV7619RegSet(0X6C,0X62,0X31);
ADV7619RegSet(0X6C,0X63,0X38);
ADV7619RegSet(0X6C,0X64,0X30);
ADV7619RegSet(0X6C,0X65,0X39);
ADV7619RegSet(0X6C,0X66,0X41);
ADV7619RegSet(0X6C,0X67,0X0A);
ADV7619RegSet(0X6C,0X68,0X20);
ADV7619RegSet(0X6C,0X69,0X20);
ADV7619RegSet(0X6C,0X6A,0X20);
ADV7619RegSet(0X6C,0X6B,0X20);
ADV7619RegSet(0X6C,0X6C,0X00);
ADV7619RegSet(0X6C,0X6D,0X00);
ADV7619RegSet(0X6C,0X6E,0X00);
ADV7619RegSet(0X6C,0X6F,0XFD);
ADV7619RegSet(0X6C,0X70,0X00);
ADV7619RegSet(0X6C,0X71,0X17);
ADV7619RegSet(0X6C,0X72,0X3D);
ADV7619RegSet(0X6C,0X73,0X0D);
ADV7619RegSet(0X6C,0X74,0X2E);
ADV7619RegSet(0X6C,0X75,0X11);
ADV7619RegSet(0X6C,0X76,0X00);
ADV7619RegSet(0X6C,0X77,0X0A);
ADV7619RegSet(0X6C,0X78,0X20);
ADV7619RegSet(0X6C,0X79,0X20);
ADV7619RegSet(0X6C,0X7A,0X20);
ADV7619RegSet(0X6C,0X7B,0X20);
ADV7619RegSet(0X6C,0X7C,0X20);
ADV7619RegSet(0X6C,0X7D,0X20);
ADV7619RegSet(0X6C,0X7E,0X01);
ADV7619RegSet(0X6C,0X7F,0X1C);
ADV7619RegSet(0X6C,0X80,0X02);
ADV7619RegSet(0X6C,0X81,0X03);
ADV7619RegSet(0X6C,0X82,0X34);
ADV7619RegSet(0X6C,0X83,0X71);
ADV7619RegSet(0X6C,0X84,0X4D);
ADV7619RegSet(0X6C,0X85,0X82);
ADV7619RegSet(0X6C,0X86,0X05);
ADV7619RegSet(0X6C,0X87,0X04);
ADV7619RegSet(0X6C,0X88,0X01);
ADV7619RegSet(0X6C,0X89,0X10);
ADV7619RegSet(0X6C,0X8A,0X11);
ADV7619RegSet(0X6C,0X8B,0X14);
ADV7619RegSet(0X6C,0X8C,0X13);
ADV7619RegSet(0X6C,0X8D,0X1F);
ADV7619RegSet(0X6C,0X8E,0X06);
ADV7619RegSet(0X6C,0X8F,0X15);
ADV7619RegSet(0X6C,0X90,0X03);
ADV7619RegSet(0X6C,0X91,0X12);
ADV7619RegSet(0X6C,0X92,0X35);
ADV7619RegSet(0X6C,0X93,0X0F);
ADV7619RegSet(0X6C,0X94,0X7F);
ADV7619RegSet(0X6C,0X95,0X07);
ADV7619RegSet(0X6C,0X96,0X17);
ADV7619RegSet(0X6C,0X97,0X1F);
ADV7619RegSet(0X6C,0X98,0X38);
ADV7619RegSet(0X6C,0X99,0X1F);
ADV7619RegSet(0X6C,0X9A,0X07);
ADV7619RegSet(0X6C,0X9B,0X30);
ADV7619RegSet(0X6C,0X9C,0X2F);
ADV7619RegSet(0X6C,0X9D,0X07);
ADV7619RegSet(0X6C,0X9E,0X72);
ADV7619RegSet(0X6C,0X9F,0X3F);
ADV7619RegSet(0X6C,0XA0,0X7F);
ADV7619RegSet(0X6C,0XA1,0X72);
ADV7619RegSet(0X6C,0XA2,0X57);
ADV7619RegSet(0X6C,0XA3,0X7F);
ADV7619RegSet(0X6C,0XA4,0X00);
ADV7619RegSet(0X6C,0XA5,0X37);
ADV7619RegSet(0X6C,0XA6,0X7F);
ADV7619RegSet(0X6C,0XA7,0X72);
ADV7619RegSet(0X6C,0XA8,0X83);
ADV7619RegSet(0X6C,0XA9,0X4F);
ADV7619RegSet(0X6C,0XAA,0X00);
ADV7619RegSet(0X6C,0XAB,0X00);
ADV7619RegSet(0X6C,0XAC,0X67);
ADV7619RegSet(0X6C,0XAD,0X03);
ADV7619RegSet(0X6C,0XAE,0X0C);
ADV7619RegSet(0X6C,0XAF,0X00);
ADV7619RegSet(0X6C,0XB0,0X10);
ADV7619RegSet(0X6C,0XB1,0X00);
ADV7619RegSet(0X6C,0XB2,0X88);
ADV7619RegSet(0X6C,0XB3,0X2D);
ADV7619RegSet(0X6C,0XB4,0X00);
ADV7619RegSet(0X6C,0XB5,0X00);
ADV7619RegSet(0X6C,0XB6,0X00);
ADV7619RegSet(0X6C,0XB7,0XFF);
ADV7619RegSet(0X6C,0XB8,0X00);
ADV7619RegSet(0X6C,0XB9,0X0A);
ADV7619RegSet(0X6C,0XBA,0X20);
ADV7619RegSet(0X6C,0XBB,0X20);
ADV7619RegSet(0X6C,0XBC,0X20);
ADV7619RegSet(0X6C,0XBD,0X20);
ADV7619RegSet(0X6C,0XBE,0X20);
ADV7619RegSet(0X6C,0XBF,0X20);
ADV7619RegSet(0X6C,0XC0,0X20);
ADV7619RegSet(0X6C,0XC1,0X20);
ADV7619RegSet(0X6C,0XC2,0X20);
ADV7619RegSet(0X6C,0XC3,0X20);
ADV7619RegSet(0X6C,0XC4,0X20);
ADV7619RegSet(0X6C,0XC5,0X20);
ADV7619RegSet(0X6C,0XC6,0X00);
ADV7619RegSet(0X6C,0XC7,0X00);
ADV7619RegSet(0X6C,0XC8,0X00);
ADV7619RegSet(0X6C,0XC9,0XFF);
ADV7619RegSet(0X6C,0XCA,0X00);
ADV7619RegSet(0X6C,0XCB,0X0A);
ADV7619RegSet(0X6C,0XCC,0X20);
ADV7619RegSet(0X6C,0XCD,0X20);
ADV7619RegSet(0X6C,0XCE,0X20);
ADV7619RegSet(0X6C,0XCF,0X20);
ADV7619RegSet(0X6C,0XD0,0X20);
ADV7619RegSet(0X6C,0XD1,0X20);
ADV7619RegSet(0X6C,0XD2,0X20);
ADV7619RegSet(0X6C,0XD3,0X20);
ADV7619RegSet(0X6C,0XD4,0X20);
ADV7619RegSet(0X6C,0XD5,0X20);
ADV7619RegSet(0X6C,0XD6,0X20);
ADV7619RegSet(0X6C,0XD7,0X20);
ADV7619RegSet(0X6C,0XD8,0X00);
ADV7619RegSet(0X6C,0XD9,0X00);
ADV7619RegSet(0X6C,0XDA,0X00);
ADV7619RegSet(0X6C,0XDB,0XFF);
ADV7619RegSet(0X6C,0XDC,0X00);
ADV7619RegSet(0X6C,0XDD,0X0A);
ADV7619RegSet(0X6C,0XDE,0X20);
ADV7619RegSet(0X6C,0XDF,0X20);
ADV7619RegSet(0X6C,0XE0,0X20);
ADV7619RegSet(0X6C,0XE1,0X20);
ADV7619RegSet(0X6C,0XE2,0X20);
ADV7619RegSet(0X6C,0XE3,0X20);
ADV7619RegSet(0X6C,0XE4,0X20);
ADV7619RegSet(0X6C,0XE5,0X20);
ADV7619RegSet(0X6C,0XE6,0X20);
ADV7619RegSet(0X6C,0XE7,0X20);
ADV7619RegSet(0X6C,0XE8,0X20);
ADV7619RegSet(0X6C,0XE9,0X20);
ADV7619RegSet(0X6C,0XEA,0X00);
ADV7619RegSet(0X6C,0XEB,0X00);
ADV7619RegSet(0X6C,0XEC,0X00);
ADV7619RegSet(0X6C,0XED,0X00);
ADV7619RegSet(0X6C,0XEE,0X00);
ADV7619RegSet(0X6C,0XEF,0X00);
ADV7619RegSet(0X6C,0XF0,0X00);
ADV7619RegSet(0X6C,0XF1,0X00);
ADV7619RegSet(0X6C,0XF2,0X00);
ADV7619RegSet(0X6C,0XF3,0X00);
ADV7619RegSet(0X6C,0XF4,0X00);
ADV7619RegSet(0X6C,0XF5,0X00);
ADV7619RegSet(0X6C,0XF6,0X00);
ADV7619RegSet(0X6C,0XF7,0X00);
ADV7619RegSet(0X6C,0XF8,0X00);
ADV7619RegSet(0X6C,0XF9,0X00);
ADV7619RegSet(0X6C,0XFA,0X00);
ADV7619RegSet(0X6C,0XFB,0X00);
ADV7619RegSet(0X6C,0XFC,0X00);
ADV7619RegSet(0X6C,0XFD,0X00);
ADV7619RegSet(0X6C,0XFE,0X00);
ADV7619RegSet(0X6C,0XFF,0XDA);
ADV7619RegSet(0X64,0X77,0X00); //Set the Most Significant Bit of the SPA location to 0
ADV7619RegSet(0X64,0X52,0X20); //Set the SPA for port B.
ADV7619RegSet(0X64,0X53,0X00); //Set the SPA for port B.
ADV7619RegSet(0X64,0X70,0X9E); //Set the Least Significant Byte of the SPA location
ADV7619RegSet(0X64,0X74,0X03); //Enable the Internal EDID for Ports

ADV7619RegSet(0x68, 0xC0, 0x03); //ADI Required Write
ADV7619RegSet(0x98, 0x01, 0x06); //Prim_Mode =110b HDMI-GR
ADV7619RegSet(0x98, 0x02, 0xF7); //Auto CSC, 0xRGB, 0xSet op_656 bit
ADV7619RegSet(0x98, 0x03, 0x82); //24 bit SDR 422 Mode 0
ADV7619RegSet(0x98, 0x05, 0x28); //AV Codes Off
ADV7619RegSet(0x98, 0x06, 0xA0); //No inversion on VS,HS pins
ADV7619RegSet(0x98, 0x0C, 0x42); //Power up part
ADV7619RegSet(0x98, 0x15, 0x80); //Disable Tristate of Pins
ADV7619RegSet(0x98, 0x19, 0x83); //LLC DLL phase
ADV7619RegSet(0x98, 0x33, 0x40); //LLC DLL MUX enable
ADV7619RegSet(0x44, 0xBA, 0x01); //Set HDMI FreeRun
ADV7619RegSet(0x44, 0x6C, 0x00); //Required ADI write
ADV7619RegSet(0x64, 0x40, 0x81); //Disable HDCP 1.1 features
ADV7619RegSet(0x4C, 0xB5, 0x01); //Setting MCLK to 256Fs
ADV7619RegSet(0x68, 0xC0, 0x03); //ADI Required write
ADV7619RegSet(0x68, 0x00, 0x08); //Set HDMI Input Port A (BG_MEAS_PORT_SEL = 001b)
ADV7619RegSet(0x68, 0x02, 0x03); //ALL BG Ports enabled
ADV7619RegSet(0x68, 0x03, 0x98); //ADI Required Write
ADV7619RegSet(0x68, 0x10, 0xA5); //ADI Required Write
ADV7619RegSet(0x68, 0x1B, 0x08); //ADI Required Write
ADV7619RegSet(0x68, 0x45, 0x04); //ADI Required Write
ADV7619RegSet(0x68, 0x97, 0xC0); //ADI Required Write
ADV7619RegSet(0x68, 0x3D, 0x10); //ADI Required Write
ADV7619RegSet(0x68, 0x3E, 0x69); //ADI Required Write
ADV7619RegSet(0x68, 0x3F, 0x46); //ADI Required Write
ADV7619RegSet(0x68, 0x4E, 0xFE); //ADI Required Write
ADV7619RegSet(0x68, 0x4F, 0x08); //ADI Required Write
ADV7619RegSet(0x68, 0x50, 0x00); //ADI Required Write
ADV7619RegSet(0x68, 0x57, 0xA3); //ADI Required Write
ADV7619RegSet(0x68, 0x58, 0x07); //ADI Required Write
ADV7619RegSet(0x68, 0x6F, 0x08); //ADI Required Write
ADV7619RegSet(0x68, 0x83, 0xFC); //Enable clock terminators for port A & B
ADV7619RegSet(0x68, 0x84, 0x03); //ADI Required Write
ADV7619RegSet(0x68, 0x85, 0x11); //ADI Required Write
ADV7619RegSet(0x68, 0x86, 0x9B); //ADI Required Write
ADV7619RegSet(0x68, 0x89, 0x03); //ADI Required Write
ADV7619RegSet(0x68, 0x9B, 0x03); //ADI Required Write
ADV7619RegSet(0x68, 0x93, 0x03); //ADI Required Write
ADV7619RegSet(0x68, 0x5A, 0x80); //ADI Required Write
ADV7619RegSet(0x68, 0x9C, 0x80); //ADI Required Write
ADV7619RegSet(0x68, 0x9C, 0xC0); //ADI Required Write
ADV7619RegSet(0x68, 0x9C, 0x00); //ADI Required Write
ADV7619RegSet(0x72, 0x01, 0x00); //Set N Value(6144)
ADV7619RegSet(0x72, 0x02, 0x18); //Set N Value(6144)
ADV7619RegSet(0x72, 0x03, 0x00); //Set N Value(6144)
ADV7619RegSet(0x72, 0x15, 0x01); //24bit Input 422 (YCrCb) with Separate Syncs, 0x44.1kHz fs
ADV7619RegSet(0x72, 0x16, 0x61); //YCrCb 444
ADV7619RegSet(0x72, 0x18, 0x46); //CSC disabled
ADV7619RegSet(0x72, 0x3B, 0x80); //PR Auto Mode
ADV7619RegSet(0x72, 0x40, 0x80); //General Control Packet Enable
ADV7619RegSet(0x72, 0x41, 0x10); //Power Down control
ADV7619RegSet(0x72, 0x48, 0x08); //Data right justified
ADV7619RegSet(0x72, 0x49, 0xA8); //Set Dither_mode - 12-to-10 bit
ADV7619RegSet(0x72, 0x4C, 0x04); //8 bit Output
ADV7619RegSet(0x72, 0x55, 0x00); //Set RGB 444 in AVinfo Frame
ADV7619RegSet(0x72, 0x56, 0x08); //Set active format Aspect
ADV7619RegSet(0x72, 0x96, 0x20); //HPD Interrupt clear
ADV7619RegSet(0x72, 0x98, 0x03); //ADI Required Write
ADV7619RegSet(0x72, 0x99, 0x02); //ADI Required Write
ADV7619RegSet(0x72, 0x9C, 0x30); //PLL Filter R1 Value
ADV7619RegSet(0x72, 0x9D, 0x61); //Set clock divide
ADV7619RegSet(0x72, 0xA2, 0xA4); //ADI Required Write
ADV7619RegSet(0x72, 0xA3, 0xA4); //ADI Required Write
ADV7619RegSet(0x72, 0xAF, 0x16); //Set HDMI Mode
ADV7619RegSet(0x72, 0xBA, 0x60); //No clock delay
ADV7619RegSet(0x72, 0xDE, 0x9C); //ADI Required Write
ADV7619RegSet(0x72, 0xE4, 0x60); //VCO Swing Reference Voltage
ADV7619RegSet(0x72, 0xFA, 0x7D); //Nbr of times to search for good phase

/* Enable EDID for PC HDMI output */
ADV7619RegSet(0x64, 0x74, 0x3); //EDID_A_ENABLE, Addr 64 (Repeater), Address 0x74[0](port A) Address 0x74[1] (portB)

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.