Post Go back to editing

GMSL Serialiser and deserialisers parts for HDMI / LVDS with Audio Support for 4K video Broadcast

Category: Hardware
Product Number: MAX9268
Software Version: 01

Hi Team ,

I am searching for Audio and Video 4K (4K / UHD  30Hz fpsTransmission chipset for my optical communication 

is there any chipset which gives me HDMI / LVDS as input and Output with  GMSL2/3 . Serializer  and  GMSL2/3 input to HDMI/LVDS output Deserializer .

can MAX9249 and MAX9268 work for my application ( are they support 4K video resolution  4K / UHD  30Hz fps work for me) ?

Regards,

Nikunj

Parents
  • Hi,

       We have chipset which can support HDMI input with MIPI-CSI output but we don't have any part which can support GMSL output. Please refer below snap.

      Can MAX9249 and MAX9268 work for my application ( are they support 4K video resolution  4K / UHD  30Hz fps work for me) ?

          This two parts seems it can support clock upto 104Mhz So it doesn't support 4K video formats and note that for 4K, the part should support clock upto 300MHz.

    Thanks,

    Poornima

Reply
  • Hi,

       We have chipset which can support HDMI input with MIPI-CSI output but we don't have any part which can support GMSL output. Please refer below snap.

      Can MAX9249 and MAX9268 work for my application ( are they support 4K video resolution  4K / UHD  30Hz fps work for me) ?

          This two parts seems it can support clock upto 104Mhz So it doesn't support 4K video formats and note that for 4K, the part should support clock upto 300MHz.

    Thanks,

    Poornima

Children