Post Go back to editing

Need a suitable IC which meets my requirement of switching between two video inputs.

Category: Hardware

Hi,

we need a suitable IC which meets my requirement  of switching between two video inputs and gives out one video output. 

Another requirement is one input which should split into four video outputs.

1. Two PAL video inputs by selection gives out one PAL video output.

2. One PAL video input, which should split into four PAL video outputs.

3. One HD-SDI video input which should split into two HD-SDI video outputs.

for the above requirement, please suggest the suitable IC's and any reference design for the same can be provided.

BR

satya

Parents
  • Hi,

       All our video decoders are single video channel parts and there is only one output bus so we would need 2 ADV part to process two inputs simultaneously similarly for 3 channels, we would need 3 ADV parts. 

       Please note that "ADI does not have a chip that can handle multiple video streams at the same time.

       As far as all analog video decoders can only select (and thus output) one stream at a time.

       If a project requires multiple video streams simultaneously, they will need multiple video decoder parts.

    Thanks,

    Poornima

Reply
  • Hi,

       All our video decoders are single video channel parts and there is only one output bus so we would need 2 ADV part to process two inputs simultaneously similarly for 3 channels, we would need 3 ADV parts. 

       Please note that "ADI does not have a chip that can handle multiple video streams at the same time.

       As far as all analog video decoders can only select (and thus output) one stream at a time.

       If a project requires multiple video streams simultaneously, they will need multiple video decoder parts.

    Thanks,

    Poornima

Children