Post Go back to editing

STANAG Lock and Resolution detection issue with adv7403.

Category: Software
Product Number: adv7403
Software Version: Petalinux

Hi,

I have the following requirements for ADV7403:

I/P Video - STANAG 3350 with Sync On Green as Input to the Chip.

1)720x576i @ 50/25Hz(Class B)video resolution, Interlaced video input,RGB(STANAG Class B)
2)720x480i @ 60/30Hz(Class C)video resolution, Interlaced video input,RGB(STANAG Class C)

O/P Video - 16bit YCbCr 4:2:2 as output from the chip.

Hardware Connections:
We have custom hardware with ADV7403 chip whose input channel configuration for RGsB is given below

Ain1 - G and SOG
Ain2 - B
Ain3 - R

How do we configure interrupt?
How do we detect the lock and unlock signal?
How do we detect resolution for the connected source?

Thanks and Regards,
Gladson

  • Hi,

       Please find the below comments,

     1. How do we configure interrupt ?

        Please make sure with following things for configuring the interrupt (INT1),

    IO Map 0x40 0xE1  ( Active until Cleared, Drive low when active)
      1) Unmask required bits.
      2) Clear the interrupt.
      3) Wait for interrupt to occur.
      4) Once interrupt occurs the STATUS bit will go high. The RAW bit will also go high while the event occurs. The Interrupt pin (INT1) will also become active.
      5) The interrupt should be then cleared.

    Also ensure that you have correctly configured the interrupt - Our interrupts are open drain by default which requires a pull up resistor external to the part. The interrupt can also be configured as "drives low when active" or "drives high when active".

    2. How do we detect the lock and unlock signal?

         By reading the below status register, We came to know whether input signal is in lock or un lock status.

         Also we can able to detect the locking status by using SDP/CP interrupt lock related registers.

    3. How do we detect resolution for the connected source?

         We can use STDI module for format/resolution information. For more details Please refer section Standard detection and identification.

    Thanks,

    Poornima

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.