Hi,
Please tell me about ADV7282.
A video signal is input and the output result is monitored.
The image scrolls up and down as if there is a vertical sync shift under certain conditions.
Even if you compare the video signal waveforms (with / without an event), there is no difference in the waveforms and the cause cannot be understood.
Could you please tell me under what conditions vertical synchronization deviation occurs?
For certain conditions, the details are as follows:
[conditions]
The input camera video signal is 2ch (black and white, color).
In addition, the cameras (2 units) are installed on a table driven by a servo motor.
Scrolling up and down the image occurs under the following specific conditions.
(Also, it occurs only in black and white.)
[Specific conditions]
-When the drive power supply (servo motor) is started and the camera is switched (color → black and white), the image scrolls up and down.
-When the drive power supply (servo motor) is started and the camera is switched (black and white → color), no event occurs.
-When the drive power supply (servo motor) is turned off, no event occurs even if the camera is switched (color → black and white, black and white → color).
-Even if the drive power supply (servo motor) is started with the camera (black and white) fixed, no event occurs.
-Even if the drive power supply (servo motor) is turned off while the image is scrolling up and down, the image remains scrolled up and down.
[Acquired waveform]
The NTSC waveform (the input part to the board and the enlargement of the vertical synchronization part) is attached. (Normal, when an event occurs)
・Normal
・Event Occurs
Best Regards,
kazuhiko