Hi,
I am using the ADI recommended script file (01_21) of "ADV7481ES3C-VER.3.6c.txt".
I have two questions about the contents of the document "ADV7481_UG-747.pdf", which is not explained with " - ".
Q1:
I am sending the (hdmi_register_02h) ”68 83 00” command in the initialization sequence.
If the "68 83 00" command is not sent (initial value 0xFF), what is the impact?
Q2:
I am sending the (mute_ctrl) ”68 1A 80” command in the initialization sequence.
If this bit7 is set to zero, what is the impact?
Best Regards.