Post Go back to editing

No video output from ADV7403 with analog RGsB (sync on green) configuration

Category: Hardware
Product Number: ADV7403

Hello,

We are trying to bring up analog RGB with sync on green to ITU-R.BT656 on a custom board. While the input is locked and valid video is recognized by the CP (from STATUS_2 register, addr: 0x12), the digital output does not contain ITU-R.BT656 data. 

We have connected RGB to AIN1,2,3 and green also to SOG pin as given in the example schematic in the datasheet. Different combinations of the configurations were tried (script used is 625I SCART RGB IN In Thru CP YPrPb 2X1 10 Bit 422 Out, with changes for manual muxing). We have also attempted to connect composite and used the script provided by ADI for autodetection (through AIN10) but in that case the SDP is free-running and has not recognized the video. 

Please find the configurations below (addr, data):

Script 1 (RGsB, CP mode, 625i 2x2):

0x00  0x00 
0x05  0x01 
0x06  0x01 
0xF1  0x0C
0xC3  0x31
0xC4  0xC2
0x03  0x00
0x04  0x57 
0x1D  0x47
0x31  0x02
0x3A  0x10
0x3B  0x80
0x3D  0xA2
0x3E  0x6A
0x3F  0xA0
0x4D  0xEE
0x67  0x01
0x73  0xD0
0x74  0x04
0x75  0x01
0x76  0x00
0x77  0x04
0x78  0x08
0x79  0x02
0x7A  0x00
0x86  0x0B
0x93  0x78
0x94  0x23
0x95  0x11
0x96  0xC0
0xC5  0x00
0xED  0xC4
0xF3  0x0F
0xC3  0xB9
0x0E  0x80
0x52  0x46
0x54  0x00
0x7F  0xFF
0x81  0x30
0x90  0xC9
0x91  0x40
0x92  0x3C
0x93  0xCA
0x94  0xD5
0xB6  0x08
0xC0  0x9A
0xCF  0x50
0xD0  0x4E
0xD1  0xB9
0xD6  0xDD
0xD7  0xE2
0xE5  0x51
0x0E  0x00

Script 2 (RGsB, CP mode, 625i 4x2):

0x00  0x00 
0x05  0x01 
0x06  0x03 
0xF1  0x0C
0xC3  0x31
0xC4  0xC2
0x03  0x00
0x04  0x57 
0x1D  0x47
0x31  0x02
0x3A  0x10
0x3B  0x80
0x3D  0xA2
0x3E  0x6A
0x3F  0xA0
0x4D  0xEE
0x67  0x01
0x73  0xD0
0x74  0x04
0x75  0x01
0x76  0x00
0x77  0x04
0x78  0x08
0x79  0x02
0x7A  0x00
0x86  0x0B
0x93  0x78
0x94  0x23
0x95  0x11
0x96  0xC0
0xC5  0x00
0xED  0xC4
0xF3  0x0F
0xC3  0xB9
0x0E  0x80
0x52  0x46
0x54  0x00
0x7F  0xFF
0x81  0x30
0x90  0xC9
0x91  0x40
0x92  0x3C
0x93  0xCA
0x94  0xD5
0xB6  0x08
0xC0  0x9A
0xCF  0x50
0xD0  0x4E
0xD1  0xB9
0xD6  0xDD
0xD7  0xE2
0xE5  0x51
0x0E  0x00

Script 3 (used for composite detection):

0x00   0x0E
0x03   0x00
0x04   0x77
0x17   0x41
0x1D   0x47
0x31   0x02
0x3A   0x17
0x3B   0x80
0x3D   0xA2
0x3E   0x6A
0x3F   0xA0
0x86   0x0B
0xF3   0x01
0xF9   0x03
0x0E   0x80
0x52   0x46
0x54   0x00
0x7F   0xFF
0x81   0x30
0x90   0xC9
0x91   0x40
0x92   0x3C
0x93   0xCA
0x94   0xD5
0xB1   0xFF
0xB6   0x08
0xC0   0x9A
0xCF   0x50
0xD0   0x4E
0xD1   0xB9
0xD6   0xDD
0xD7   0xE2
0xE5   0x51
0x0E   0x00

Please let us know what is to be done at the earliest.