Post Go back to editing

[ADV7189] I2C communication Not reponding at specific LOT.

Thread Summary

The user is experiencing I2C responding errors during boot sessions with the ADV7189 video processing module. The final answer suggests verifying reset and power-down pin control, power rail stability, correct SDA and SCL pin connections, proper pull-up resistor values, and signal integrity. Additionally, the user should check if other devices on the I2C bus are accessible and ensure the I2C software routines use the correct address format (7-bit or 8-bit).
AI Generated Content
Category: Hardware
Product Number: ADV7189BBSTZ


Hi, I'm looking forward to get some help.

Our video processing modules are using ADV7189, and this solution
used for more than 10 years for mission critical solution.

But for these days, we are suffering from I2C responding error while
boot session.

Have you ever get reported about fake component or failed lot around
2020~2022 ?

  • Hi,

       Could you please ensure with below things,

        1.Ensure Reset and Power-down pins are controlled during I2C communication
        2.Make sure the power rails are good
        3.Make sure the device is out of reset and the reset goes high after both power rails are stable.
        4.Make sure SDA and SCL signals are going to the right pins. 
        5.Verify the pull up resistors on SDA and SCL as per reference schematic.
        6.Verify the SDA and SCK signals wiggle and are the right amplitude.
        7.Check to see if you can access anything else tied to the I2C bus, like eeprom.  Tie something to the bus to make sure the bus is working as expected.

      Also check I2C software routines expect 7-bit addresses or 8-bit addresses.
      Below is a good application please note on that:
       7-bit, 8-bit, and 10-bit I2C Slave Addressing – Total Phase

    Please refer this thread, Here expert given some suggestion about the I2C problem (+) ADV7280A I2C problem - Q&A - Video - EngineerZone (analog.com)

    Thanks,

    Poornima

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.