Post Go back to editing

HDMI2.1 retimer(redriver) IC

Category: Datasheet/Specs

My customer want to get some recommendation about HDMI2.1 retimer(redriver) IC from ADI.

Requirement Specs are like below. And it will be applied to TV application.

- Support HDMI2.1 signal conditioning.

- Support pin mode or I2C mode for equalization, DC gain and output swing configuration.

Do we have any candidates for this requirement? And, ADV7674's repeater mode is suitable for the requirement?

Also, please let me know the meaning of the retimer(redriver) IC on the HDMI part if you can.

Thanks,

Top Replies

  • FormerMember
    FormerMember
May 3, 2023 in reply to TTAEKYU +1 verified

Yes, those a good devices if you need a 4:1 mux.  Note the -D does not have any audio ports so it cannot do audio insertion/extraction.  If you are only doing a single channel retiming then the ADV7671 might…

Parents
  • FormerMember
    0 FormerMember
on May 2, 2023 8:54 AM

The ADV7671 might be a candidate, Up to 48Gbps and handle HDCP 2.3.  You don't need to utilize the audio port, just set it up as a true pass through.

www.analog.com/.../adv7671.html

  • Thank you for your reply.

    Then, Can the ADV76748A or ADV76748D be a candidate? 

  • FormerMember
    +1 FormerMember on May 3, 2023 10:22 AM in reply to TTAEKYU

    Yes, those a good devices if you need a 4:1 mux.  Note the -D does not have any audio ports so it cannot do audio insertion/extraction.  If you are only doing a single channel retiming then the ADV7671 might be a better choice.  I'd need more information on you system requirements to offer a suggestion of which is better ADV7671, ADV7671A, ADV7672 or ADV7674

  • Reply
    • FormerMember
      +1 FormerMember
    on May 3, 2023 10:22 AM in reply to TTAEKYU

    Yes, those a good devices if you need a 4:1 mux.  Note the -D does not have any audio ports so it cannot do audio insertion/extraction.  If you are only doing a single channel retiming then the ADV7671 might be a better choice.  I'd need more information on you system requirements to offer a suggestion of which is better ADV7671, ADV7671A, ADV7672 or ADV7674

    Children
    No Data