What are the requirements (capacitance, ESR, drive level, etc) for the 28.63636MHz XTAL for the ADV7611?
We are looking at a couple of XTAL options (table below), can we can get confirmation that they would be compatible?
ADV7611
Recommended for New Designs
The ADV7611 is offered in automotive, professional (no HDCP), and industrial versions. The operating temperature range is -40°C to +85°C.
The UG-180 contains...
Datasheet
ADV7611 on Analog.com
What are the requirements (capacitance, ESR, drive level, etc) for the 28.63636MHz XTAL for the ADV7611?
We are looking at a couple of XTAL options (table below), can we can get confirmation that they would be compatible?
The original crystal oscillator was designed with the MA01377 used in the simulations. All later devices used the same oscillator circuit design.
All four shown here appear to be compatible.
This application note applies to these oscillator circuits.
Of course the real test will be on the final board and run over temperature.
The original crystal oscillator was designed with the MA01377 used in the simulations. All later devices used the same oscillator circuit design.
All four shown here appear to be compatible.
This application note applies to these oscillator circuits.
Of course the real test will be on the final board and run over temperature.