Hello,
We are using ADV7393 to output an NTSC video signal on its DAC output pin DAC1 (pin 28). The chip is being used in low-drive operation with a 300 Ohm load.
An offset of 40mV-50mV (with respect to GND) was observed on the output video signal. The offset is observed even when the output is decoupled from the rest of the circuitry (while still leaving the 300 Ohm load). The same DC offset is observed on the output when the video signal is turned off/disabled.
I'll ask questions that were asked in a similar thread for the ADV7341 chip (linked here: RE: DC Offset on ADV7341 video output).
1) Is there a way to remove or minimize this offset with either a register setting or a passive component change?
2) What is causing this offset? Is this an inherent characteristic of the chip?

Our video image quality is good, however, this offset is causing us to fail one of our requirements. We are looking for a solution that does not require additional circuitry (e.g., AC coupling into a buffer to remove the offset).
Regards,
Aki