Post Go back to editing

AD7619 IO 0x02

Category: Datasheet/Specs
Product Number: AD7619

Hi.

Is it necessary to change the setting of IO: 0x02 "INP_COLOR_SPACE[3:0],RGB_OUT,ALT_GAMMA" according to the color space of the input video?

If automatic setting is fine, is default value 0x02 = "11110000:F0h" okay?

Best regards.

Parents
  • Hi,

    Please find the below comments,

      Is it necessary to change the setting of IO: 0x02 "INP_COLOR_SPACE[3:0],RGB_OUT,ALT_GAMMA" according to the color space of the input video ?

        Yes, We can use these three registers for setting the Input and output color space.

    If automatic setting is fine, is default value 0x02 = "11110000:F0h" okay?

      INP_COLOR_SPACE[3:0] control is used to set the color space of the input video and this to be used in conjunction with ALT_GAMMA and RGB_OUT to configure the required Color Space . 

    Thanks,

    Poornima

Reply
  • Hi,

    Please find the below comments,

      Is it necessary to change the setting of IO: 0x02 "INP_COLOR_SPACE[3:0],RGB_OUT,ALT_GAMMA" according to the color space of the input video ?

        Yes, We can use these three registers for setting the Input and output color space.

    If automatic setting is fine, is default value 0x02 = "11110000:F0h" okay?

      INP_COLOR_SPACE[3:0] control is used to set the color space of the input video and this to be used in conjunction with ALT_GAMMA and RGB_OUT to configure the required Color Space . 

    Thanks,

    Poornima

Children