Post Go back to editing

ADV7181D PLL Jitter Improvement

Category: Hardware
Product Number: ADV7181D

Regarding EVAL_ADV7181DEBZ, the recommended setting (SD CVBS) of Materials (ADV7181D_ADV7181D@_ADV7341-VER.1.0c.txt) is sent and the CVBS from TSG-170D is input to get Y output.
I checked the SD/HS/3G/12G-SDI performance using this Y output (black burst signal) as a GENLOCK reference, but the SDI timing jitter exceeds the SMPTE standard values.
(PHABRIX's Qx (rasterizer) can measure it) This problem does not occur when the TSG-170D signal is used and directly input as a GENLOCK reference.

Therefore, I think I should improve the PLL clock jitter of the ADV7181D.
I wonder if there is a register to change various PLL settings in SD mode for the better jitter?
As for the resister "0x3C[2:0]: PLL_QPUMP", I tried changing it, but it didn't work very much.

Parents on Mar 15, 2023 9:54 AM in reply to PoornimaSubramani
0

PLL jitter can also be caused by schematic implementation and layout

  • Encoder is ADV7341 mounted on EVAL_ADV7181D board.
    The setting is also sending "SD CVBS (Address 0x56)" of "ADV7181D_ADV7181D@_ADV7341-VER.1.0c.txt".
    The Jitter characteristics of Y(DAC1) measured by VM700T are shown below.
    Jitter measurements are very unstable.

    Best regards,

  • Regarding the layout of the EVAL_ADV7181D board,
    The CR component connected to pin-30 (ELF) appears to be far from the terminal.
    Is this layout the best pattern?

  • FormerMember
    FormerMember on Mar 15, 2023 9:46 PM in reply to CTCMO
    0

    In general the ELF components should be as close to pin 30 as possible and supplied by a clean PVDD_1.8V.

    Beyond that this board is a 10+ year old design and has not shown any jitter issues in the past.

    There is a note in the manual "Any noise that gets onto the HS_IN input trace will add jitter to the system".  But since you are using CVBS only HS_IN should be quiet.  Out of curiosity you might try grounding HS_IN.  By default this input is left floating

    The ADV7341 CLKIN_x input jitter limit is 2ns

    Note CVBS jitter should be < 1ns

    I'm beginning to wonder if this board has been damaged somehow.

    1) Can you check the ADV7181 LLC signal for jitter . Quick check.

  • I measured LLC (PCLK) Clock Jitter.

          

    Also, I changed HS_IN from open to GND connection.

    However, there was no change in SDI characteristics (Timing Jitter) during GENLOCK due to CVBS

    and LCC Clock Jitter characteristics.

  • FormerMember
    FormerMember on Mar 23, 2023 12:10 PM in reply to CTCMO
    0

    At this point all I can suggest is there is some issue with this particular board.  Do you have access to another EVAL-ADV7181D board?

  • EVAL-ADV7181DEBZ is very expensive, so I only own one.
    I have one EVAL-ADV7182AEBZ, so I did the same evaluation.

    The result of CVBS output Jitter rampage was the same as EVAL-ADV7181D.
    Also, the SDI characteristics (Timing Jitter) during genlock synchronization with CVBS did not meet the SMPTE standard, and was the same as the EVAL-ADV7181D.
    Therefore, I don't think it's an issue only for the EVAL-ADV7181DEBZ that I own.
    (It is very likely that other EVAL-ADV7181DEBZ will have the same characteristics.)
    Could it be that the CVBS output via the ANALOG DEVICE Decoder is not suitable for SDI genlock synchronization?

  • FormerMember
    FormerMember on Mar 23, 2023 10:44 PM in reply to CTCMO
    0

    Both the ADV7182 and ADV7181D implement Adaptive Digital Line Length Tracking (ADLLT) which is designed to track variable sources like VCRs.  It might be that this circuit adds some jitter noise to the output.  I have no evidence of this.

    One possible test (remove input) is to set the chip in free run mode and check the output jitter again.  Not sure if will give us useful information but i would try if I had the setup here.

  • Regarding EVAL-ADV7181DEBZ, I did Jitter measurement in Free-run (Blue screen).
    Compared to CVBS input, Jitter characteristics changed, but "CVBS-jitter periodic rampage" can be confirmed.
    SDI characteristics (Timing Jitter) when free-run mode output is genlock-synchronized periodically repeats OK and NG of SMPTE standard values. There may be a correlation with "periodic rampage of CVBS-jitter".

    Paste the video.
    001: TG700 Jitter
    002: Jitter when CVBS is input to EVAL-ADV7181D
    003: Jitter in Free-rum mode of EVAL-ADV7181D
    004_Free-run_EVAL-ADV7181D_and_PHABRIX(12G-SDI_TimingJitter)

  • Reply
    • Regarding EVAL-ADV7181DEBZ, I did Jitter measurement in Free-run (Blue screen).
      Compared to CVBS input, Jitter characteristics changed, but "CVBS-jitter periodic rampage" can be confirmed.
      SDI characteristics (Timing Jitter) when free-run mode output is genlock-synchronized periodically repeats OK and NG of SMPTE standard values. There may be a correlation with "periodic rampage of CVBS-jitter".

      Paste the video.
      001: TG700 Jitter
      002: Jitter when CVBS is input to EVAL-ADV7181D
      003: Jitter in Free-rum mode of EVAL-ADV7181D
      004_Free-run_EVAL-ADV7181D_and_PHABRIX(12G-SDI_TimingJitter)

    Children
    No Data