ADV7611
Recommended for New Designs
The ADV7611 is offered in automotive, professional (no HDCP), and industrial versions. The operating temperature range is −40°C to +85°C.
The UG-180...
Datasheet
ADV7611 on Analog.com
AD9398
Obsolete
The AD9398 offers a high definition multimedia interface (HDMI) receiver integrated on a single chip. Also included is support for high bandwidth digital...
Datasheet
AD9398 on Analog.com
The AD9398 is not recommended for new designs. I recommend the ADV7611 even with its 3.3V digital outputs. IF you really want to use the AD9398 I can get you a reference schematic however support for the part maybe lacking due to its age and people have moved on. We currently have full support from the ADV7611
Hi,
Please note AD9398 is not recommended for new designs and has not been recommended for new designs in quite a while.
But most of our receivers such as ADV7610,ADV7611,ADV7612, ADV7619 ,ADV7625,ADV7604 can support 24 digital bus.But most of them can output high voltage as 2.4V
So kindly use level shifter accordingly.
Thanks,
Poornima
Hi
thanks for reply.
is it possible please to let me have part number of level shifter you recommend to be used for RGB and with AD7611?
Also any design reference schematic.
thanks
Thanks for your reply,
Understood and will take your advice.
Hi,
Could you please check with other community about level shifter (for example - (+) Interface and Isolation - EngineerZone (analog.com) Please check frequent level shifter the customer used at their end) since i am not aware about that. Sorry.
Thanks,
Poornima