Post Go back to editing

About the I2P settings of the ADV7280A.

Category: Hardware

I would like to use the I2P function of the ADV7280A to convert an input signal in NTSC (480i) video format.
We would like to convert the input signal in NTSC (480i) video format to a progressive (480p) signal and output it in 8-bit ITU-R BT.656 YCrCb 4:2:2.

A test pattern (color bar) input in NTSC (480i) video format to the ADV7280A is converted to progressive using the I2P function.
The converted signal is converted to progressive.
The converted signal was encoded in 480p30 video format.
Upon checking the encoded signal, we found that the color bar was only displayed in the upper half of the image (see attached figure).

Do you have any ideas about the cause of this problem?
The register is set as follows.

--------------

addr data

0x0F 0x00
0x52 0xCD
0x00 0x00
0x0E 0x80
0x9C 0x00
0x9C 0xFF
0x0E 0x00
0x80 0x51
0x81 0x51
0x82 0x68
0x17 0x41
0x03 0x0C
0x04 0x07
0x13 0x00
0x1D 0x40
0xFD 0x84
0x41 0x80
0x5B 0x00

--------------

attached figure↓

Parents
  • Hi,

     Could you please ensure such issue in free run by using following register configuration values and let us know the result. 

      In this mode the ADV728x ignore the analog video input and outputs a color bars test pattern. If the issue is not present in free run then we can came to know the issue is with the analog video source or the Analog Front End of the ADV728x

     Also make sure with crystal / oscillator is outputting 28.63636MHz.

    :Free-run, Color Bars 480p YPrPb Out:
    delay 10 ;
    42 0F 00 ; Exit Power Down Mode [ADV7280 writes begin]
    42 00 07 ; ADI Required Write
    42 0C 37 ; Force Free run mode
    42 02 54 ; Force standard to NTSC-M
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable INTRQ output driver
    42 17 41 ; Enable SH1
    42 1D 40 ; Enable LLC output driver
    42 52 CD ; ADI Required Write
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280 VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280 writes finished]

      

    Thanks,

    Poornima

  • Thank you for your prompt response.

    I have set the ADV7280A to the following register.

    ---------------------------------------------------------------------------------------------------

    42 0F 00 ; Exit Power Down Mode [ADV7280 writes begin]
    42 00 07 ; ADI Required Write
    42 0C 37 ; Force Free run mode
    42 02 54 ; Force standard to NTSC-M
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable INTRQ output driver
    42 17 41 ; Enable SH1
    42 1D 40 ; Enable LLC output driver
    42 52 CD ; ADI Required Write
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280 VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280 writes finished]

    ---------------------------------------------------------------------------------------------------

    The encoded video was captured.
    The color bar was only displayed in the upper half of the video (see attached figure).
    The encoding was done in 480p30 video format.

    The output frequency of crystal was 28.63636 MHz.

      see attached figure

  • Hi,

       FreeRun should work. Could you please crosscheck your schematics with reference one.

       Also Please refer this FAQ How Does the Free-run Mode Work in the ADV728x Devices ?

       Also let us know, Are you using any other chip other than ADV7280A to get encoded output?

    Thanks,

    Poornima

  • Thank you for your prompt response.

    Also see this FAQ How does the free-run mode of the ADV728x device work?
     We measured the following values for HS, VS, and CLK(LLC) on the ADV7280A.(Free-run, Color Bars 480p YPrPb Out
     HS: 15.73kHz
     VS: 29.97Hz
     CLK: 27MHz

    Also, can you tell me if you are using a chip other than the ADV7280A to get the encoded output?
     We are using.
     The ADV7280A output (HS, VS, CLK, Data[7:0]) is input to a SoC with Video codec function.
     The signal input from the ADV7280A is encoded by the SoC.

    Thanks.

  • Hi,

       Could you please check the HS, VS, and CLK(LLC) values from ADV7280A for 480P60 in free run mode and compare such values with below referred image and let us know the result to segrate the issue.

        

    Thanks,

    Poornima

  • Hi,

    For reference, could you please tell me what register settings to use to set the 480P60 free-run mode?

    Thanks.

  • Hi,

      Could you please this entire scrpit for ":Free-run, Color Bars 480p YPrPb Out:" and compare the "HS, VS, and CLK(LLC)" values with above attached image for validating the part.

      Also Please check without I2P whether you are getting the same display problem at the output.

       Generally, "A full frame is comprised of an even and an odd field so if we are not converting the interlaced images properly into a progressive display then we might have chance to get such display with zero half field.

       Kindly note that ADV7280A will not transmit a half a field of Zeros. So Please ensure with your SoC side.

    Thanks,

    Poornima

  • Hi,

    I have decoded Video timing reference codes (F,V,H) in FPGA from video signals converted by I2P function.
    During the period when the V bit of the timing reference signals (TRS) was high, the H bit remained low.
    Why is this?
    Please see the attached image for reference.
    ext_trsdec_hb_n: TRS H bit
    ext_trsdec_vb_n: TRS V bit
    ext_trsdec_fld_n: TRS F bit

    The ADV7280A register settings are as follows.

    ---------------------------------------------------------------------------------------------------

    42 0F 00 ; Exit Power Down Mode [ADV7280 writes begin]
    42 00 07 ; ADI Required Write
    42 0C 37 ; Force Free run mode
    42 02 54 ; Force standard to NTSC-M
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable INTRQ output driver
    42 17 41 ; Enable SH1
    42 1D 40 ; Enable LLC output driver
    42 52 CD ; ADI Required Write
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280 VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280 writes finished]

    ---------------------------------------------------------------------------------------------------

Reply
  • Hi,

    I have decoded Video timing reference codes (F,V,H) in FPGA from video signals converted by I2P function.
    During the period when the V bit of the timing reference signals (TRS) was high, the H bit remained low.
    Why is this?
    Please see the attached image for reference.
    ext_trsdec_hb_n: TRS H bit
    ext_trsdec_vb_n: TRS V bit
    ext_trsdec_fld_n: TRS F bit

    The ADV7280A register settings are as follows.

    ---------------------------------------------------------------------------------------------------

    42 0F 00 ; Exit Power Down Mode [ADV7280 writes begin]
    42 00 07 ; ADI Required Write
    42 0C 37 ; Force Free run mode
    42 02 54 ; Force standard to NTSC-M
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable INTRQ output driver
    42 17 41 ; Enable SH1
    42 1D 40 ; Enable LLC output driver
    42 52 CD ; ADI Required Write
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280 VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280 writes finished]

    ---------------------------------------------------------------------------------------------------

Children