Post Go back to editing

Differential receiver setup?

Category: Hardware
Product Number: AD8120, AD8122, AD8123

I have a camera that outputs 1920x1080p via differential component video using a ADV7123/AD8133 combo.  I need to build a board for receiving this differential component video up to 300 meters away over UTP.  I also need the ability to digitally control the line delay.  The AD8120 seems perfect for handling that, but what differential receiver should be used with it?  CN-0275 shows the AD8122 with the AD8120, but the datasheet for the AD8120 shows a reference design using the AD8123.  Which better and why?  This will always be using UTP, never coax.  The run length will vary from setup to setup from 50 meters to 300 meters.  One board has to work with all configurations.  What is the recommended way to go to meet my requirements?

Parents
  • FormerMember
    FormerMember
on Feb 7, 2023 10:39 AM
0

I've forwarded this question to the AD8122 experts

  • Thanks... if there is a better solution using any other of the AD chips then I am open to that.  I just need to make sure I can control the line delay from a microcontroller and the signal works up to 300 meters.  I can't change the camera side, but I can do anything on the receiver side.

  • Reply Children
    No Data