Post Go back to editing

Color-bar test pattern broken from ADV7280-M

Category: Hardware
Product Number: ADV7280-M
Software Version: raspberry pi lite bullseye rpi-5.15.y

I have design custom board for raspberry pi board to support analog camera image.

as result i have get broken color-bar test pattern.

Is there any check point to resolve this issue?

Thanks for reply

(1) color-bar test pattern output

(2) used i2c script

* I used "Color Bars 480i MIPI Out" from ADV7280M_Cust-VER.4.1.txt

42 0F 00 ; Exit Power Down Mode
42 0E 00 ; Enter User Sub Map
42 0C 37 ; Force Free-run mode
42 02 54 ; Force standard to NTSC-M
42 14 11 ; Set Free-run pattern to color bars
42 03 4E ; ADI Required Write
42 04 57 ; Power-up INTRQ pin
42 13 00 ; Enable INTRQ output driver
42 17 41 ; select SH1
42 1D C0 ; Tri-State LLC output driver
42 52 CD ; ADI Required Write
42 80 51 ; ADI Required Write
42 81 51 ; ADI Required Write
42 82 68 ; ADI Required Write
42 FE 88 ; Set CSI Map Address
88 DE 02 ; Power up MIPI D-PHY
88 D2 F7 ; ADI Required Write
88 D8 65 ; ADI Required Write
88 E0 09 ; ADI Required Write
88 2C 00 ; ADI Required Write
88 00 00 ; Power up MIPI CSI-2 Tx

(3) schematic



.
[edited by: YigeunLee at 8:04 AM (GMT -5) on 27 Jan 2023]