Post Go back to editing

Please suggest an alternative part for AD724, which is having industrial grade operating temperature.

Thread Summary

The user inquires about an alternative to the AD724 that operates at -40 to 85°C or higher. The support engineer suggests checking the AD723 or AD725, which support industrial grade operating temperatures. Additionally, the ADV739x/ADV734x series can also meet this requirement. Refer to the Selection Table for Video Encoders for more options.
AI Generated Content
Category: Hardware
Product Number: AD724

Is there any alternative part of AD724 which can operate at -40 to 85 degC or more.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.