Post Go back to editing

ADV7401 Front End Filter Circuit using ADA4412-3

Category: Hardware
Product Number: ADV7401

Hi,

We are designing a Video interface board with STANAG3350 input & output. ADV7401 is selected as STANAG3350 video decoder IC. The board will receive STANAG3350 as differential analog signal. Video differential receiver IC AD8145 (+-5V supply) is used to convert to single ended analog signal. This single ended signal is interfaced to Video filter IC ADA4412-3 (+5V single supply with output DC offset set at 0.6V). The output of  ADA4412-3 is connected to AIN pins of ADV7401 directly to convert to RGB pixel bus data which is inerfaced to on board FPGA.

STANAG3350 --> AD8145 (+-5V) --> ADA4412-3 (+5V) --> ADV7401 --> FPGA is the flow.

Please confirm whether the flow of interconnection is ok to proceed. Give feedback if any issue in interfacing like this.

Regards

Hafiz Haja

Parents Reply Children
No Data