Category: Hardware
Product Number: ADV7619&ADV7511
Hi,teams
I connected only the video data line, but I need audio data, so I'm considering supporting only S/PDIF.
Will S/PDIF work if I connect the following signals?
●ADV7619
Required pins: 5 pins AD0-4. No need for MCLK?
See p9 block diagram and p65 in the following materials
https://www.analog.com/media/en/technical-documentation/user-guides/UG-237.pdf
●ADV7511
Required pins: 2 pins, S/PDIF and MCLK.
See p11 block diagram and p15 Figure 4 in the following materials
https://www.analog.com/media/en/technical-documentation/user-guides/ADV7511_Hardware_Users_Guide.pdf
Best Regard.