Hi,teams
I want to output 2 HDMI input 4k30p using ADV8005.
The environment is as follows
HDMI Input(3840x2160p30)
HDMI output(3840x2160p30) x 2
The register settings are as shown in the text below.
The RX and TX cores are connected.
When set as shown, different frequency clocks are output and the waveform of the data lane is also constant. (Is this a test waveform?).
I have confirmed that the ADV8005 is able to recognize the input InfoFrame at this setting.
Are there any other necessary settings?
We have confirmed that the ADV8005 works with 720x480p60 and 1920x1080p60 input/output with almost the same settings except for TX_STERM_DISABLE and registers other than those related to InfoFrame.
Best regards.
maru
0x1A5F 0x00 0x1A61 0x06 0x1AA0 0x13 0x1AA1 0x01 0x1AA4 0x81 0x1AA5 0x81 0x1AFE 0x08 0xE0C0 0xC4 0x1A45 0x00 0x1A46 0xA8 0x1A47 0x00 0x1A48 0xFB 0x1BE0 0x80 0xE869 0x10 0xE881 0x70 0xE660 0x70 0x1A03 0x66 0x1A39 0x01 0x1B88 0x06 0x1B89 0x10 0x1A07 0xE4 0x1B8A 0x06 0xE283 0xFE 0xE289 0x01 0xE28A 0xF3 0xEC83 0x00 0xEC84 0x00 0xEC85 0x00 0xEC86 0x00 0xF483 0x00 0xF484 0x00 0xF485 0x00 0xF486 0x00 0xEC80 0x7F 0xF480 0x7F 0xEC44 0x11 0xF444 0x11 0xEC17 0x02 0xF417 0x02 0x1A87 0x10 0x1A89 0x10 0xEC81 0x88 0xEC82 0x88 0xF481 0x88 0xF482 0x88 0xECEA 0x85 0xF4EA 0x85 0x1A00 0x70 0xEC40 0x82 0xF440 0x82 0xEC41 0x80 0xF441 0x80 0xECAF 0x16 0xF4AF 0x16 0xEC4B 0x80 0xF44B 0x80 0xECE6 0x20 0xF4E6 0x20