Post Go back to editing

ADV7182 Slow To Sync

Thread Summary

The user experienced slow lock times with the ADV7182 on initial power-up, which was resolved by ensuring the input signal was not floating and by forcing the clamps to respond quickly through specific register settings. The engineer also suggested verifying the power-up sequence and the 5ms reset. For free-running mode, the user should configure the registers as per the reference script and use a 28.63636 MHz crystal with ±50ppm accuracy to maintain correct color subcarrier frequency.
AI Generated Content
Category: Hardware
Product Number: ADV7182

Hi, 

A circuit I designed uses the ADV7182 application circuit as set out in the datasheet.

I've noticed that on first power-up, the chip is very slow to achieve lock with any known good video signals - up to several minutes.

I've checked the clock frequency and tried driving it with multiple sources, but the problem persists.

Once the circuit has been running for a few minutes it locks to any video signal immediately, no problem: there's only an issue in the first few minutes after powering-up.

Enabling "fast lock" as described in the application note has no effect.

Any ideas on what would be causing this are greatly appreciated.