Post Go back to editing

ADV7182 Slow To Sync

Thread Summary

The user experienced slow lock times with the ADV7182 on initial power-up, which was resolved by ensuring the input signal was not floating and by forcing the clamps to respond quickly through specific register settings. The engineer also suggested verifying the power-up sequence and the 5ms reset. For free-running mode, the user should configure the registers as per the reference script and use a 28.63636 MHz crystal with ±50ppm accuracy to maintain correct color subcarrier frequency.
AI Generated Content
Category: Hardware
Product Number: ADV7182

Hi, 

A circuit I designed uses the ADV7182 application circuit as set out in the datasheet.

I've noticed that on first power-up, the chip is very slow to achieve lock with any known good video signals - up to several minutes.

I've checked the clock frequency and tried driving it with multiple sources, but the problem persists.

Once the circuit has been running for a few minutes it locks to any video signal immediately, no problem: there's only an issue in the first few minutes after powering-up.

Enabling "fast lock" as described in the application note has no effect.

Any ideas on what would be causing this are greatly appreciated.

Parents
  • Hi,

       Please ensure whether you are following the order given in the fast switch script.

       Also note that some functionality (like Macrovision) doesn't work in fast switch mode.

       Kindly ensure with below expert suggestion,

         For some reason the input signal on your board is floating or leaking to a supply instead of ground which often happens.

         After the AC coupling capacitor, the signal can float, the internal clamps turn on and pull the signal to the correct level. If there was large leakage on the board to a supply voltage, it could be outside the clamping range ( Too high) and the clamps may take time to turn on and clamp the signal.

         As an experiment to prove this if you add a large resistor few MOhm to ground from the Ain pin, this will pull it to ground. That is only an experiment to prove the point.

         For register settings, if you add the following writes to your script, it may help.

    Please add just after switching or connecting new input.

    42 0E 80

    42 9c 00

    42 9c FF

    42 0E 00

      This forces the clamps to respond very quickly.

    Also the power-up sequence described in the datasheet is the most conservative / correct way of powering up the ADV7182. Care must be taken to ensure that a 1.8V supply does not go higher than the 3.3V supply during power-up.

    Also the 5ms reset after power-up is required.

    Thanks,

    Poornima

  • Yes that seems to have solved the problem, thanks!

    Is there also any way to adjust the frequency in free-running mode. It tends to run a bit too fast, even though the input crystal frequency is correct, which means the colour subcarrier is off.

    Thanks

  • Hi,

      Could you please configure the register as like reference script configuration and let us know the result. Free run related configuration been available at 8484.ADV7182CUST-VER.5.0.txt.zip 

       Please note the device was qualified with a '28.63636MHz +-50ppm', So this is all we can state on the data sheet Unless a 28.63636 MHz crystal with a +/-50ppm accuracy is used, then only the ADV7182/ADV728x will not be able to lock to the color sub-carrier frequency burst of incoming analog video . 

    Thanks,

    Poornima

Reply
  • Hi,

      Could you please configure the register as like reference script configuration and let us know the result. Free run related configuration been available at 8484.ADV7182CUST-VER.5.0.txt.zip 

       Please note the device was qualified with a '28.63636MHz +-50ppm', So this is all we can state on the data sheet Unless a 28.63636 MHz crystal with a +/-50ppm accuracy is used, then only the ADV7182/ADV728x will not be able to lock to the color sub-carrier frequency burst of incoming analog video . 

    Thanks,

    Poornima

Children
No Data