Post Go back to editing

ADV7282AM no image

Category: Hardware
Product Number: ADV7282AM

Hello!

We are trying to get ADV7282AM evaluation board going. We are using DVP Eval software and ADV7282M_CUST scripts to enable colorbar test pattern on the board, however when we try to receive this signal on the raspberry pi 4 there is none. We see that there is a signal on D0N and D0P lanes and something that seems like DC offset on clock lanes (we have 200 MHz oscilloscope, so I assume it is to be expected). We've also noticed that CLKP lane has quite small resistance to ground compared to other lanes - 120 Ohms. Is this normal? Should the board work right away with RPi4 provided there are already drivers and device tree overlays in the kernel? What else could we check?

Parents Reply Children
No Data