Post Go back to editing

AD725 input crystal frequency options

Thread Summary

The user asks if the AD725 can accept 3.3V crystal signals for 4FSC, particularly for NTSC and PAL. The final answer confirms that a 3.3V oscillator should work as the Vhi_min is 2V. The user is advised to use a 10k pull-up resistor to 3.3V for the OE pin to ensure the oscillator output is enabled. The AD725 evaluation board schematic is referenced for a similar mechanical switch setup, and the use of MEMS oscillators is discouraged due to potential jitter issues.
AI Generated Content
Category: Hardware
Product Number: AD725

Hello

I found that AD725 requires TTL levels for 4FSC but I could not find NTSC crystal which is 5v! so I thought will a 3.3v crystal work fine??

as seen in my picture, the circuit is simple. I have a SP3T switch (or any mechanism) that feeds 0v for choosing PAL, 3,3v for NTSC or just another throw for auto detection (circuit not shown here). this circuit needs more tuning but you get the idea.

I really need very easy and stable solution which doesn't require tuning...

so can AD725 accept 3.3v crystal signals?

what crystals do you suggest? I need some part numbers please since finding them is very hard now.

thanks

Parents Reply
  • hello

    what does "weak pulldown" even mean? I will pull it up to 3.3v using 10k or similar for sure, that is when I want it to be active. but when not active I pull it down to 0v using 10k as seen in my picture above. please check.

    lead time is ok for now since first step is making a test board.

    I am still waiting answers to other questions I posted in this section though.

Children
  • FormerMember
    FormerMember on Nov 9, 2022 10:31 AM in reply to VEGETA
    0

    To me a weak pull resistor is >= 100k,  medium pull is ~10-22k and strong pull is <=2K.. Some devices have weak pull resistors on their inputs so the inputs are not floating which can cause problems.  This OE has a weak pull down to turn off the output when OE is not connected to anything.  If you add a 10K pullup to the pin then the pin will have 3.3V * (100/(100+10) = 3V which is greater then Vih_min turning on the output.

  • hello

    so you recommend putting 10k or similar? in my circuit above, I will feed 3.3v directly via analog switch without any pull-up resistors... but without the switch being active, I will put 10k as pull-down resistor. what do you think?

  • FormerMember
    FormerMember on Nov 9, 2022 1:36 PM in reply to VEGETA
    +1

    You can pull directly to 3.3V via the switch.  The 10k pull-down will just go in parallel with the internal 100k pull down.  Not a problem.