Post Go back to editing

AD725 input crystal frequency options

Thread Summary

The user asks if the AD725 can accept 3.3V crystal signals for 4FSC, particularly for NTSC and PAL. The final answer confirms that a 3.3V oscillator should work as the Vhi_min is 2V. The user is advised to use a 10k pull-up resistor to 3.3V for the OE pin to ensure the oscillator output is enabled. The AD725 evaluation board schematic is referenced for a similar mechanical switch setup, and the use of MEMS oscillators is discouraged due to potential jitter issues.
AI Generated Content
Category: Hardware
Product Number: AD725

Hello

I found that AD725 requires TTL levels for 4FSC but I could not find NTSC crystal which is 5v! so I thought will a 3.3v crystal work fine??

as seen in my picture, the circuit is simple. I have a SP3T switch (or any mechanism) that feeds 0v for choosing PAL, 3,3v for NTSC or just another throw for auto detection (circuit not shown here). this circuit needs more tuning but you get the idea.

I really need very easy and stable solution which doesn't require tuning...

so can AD725 accept 3.3v crystal signals?

what crystals do you suggest? I need some part numbers please since finding them is very hard now.

thanks

Parents Reply
  • FormerMember
    FormerMember on Nov 7, 2022 5:53 PM in reply to VEGETA
    0

    According to the AD725 spec Vih_min = 2V with Vcc=+5V.  As stated above, as long as the oscillator output exceeds 2V then it should work.

    I understand the issues with part availability, I face them all the time.  

    It is recommended to use oscillators for the 4FSC input for accuracy and stability issues.  Of course you can design the system anyway you want to.  Personally I'd will not use MEMs because of potential problems.

Children