Post Go back to editing

Composite sync generation on AD724

Thread Summary

The user inquires about generating a composite sync signal without color burst using the AD724. The AD724 can combine HSYNC and VSYNC to create a composite sync signal, and the LUMA output can produce a monochrome signal without color burst without needing FIN. However, if HSYNC and VSYNC inputs lack equalization and serration pulses, the AD724 will not add them to the outputs.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD724

Hello. 

I have a couple of queries regarding AD724.

1) Is it possible to drive only hsync and vsync to AD724 while grounding the RGB inputs to generate a composite sync signal?  

2) Can a composite sync signal without color burst be generated from AD724? The datasheet provides details on providing FIN for color burst but I do not require color burst for the composite sync. 

3) Will the chip support non-standard horizontal timing? The vertical timing (and the number of lines) will be as per NTSC/PAL standard.

Regards,

Akhil A

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.