Post Go back to editing

ADV7282A 28.636MHz Quartz Specification

Category: Datasheet/Specs
Product Number: ADV7282A

How critical is the ESR value for the 28.63636MHz for this product, I am having a few issues with suppliers.

I have various suppliers with different ESR Max values, 35ohms another with 40 ohms and another with 50ohms on their datasheets for this 28.63636MHz quartz in this package size.

How will this affect or not affect my setup.

Also I would like clarification on the total frequency tolerance required for this product, on page 6 of the datasheet is states 

,Frequency Stability ±50 ppm

But then in the table on page 16 it states,

Frequency Calibration (at 25°C) ±20 ppm
Frequency Temperature StabilityTolerance ±50 ppm

Aging per Year ±3 ppm

So does that mean that to get the total tolerance I have 20ppm + 50ppm + aging?

Top Replies

  • FormerMember
    FormerMember
Sep 26, 2022 in reply to JrjH +1 verified

The crystal used to design the original oscillator is attached.  The basic design has changed very little over the years.  See the attached pdf.  This part is hard to get now but readily available from other…

Parents
  • FormerMember
    0 FormerMember
on Sep 13, 2022 11:02 AM

PDF

The original oscillator design was based on a 30 Ohm crystal.  This application note shows that you can change the load capacitors to work with other crystal impedances.  The goal is to get the crystal to spin at the right frequency at room temp.

The 50+-ppm is for total tolerance over temperature.  What is important is the initial frequency at 25C.  For load caps use COG(NPO) caps.  They have the best temperature stability.

Reply
  • FormerMember
    0 FormerMember
on Sep 13, 2022 11:02 AM

PDF

The original oscillator design was based on a 30 Ohm crystal.  This application note shows that you can change the load capacitors to work with other crystal impedances.  The goal is to get the crystal to spin at the right frequency at room temp.

The 50+-ppm is for total tolerance over temperature.  What is important is the initial frequency at 25C.  For load caps use COG(NPO) caps.  They have the best temperature stability.

Children on Sep 26, 2022 9:45 AM in reply to JrjH

The crystal used to design the original oscillator is attached.  The basic design has changed very little over the years.  See the attached pdf.  This part is hard to get now but readily available from other vendors.

PDF

Initial tolerance += 30 ppm

Over temp +- 50 ppm

ageing +- 3ppm/year.

Depending on the circuit this crystal is used to generate the color burst frequency,  Other circuits use it for timing measurement.