Hi,
I have some questions about the MIPI output of the ADV7480.
I asked about the MIPI output state in the start-up/power-down sequence
in the following session.
Q1) When the following MIPI-TXA power down processing is executed, will the MIPI output be LP-11?
I understand that the output does not go from HS to LP state immediately.
CSI-TXA Map
1) 94 31 82
2) 94 1E 00
3) 94 00 84
4) 94 DA 00
5) 94 C1 3B
Q2) In the following MIPI-TXA startup processing,
I think that it will be in the LP state around the 12th step.
Is the LP state in this case LP-11?
CSI-TXA Map
1) 94 00 84
2) 94 00 A4
3) 94 DB 10
4) 94 D6 07
5) 94 C4 0A
6) 94 71 33
7) 94 72 11
8) 94 F0 00
9) 94 31 82
10) 94 1E 40
11) 94 DA 01
12) 94 00 24
13) 94 C1 2B
14) 94 31 80
Best regards.