Post Go back to editing

Adv7280-m with mipi-csi in iMX8MP

Category: Choose a category

Hello Everyone,

We are working on adv7280 -m video decoder with cvbs to mipi-csi interface on i.MX8Mplus. [ 5.10 hardknott].

We have this case below in NXP Support.

https://community.nxp.com/t5/i-MX-Processors/iMX8MP-MIPI-CSI2-Problem-with-ADV7280-and-Camera/m-p/1507469#M193945

We were able to make the [adv7180 1-0020] => [mxc-mipi-csi2.0] this connection.

However, even though everything seems correct, we still don't get any video capture frames from the camera. All the mipi-csi and iMX connections are made, isi connections are correct, and we have introduced the required pins in device tree correctly. You can see the device tree(imx9mp-evk.dts) , adv7180.c(adv driver) and terminal debug print below.

""""adv7180.c """"

// SPDX-License-Identifier: GPL-2.0
/*
 * adv7180.c Analog Devices ADV7180 video decoder driver
 * Copyright (c) 2009 Intel Corporation
 * Copyright (C) 2013 Cogent Embedded, Inc.
 * Copyright (C) 2013 Renesas Solutions Corp.
 */
#include <linux/module.h>
#include <linux/init.h>
#include <linux/errno.h>
#include <linux/kernel.h>
#include <linux/interrupt.h>
#include <linux/i2c.h>
#include <linux/slab.h>
#include <linux/of.h>
#include <linux/gpio/consumer.h>
#include <linux/videodev2.h>
#include <media/v4l2-ioctl.h>
#include <media/v4l2-event.h>
#include <media/v4l2-device.h>
#include <media/v4l2-ctrls.h>
#include <linux/mutex.h>
#include <linux/delay.h>

#define ADV7180_STD_AD_PAL_BG_NTSC_J_SECAM		0x0
#define ADV7180_STD_AD_PAL_BG_NTSC_J_SECAM_PED		0x1
#define ADV7180_STD_AD_PAL_N_NTSC_J_SECAM		0x2
#define ADV7180_STD_AD_PAL_N_NTSC_M_SECAM		0x3
#define ADV7180_STD_NTSC_J				0x4
#define ADV7180_STD_NTSC_M				0x5
#define ADV7180_STD_PAL60				0x6
#define ADV7180_STD_NTSC_443				0x7
#define ADV7180_STD_PAL_BG				0x8
#define ADV7180_STD_PAL_N				0x9
#define ADV7180_STD_PAL_M				0xa
#define ADV7180_STD_PAL_M_PED				0xb
#define ADV7180_STD_PAL_COMB_N				0xc
#define ADV7180_STD_PAL_COMB_N_PED			0xd
#define ADV7180_STD_PAL_SECAM				0xe
#define ADV7180_STD_PAL_SECAM_PED			0xf

#define ADV7180_REG_INPUT_CONTROL			0x0000
#define ADV7180_INPUT_CONTROL_INSEL_MASK		0x0f

#define ADV7182_REG_INPUT_VIDSEL			0x0002
#define ADV7182_REG_INPUT_RESERVED			BIT(2)

#define ADV7180_REG_OUTPUT_CONTROL			0x0003
#define ADV7180_REG_EXTENDED_OUTPUT_CONTROL		0x0004
#define ADV7180_EXTENDED_OUTPUT_CONTROL_NTSCDIS		0xC5

#define ADV7180_REG_AUTODETECT_ENABLE			0x0007
#define ADV7180_AUTODETECT_DEFAULT			0x7f
/* Contrast */
#define ADV7180_REG_CON		0x0008	/*Unsigned */
#define ADV7180_CON_MIN		0
#define ADV7180_CON_DEF		128
#define ADV7180_CON_MAX		255
/* Brightness*/
#define ADV7180_REG_BRI		0x000a	/*Signed */
#define ADV7180_BRI_MIN		-128
#define ADV7180_BRI_DEF		0
#define ADV7180_BRI_MAX		127
/* Hue */
#define ADV7180_REG_HUE		0x000b	/*Signed, inverted */
#define ADV7180_HUE_MIN		-127
#define ADV7180_HUE_DEF		0
#define ADV7180_HUE_MAX		128

#define ADV7180_REG_DEF_VALUE_Y	0x000c
#define ADV7180_DEF_VAL_EN		0x1
#define ADV7180_DEF_VAL_AUTO_EN	0x2
#define ADV7180_REG_CTRL		0x000e
#define ADV7180_CTRL_IRQ_SPACE		0x20

#define ADV7180_REG_PWR_MAN		0x0f
#define ADV7180_PWR_MAN_ON		0x04
#define ADV7180_PWR_MAN_OFF		0x24
#define ADV7180_PWR_MAN_RES		0x80

#define ADV7180_REG_STATUS1		0x0010
#define ADV7180_STATUS1_IN_LOCK		0x01
#define ADV7180_STATUS1_AUTOD_MASK	0x70
#define ADV7180_STATUS1_AUTOD_NTSM_M_J	0x00
#define ADV7180_STATUS1_AUTOD_NTSC_4_43 0x10
#define ADV7180_STATUS1_AUTOD_PAL_M	0x20
#define ADV7180_STATUS1_AUTOD_PAL_60	0x30
#define ADV7180_STATUS1_AUTOD_PAL_B_G	0x40
#define ADV7180_STATUS1_AUTOD_SECAM	0x50
#define ADV7180_STATUS1_AUTOD_PAL_COMB	0x60
#define ADV7180_STATUS1_AUTOD_SECAM_525	0x70

#define ADV7180_REG_IDENT 0x0011
#define ADV7180_ID_7180 0x18

#define ADV7180_REG_STATUS3		0x0013
#define ADV7180_REG_ANALOG_CLAMP_CTL	0x0014
#define ADV7180_REG_SHAP_FILTER_CTL_1	0x0017
#define ADV7180_REG_CTRL_2		0x001d
#define ADV7180_REG_VSYNC_FIELD_CTL_1	0x0031
#define ADV7180_VSYNC_FIELD_CTL_1_NEWAV 0x12
#define ADV7180_REG_MANUAL_WIN_CTL_1	0x003d
#define ADV7180_REG_MANUAL_WIN_CTL_2	0x003e
#define ADV7180_REG_MANUAL_WIN_CTL_3	0x003f
#define ADV7180_REG_LOCK_CNT		0x0051
#define ADV7180_REG_CVBS_TRIM		0x0052
#define ADV7180_REG_CLAMP_ADJ		0x005a
#define ADV7180_REG_RES_CIR		0x005f
#define ADV7180_REG_DIFF_MODE		0x0060

#define ADV7180_REG_ICONF1		0x2040
#define ADV7180_ICONF1_ACTIVE_LOW	0x01
#define ADV7180_ICONF1_PSYNC_ONLY	0x10
#define ADV7180_ICONF1_ACTIVE_TO_CLR	0xC0
/* Saturation */
#define ADV7180_REG_SD_SAT_CB	0x00e3	/*Unsigned */
#define ADV7180_REG_SD_SAT_CR	0x00e4	/*Unsigned */
#define ADV7180_SAT_MIN		0
#define ADV7180_SAT_DEF		128
#define ADV7180_SAT_MAX		255

#define ADV7180_IRQ1_LOCK	0x01
#define ADV7180_IRQ1_UNLOCK	0x02
#define ADV7180_REG_ISR1	0x2042
#define ADV7180_REG_ICR1	0x2043
#define ADV7180_REG_IMR1	0x2044
#define ADV7180_REG_IMR2	0x2048
#define ADV7180_IRQ3_AD_CHANGE	0x08
#define ADV7180_REG_ISR3	0x204A
#define ADV7180_REG_ICR3	0x204B
#define ADV7180_REG_IMR3	0x204C
#define ADV7180_REG_IMR4	0x2050

#define ADV7180_REG_NTSC_V_BIT_END	0x00E6
#define ADV7180_NTSC_V_BIT_END_MANUAL_NVEND	0x4F

#define ADV7180_REG_VPP_SLAVE_ADDR	0xFD
#define ADV7180_REG_CSI_SLAVE_ADDR	0xFE

#define ADV7180_REG_ACE_CTRL1		0x4080
#define ADV7180_REG_ACE_CTRL5		0x4084
#define ADV7180_REG_FLCONTROL		0x40e0
#define ADV7180_FLCONTROL_FL_ENABLE 0x1

#define ADV7180_REG_RST_CLAMP	0x809c
#define ADV7180_REG_AGC_ADJ1	0x80b6
#define ADV7180_REG_AGC_ADJ2	0x80c0

#define ADV7180_CSI_REG_PWRDN	0x00
#define ADV7180_CSI_PWRDN	0x80

#define ADV7180_INPUT_CVBS_AIN1 0x00
#define ADV7180_INPUT_CVBS_AIN2 0x01
#define ADV7180_INPUT_CVBS_AIN3 0x02
#define ADV7180_INPUT_CVBS_AIN4 0x03
#define ADV7180_INPUT_CVBS_AIN5 0x04
#define ADV7180_INPUT_CVBS_AIN6 0x05
#define ADV7180_INPUT_SVIDEO_AIN1_AIN2 0x06
#define ADV7180_INPUT_SVIDEO_AIN3_AIN4 0x07
#define ADV7180_INPUT_SVIDEO_AIN5_AIN6 0x08
#define ADV7180_INPUT_YPRPB_AIN1_AIN2_AIN3 0x09
#define ADV7180_INPUT_YPRPB_AIN4_AIN5_AIN6 0x0a

#define ADV7182_INPUT_CVBS_AIN1 0x00
#define ADV7182_INPUT_CVBS_AIN2 0x01
#define ADV7182_INPUT_CVBS_AIN3 0x02
#define ADV7182_INPUT_CVBS_AIN4 0x03
#define ADV7182_INPUT_CVBS_AIN5 0x04
#define ADV7182_INPUT_CVBS_AIN6 0x05
#define ADV7182_INPUT_CVBS_AIN7 0x06
#define ADV7182_INPUT_CVBS_AIN8 0x07
#define ADV7182_INPUT_SVIDEO_AIN1_AIN2 0x08
#define ADV7182_INPUT_SVIDEO_AIN3_AIN4 0x09
#define ADV7182_INPUT_SVIDEO_AIN5_AIN6 0x0a
#define ADV7182_INPUT_SVIDEO_AIN7_AIN8 0x0b
#define ADV7182_INPUT_YPRPB_AIN1_AIN2_AIN3 0x0c
#define ADV7182_INPUT_YPRPB_AIN4_AIN5_AIN6 0x0d
#define ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2 0x0e
#define ADV7182_INPUT_DIFF_CVBS_AIN3_AIN4 0x0f
#define ADV7182_INPUT_DIFF_CVBS_AIN5_AIN6 0x10
#define ADV7182_INPUT_DIFF_CVBS_AIN7_AIN8 0x11

#define ADV7180_DEFAULT_CSI_I2C_ADDR 0x44
#define ADV7180_DEFAULT_VPP_I2C_ADDR 0x42

#define V4L2_CID_ADV_FAST_SWITCH	(V4L2_CID_USER_ADV7180_BASE + 0x00)

/* Initial number of frames to skip to avoid possible garbage */
#define ADV7180_NUM_OF_SKIP_FRAMES       2

struct adv7180_state;

#define ADV7180_FLAG_RESET_POWERED	BIT(0)
#define ADV7180_FLAG_V2			BIT(1)
#define ADV7180_FLAG_MIPI_CSI2		BIT(2)
#define ADV7180_FLAG_I2P		BIT(3)

struct adv7180_chip_info {
	unsigned int flags;
	unsigned int valid_input_mask;
	int (*set_std)(struct adv7180_state *st, unsigned int std);
	int (*select_input)(struct adv7180_state *st, unsigned int input);
	int (*init)(struct adv7180_state *state);
};

struct adv7180_state {
	struct v4l2_ctrl_handler ctrl_hdl;
	struct v4l2_subdev	sd;
	struct media_pad	pad;
	struct mutex		mutex; /* mutual excl. when accessing chip */
	int			irq;
	struct gpio_desc	*pwdn_gpio;
	struct gpio_desc	*rst_gpio;
	v4l2_std_id		curr_norm;
	bool			powered;
	bool			streaming;
	u8			input;

	struct i2c_client	*client;
	unsigned int		register_page;
	struct i2c_client	*csi_client;
	struct i2c_client	*vpp_client;
	const struct adv7180_chip_info *chip_info;
	enum v4l2_field		field;
	bool			force_bt656_4;
};
#define to_adv7180_sd(_ctrl) (&container_of(_ctrl->handler,		\
					    struct adv7180_state,	\
					    ctrl_hdl)->sd)

static int adv7180_select_page(struct adv7180_state *state, unsigned int page)
{
	if (state->register_page != page) {
		i2c_smbus_write_byte_data(state->client, ADV7180_REG_CTRL,
			page);
		state->register_page = page;
	}
	printk("ADV7180 Status : Girdi 1\n");
	return 0;
}

static int adv7180_write(struct adv7180_state *state, unsigned int reg,
	unsigned int value)
{
	lockdep_assert_held(&state->mutex);
	adv7180_select_page(state, reg >> 8);
	printk("ADV7180 Status : Girdi 2\n");
	return i2c_smbus_write_byte_data(state->client, reg & 0xff, value);
}

static int adv7180_read(struct adv7180_state *state, unsigned int reg)
{
	lockdep_assert_held(&state->mutex);
	adv7180_select_page(state, reg >> 8);
	printk("ADV7180 Status : Girdi 3\n");
	return i2c_smbus_read_byte_data(state->client, reg & 0xff);
}

static int adv7180_csi_write(struct adv7180_state *state, unsigned int reg,
	unsigned int value)
{
	printk("ADV7180 Status : Girdi 4\n");
	return i2c_smbus_write_byte_data(state->csi_client, reg, value);
}

static int adv7180_set_video_standard(struct adv7180_state *state,
	unsigned int std)
{
	printk("ADV7180 Status : Girdi 5\n");
	return state->chip_info->set_std(state, std);
}

static int adv7180_vpp_write(struct adv7180_state *state, unsigned int reg,
	unsigned int value)
{
	printk("ADV7180 Status : Girdi 6\n");
	return i2c_smbus_write_byte_data(state->vpp_client, reg, value);
}

static v4l2_std_id adv7180_std_to_v4l2(u8 status1)
{
	printk("ADV7180 Status v4l2_std_id adv7180_std_to_v4l2: GIRDI n");
	/* in case V4L2_IN_ST_NO_SIGNAL */
	if (!(status1 & ADV7180_STATUS1_IN_LOCK))
	{
		printk("ADV7180 Status : NO Signal - V4L2_STD_UNKNOWN\n");
		return V4L2_STD_UNKNOWN;
	}

	switch (status1 & ADV7180_STATUS1_AUTOD_MASK) {
	case ADV7180_STATUS1_AUTOD_NTSM_M_J:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_NTSM_M_J\n");
		return V4L2_STD_NTSC;
	case ADV7180_STATUS1_AUTOD_NTSC_4_43:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_NTSC_4_43\n");
		return V4L2_STD_NTSC_443;
	case ADV7180_STATUS1_AUTOD_PAL_M:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_PAL_M\n");
		return V4L2_STD_PAL_M;
	case ADV7180_STATUS1_AUTOD_PAL_60:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_PAL_60\n");
		return V4L2_STD_PAL_60;
	case ADV7180_STATUS1_AUTOD_PAL_B_G:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_PAL_B_G\n");
		return V4L2_STD_PAL;
	case ADV7180_STATUS1_AUTOD_SECAM:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_SECAM\n");
		return V4L2_STD_SECAM;
	case ADV7180_STATUS1_AUTOD_PAL_COMB:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_PAL_COMB\n");
		return V4L2_STD_PAL_Nc | V4L2_STD_PAL_N;
		printk("ADV7180 Status : NO Signal - V4L2_STD_PAL_N\n");
	case ADV7180_STATUS1_AUTOD_SECAM_525:
		printk("ADV7180 Status : NO Signal - ADV7180_STATUS1_AUTOD_SECAM_525\n");
		return V4L2_STD_SECAM;
	default:
		{	
		printk("ADV7180 Status : V4L2_STD_UNKNOWN\n");
		return V4L2_STD_UNKNOWN;
		}	
	}
}

static int v4l2_std_to_adv7180(v4l2_std_id std)
{
	printk("ADV7180 Status : Girdi 7\n");
	if (std == V4L2_STD_PAL_60)
		return ADV7180_STD_PAL60;
	if (std == V4L2_STD_NTSC_443)
		return ADV7180_STD_NTSC_443;
	if (std == V4L2_STD_PAL_N)
		return ADV7180_STD_PAL_N;
	if (std == V4L2_STD_PAL_M)
		return ADV7180_STD_PAL_M;
	if (std == V4L2_STD_PAL_Nc)
		return ADV7180_STD_PAL_COMB_N;

	if (std & V4L2_STD_PAL)
		return ADV7180_STD_PAL_BG;
	if (std & V4L2_STD_NTSC)
		return ADV7180_STD_NTSC_M;
	if (std & V4L2_STD_SECAM)
		return ADV7180_STD_PAL_SECAM;

	return -EINVAL;
}

static u32 adv7180_status_to_v4l2(u8 status1)
{
	printk("ADV7180 Status : Girdi 8\n");
	if (!(status1 & ADV7180_STATUS1_IN_LOCK))
	{
		printk("ADV7180 Status : NO Signal\n");
		return V4L2_IN_ST_NO_SIGNAL;
	}
	printk("ADV7180 Status : Signal !\n");
	return 0;
}

static int __adv7180_status(struct adv7180_state *state, u32 *status,
			    v4l2_std_id *std)
{
	printk("ADV7180 Status : Girdi 9\n");
	int status1 = adv7180_read(state, ADV7180_REG_STATUS1);

	if (status1 < 0)
		return status1;

	if (status)
		*status = adv7180_status_to_v4l2(status1);
	if (std)
		*std = adv7180_std_to_v4l2(status1);

	return 0;
}

static inline struct adv7180_state *to_state(struct v4l2_subdev *sd)
{
	printk("ADV7180 Status : Girdi 10\n");
	return container_of(sd, struct adv7180_state, sd);
}

static int adv7180_querystd(struct v4l2_subdev *sd, v4l2_std_id *std)
{
	printk("ADV7180 Status : Girdi 11\n");
	struct adv7180_state *state = to_state(sd);
	int err = mutex_lock_interruptible(&state->mutex);
	if (err)
		return err;

	if (state->streaming) {
		err = -EBUSY;
		goto unlock;
	}

	err = adv7180_set_video_standard(state,
			ADV7180_STD_AD_PAL_BG_NTSC_J_SECAM);
	if (err)
		goto unlock;

	msleep(100);
	__adv7180_status(state, NULL, std);

	err = v4l2_std_to_adv7180(state->curr_norm);
	if (err < 0)
		goto unlock;

	err = adv7180_set_video_standard(state, err);

unlock:
	mutex_unlock(&state->mutex);
	return err;
}

static int adv7180_s_routing(struct v4l2_subdev *sd, u32 input,
			     u32 output, u32 config)
{
	printk("ADV7180 Status : Girdi 12\n");
	struct adv7180_state *state = to_state(sd);
	int ret = mutex_lock_interruptible(&state->mutex);

	if (ret)
		return ret;

	if (input > 31 || !(BIT(input) & state->chip_info->valid_input_mask)) {
		ret = -EINVAL;
		goto out;
	}

	ret = state->chip_info->select_input(state, input);

	if (ret == 0)
		state->input = input;
out:
	mutex_unlock(&state->mutex);
	return ret;
}

static int adv7180_g_input_status(struct v4l2_subdev *sd, u32 *status)
{
	printk("ADV7180 Status : Girdi 13\n");
	struct adv7180_state *state = to_state(sd);
	int ret = mutex_lock_interruptible(&state->mutex);
	if (ret)
		return ret;

	ret = __adv7180_status(state, status, NULL);
	mutex_unlock(&state->mutex);
	return ret;
}

static int adv7180_program_std(struct adv7180_state *state)
{
	printk("ADV7180 Status : Girdi 14\n");
	int ret;

	ret = v4l2_std_to_adv7180(state->curr_norm);
	if (ret < 0)
		return ret;

	ret = adv7180_set_video_standard(state, ret);
	if (ret < 0)
		return ret;
	return 0;
}

static int adv7180_s_std(struct v4l2_subdev *sd, v4l2_std_id std)
{
	printk("ADV7180 Status : Girdi 15\n");
	struct adv7180_state *state = to_state(sd);
	int ret = mutex_lock_interruptible(&state->mutex);

	if (ret)
		return ret;

	/* Make sure we can support this std */
	ret = v4l2_std_to_adv7180(std);
	if (ret < 0)
		goto out;

	state->curr_norm = std;

	ret = adv7180_program_std(state);
out:
	mutex_unlock(&state->mutex);
	return ret;
}

static int adv7180_g_std(struct v4l2_subdev *sd, v4l2_std_id *norm)
{
	printk("ADV7180 Status : Girdi 16\n");
	struct adv7180_state *state = to_state(sd);

	*norm = state->curr_norm;

	return 0;
}

static int adv7180_g_frame_interval(struct v4l2_subdev *sd,
				    struct v4l2_subdev_frame_interval *fi)
{
	printk("ADV7180 Status : Girdi 17\n");
	struct adv7180_state *state = to_state(sd);

	if (state->curr_norm & V4L2_STD_525_60) {
		fi->interval.numerator = 1001;
		fi->interval.denominator = 30000;
	} else {
		fi->interval.numerator = 1;
		fi->interval.denominator = 25;
	}

	return 0;
}

static void adv7180_set_power_pin(struct adv7180_state *state, bool on)
{
	printk("ADV7180 Status : Girdi 18\n");
	if (!state->pwdn_gpio)
		return;

	if (on) {
		gpiod_set_value_cansleep(state->pwdn_gpio, 0);
		usleep_range(5000, 10000);
	} else {
		gpiod_set_value_cansleep(state->pwdn_gpio, 1);
	}
}

static void adv7180_set_reset_pin(struct adv7180_state *state, bool on)
{
	if (!state->rst_gpio)
		return;

	if (on) {
		gpiod_set_value_cansleep(state->rst_gpio, 1);
	} else {
		gpiod_set_value_cansleep(state->rst_gpio, 0);
		usleep_range(5000, 10000);
	}
}

static int adv7180_set_power(struct adv7180_state *state, bool on)
{
	printk("ADV7180 Status : Girdi 19\n");
	u8 val;
	int ret;

	if (on)
		val = ADV7180_PWR_MAN_ON;
	else
		val = ADV7180_PWR_MAN_OFF;

	ret = adv7180_write(state, ADV7180_REG_PWR_MAN, val);
	if (ret)
		return ret;

	if (state->chip_info->flags & ADV7180_FLAG_MIPI_CSI2) {
		if (on) {
			adv7180_csi_write(state, 0xDE, 0x02);
			adv7180_csi_write(state, 0xD2, 0xF7);
			adv7180_csi_write(state, 0xD8, 0x65);
			adv7180_csi_write(state, 0xE0, 0x09);
			adv7180_csi_write(state, 0x2C, 0x00);
			if (state->field == V4L2_FIELD_NONE)
				adv7180_csi_write(state, 0x1D, 0x80);
			adv7180_csi_write(state, 0x00, 0x00);
		} else {
			adv7180_csi_write(state, 0x00, 0x80);
		}
	}

	return 0;
}

static int adv7180_s_power(struct v4l2_subdev *sd, int on)
{
	printk("ADV7180 Status : Girdi 20\n");
	struct adv7180_state *state = to_state(sd);
	int ret;

	ret = mutex_lock_interruptible(&state->mutex);
	if (ret)
		return ret;

	ret = adv7180_set_power(state, on);
	if (ret == 0)
		state->powered = on;

	mutex_unlock(&state->mutex);
	return ret;
}

static int adv7180_s_ctrl(struct v4l2_ctrl *ctrl)
{
	printk("ADV7180 Status : Girdi 21\n");
	struct v4l2_subdev *sd = to_adv7180_sd(ctrl);
	struct adv7180_state *state = to_state(sd);
	int ret = mutex_lock_interruptible(&state->mutex);
	int val;

	if (ret)
		return ret;
	val = ctrl->val;
	switch (ctrl->id) {
	case V4L2_CID_BRIGHTNESS:
		ret = adv7180_write(state, ADV7180_REG_BRI, val);
		break;
	case V4L2_CID_HUE:
		/*Hue is inverted according to HSL chart */
		ret = adv7180_write(state, ADV7180_REG_HUE, -val);
		break;
	case V4L2_CID_CONTRAST:
		ret = adv7180_write(state, ADV7180_REG_CON, val);
		break;
	case V4L2_CID_SATURATION:
		/*
		 *This could be V4L2_CID_BLUE_BALANCE/V4L2_CID_RED_BALANCE
		 *Let's not confuse the user, everybody understands saturation
		 */
		ret = adv7180_write(state, ADV7180_REG_SD_SAT_CB, val);
		if (ret < 0)
			break;
		ret = adv7180_write(state, ADV7180_REG_SD_SAT_CR, val);
		break;
	case V4L2_CID_ADV_FAST_SWITCH:
		if (ctrl->val) {
			/* ADI required write */
			adv7180_write(state, 0x80d9, 0x44);
			adv7180_write(state, ADV7180_REG_FLCONTROL,
				ADV7180_FLCONTROL_FL_ENABLE);
		} else {
			/* ADI required write */
			adv7180_write(state, 0x80d9, 0xc4);
			adv7180_write(state, ADV7180_REG_FLCONTROL, 0x00);
		}
		break;
	default:
		ret = -EINVAL;
	}

	mutex_unlock(&state->mutex);
	return ret;
}

static const struct v4l2_ctrl_ops adv7180_ctrl_ops = {
	.s_ctrl = adv7180_s_ctrl,
};

static const struct v4l2_ctrl_config adv7180_ctrl_fast_switch = {
	.ops = &adv7180_ctrl_ops,
	.id = V4L2_CID_ADV_FAST_SWITCH,
	.name = "Fast Switching",
	.type = V4L2_CTRL_TYPE_BOOLEAN,
	.min = 0,
	.max = 1,
	.step = 1,
};

static int adv7180_init_controls(struct adv7180_state *state)
{
	printk("ADV7180 Status : Girdi 22\n");
	v4l2_ctrl_handler_init(&state->ctrl_hdl, 4);

	v4l2_ctrl_new_std(&state->ctrl_hdl, &adv7180_ctrl_ops,
			  V4L2_CID_BRIGHTNESS, ADV7180_BRI_MIN,
			  ADV7180_BRI_MAX, 1, ADV7180_BRI_DEF);
	v4l2_ctrl_new_std(&state->ctrl_hdl, &adv7180_ctrl_ops,
			  V4L2_CID_CONTRAST, ADV7180_CON_MIN,
			  ADV7180_CON_MAX, 1, ADV7180_CON_DEF);
	v4l2_ctrl_new_std(&state->ctrl_hdl, &adv7180_ctrl_ops,
			  V4L2_CID_SATURATION, ADV7180_SAT_MIN,
			  ADV7180_SAT_MAX, 1, ADV7180_SAT_DEF);
	v4l2_ctrl_new_std(&state->ctrl_hdl, &adv7180_ctrl_ops,
			  V4L2_CID_HUE, ADV7180_HUE_MIN,
			  ADV7180_HUE_MAX, 1, ADV7180_HUE_DEF);
	v4l2_ctrl_new_custom(&state->ctrl_hdl, &adv7180_ctrl_fast_switch, NULL);

	state->sd.ctrl_handler = &state->ctrl_hdl;
	if (state->ctrl_hdl.error) {
		int err = state->ctrl_hdl.error;

		v4l2_ctrl_handler_free(&state->ctrl_hdl);
		return err;
	}
	v4l2_ctrl_handler_setup(&state->ctrl_hdl);

	return 0;
}
static void adv7180_exit_controls(struct adv7180_state *state)
{
	printk("ADV7180 Status : Girdi 23\n");
	v4l2_ctrl_handler_free(&state->ctrl_hdl);
}

static int adv7180_enum_mbus_code(struct v4l2_subdev *sd,
				  struct v4l2_subdev_pad_config *cfg,
				  struct v4l2_subdev_mbus_code_enum *code)
{
	printk("ADV7180 Status : Girdi 24\n");
	if (code->index != 0)
		return -EINVAL;

	code->code = MEDIA_BUS_FMT_UYVY8_2X8;

	return 0;
}

static int adv7180_mbus_fmt(struct v4l2_subdev *sd,
			    struct v4l2_mbus_framefmt *fmt)
{
	printk("ADV7180 Status : Girdi 25\n");
	struct adv7180_state *state = to_state(sd);

	fmt->code = MEDIA_BUS_FMT_UYVY8_2X8;
	fmt->colorspace = V4L2_COLORSPACE_SMPTE170M;
	fmt->width = 720;
	fmt->height = state->curr_norm & V4L2_STD_525_60 ? 480 : 288;

	if (state->field == V4L2_FIELD_ALTERNATE)
		fmt->height /= 2;

	return 0;
}

static int adv7180_set_field_mode(struct adv7180_state *state)
{
	printk("ADV7180 Status : Girdi 26\n");
	if (!(state->chip_info->flags & ADV7180_FLAG_I2P))
		return 0;

	if (state->field == V4L2_FIELD_NONE) {
		if (state->chip_info->flags & ADV7180_FLAG_MIPI_CSI2) {
			adv7180_csi_write(state, 0x01, 0x20);
			adv7180_csi_write(state, 0x02, 0x28);
			adv7180_csi_write(state, 0x03, 0x38);
			adv7180_csi_write(state, 0x04, 0x30);
			adv7180_csi_write(state, 0x05, 0x30);
			adv7180_csi_write(state, 0x06, 0x80);
			adv7180_csi_write(state, 0x07, 0x70);
			adv7180_csi_write(state, 0x08, 0x50);
		}
		adv7180_vpp_write(state, 0xa3, 0x00);
		adv7180_vpp_write(state, 0x5b, 0x00);
		adv7180_vpp_write(state, 0x55, 0x80);
	} else {
		if (state->chip_info->flags & ADV7180_FLAG_MIPI_CSI2) {
			adv7180_csi_write(state, 0x01, 0x18);
			adv7180_csi_write(state, 0x02, 0x18);
			adv7180_csi_write(state, 0x03, 0x30);
			adv7180_csi_write(state, 0x04, 0x20);
			adv7180_csi_write(state, 0x05, 0x28);
			adv7180_csi_write(state, 0x06, 0x40);
			adv7180_csi_write(state, 0x07, 0x58);
			adv7180_csi_write(state, 0x08, 0x30);
		}
		adv7180_vpp_write(state, 0xa3, 0x70);
		adv7180_vpp_write(state, 0x5b, 0x80);
		adv7180_vpp_write(state, 0x55, 0x00);
	}

	return 0;
}

static int adv7180_get_pad_format(struct v4l2_subdev *sd,
				  struct v4l2_subdev_pad_config *cfg,
				  struct v4l2_subdev_format *format)
{
	printk("ADV7180 Status : Girdi 27\n");
	struct adv7180_state *state = to_state(sd);

	if (format->which == V4L2_SUBDEV_FORMAT_TRY) {
		format->format = *v4l2_subdev_get_try_format(sd, cfg, 0);
	} else {
		adv7180_mbus_fmt(sd, &format->format);
		format->format.field = state->field;
	}

	return 0;
}

static int adv7180_set_pad_format(struct v4l2_subdev *sd,
				  struct v4l2_subdev_pad_config *cfg,
				  struct v4l2_subdev_format *format)
{
	printk("ADV7180 Status : Girdi 28\n");
	struct adv7180_state *state = to_state(sd);
	struct v4l2_mbus_framefmt *framefmt;
	int ret;

	switch (format->format.field) {
	case V4L2_FIELD_NONE:
		if (state->chip_info->flags & ADV7180_FLAG_I2P)
			break;
		fallthrough;
	default:
		format->format.field = V4L2_FIELD_ALTERNATE;
		break;
	}

	ret = adv7180_mbus_fmt(sd,  &format->format);

	if (format->which == V4L2_SUBDEV_FORMAT_ACTIVE) {
		if (state->field != format->format.field) {
			state->field = format->format.field;
			adv7180_set_power(state, false);
			adv7180_set_field_mode(state);
			adv7180_set_power(state, true);
		}
	} else {
		framefmt = v4l2_subdev_get_try_format(sd, cfg, 0);
		*framefmt = format->format;
	}

	return ret;
}

static int adv7180_init_cfg(struct v4l2_subdev *sd,
			    struct v4l2_subdev_pad_config *cfg)
{
	printk("ADV7180 Status : Girdi 29\n");
	struct v4l2_subdev_format fmt = {
		.which = cfg ? V4L2_SUBDEV_FORMAT_TRY
			: V4L2_SUBDEV_FORMAT_ACTIVE,
	};

	return adv7180_set_pad_format(sd, cfg, &fmt);
}

static int adv7180_get_mbus_config(struct v4l2_subdev *sd,
				   unsigned int pad,
				   struct v4l2_mbus_config *cfg)
{
	printk("ADV7180 Status : Girdi 30\n");
	struct adv7180_state *state = to_state(sd);

	if (state->chip_info->flags & ADV7180_FLAG_MIPI_CSI2) {
		cfg->type = V4L2_MBUS_CSI2_DPHY;
		cfg->flags = V4L2_MBUS_CSI2_1_LANE |
				V4L2_MBUS_CSI2_CHANNEL_0 |
				V4L2_MBUS_CSI2_CONTINUOUS_CLOCK;
	} else {
		/*
		 * The ADV7180 sensor supports BT.601/656 output modes.
		 * The BT.656 is default and not yet configurable by s/w.
		 */
		cfg->flags = V4L2_MBUS_MASTER | V4L2_MBUS_PCLK_SAMPLE_RISING |
				 V4L2_MBUS_DATA_ACTIVE_HIGH;
		cfg->type = V4L2_MBUS_BT656;
	}

	return 0;
}

static int adv7180_get_skip_frames(struct v4l2_subdev *sd, u32 *frames)
{
	printk("ADV7180 Status : Girdi 31\n");
	*frames = ADV7180_NUM_OF_SKIP_FRAMES;

	return 0;
}

static int adv7180_g_pixelaspect(struct v4l2_subdev *sd, struct v4l2_fract *aspect)
{
	printk("ADV7180 Status : Girdi 32\n");
	struct adv7180_state *state = to_state(sd);

	if (state->curr_norm & V4L2_STD_525_60) {
		aspect->numerator = 11;
		aspect->denominator = 10;
	} else {
		aspect->numerator = 54;
		aspect->denominator = 59;
	}

	return 0;
}

static int adv7180_g_tvnorms(struct v4l2_subdev *sd, v4l2_std_id *norm)
{
	printk("ADV7180 Status : Girdi 33\n");
	*norm = V4L2_STD_ALL;
	return 0;
}

static int adv7180_s_stream(struct v4l2_subdev *sd, int enable)
{
	printk("ADV7180 Status : Girdi 34\n");
	struct adv7180_state *state = to_state(sd);
	int ret;

	/* It's always safe to stop streaming, no need to take the lock */
	if (!enable) {
		printk("ADV7180 Status : Girdi 34 ENABLE IF\n");
		state->streaming = enable;
		return 0;
	}

	/* Must wait until querystd released the lock */
	ret = mutex_lock_interruptible(&state->mutex);
	if (ret)
		return ret;
	printk("ADV7180 Status : Girdi 34 ENABLE RET IF\n");
	state->streaming = enable;
	mutex_unlock(&state->mutex);
	return 0;
}

static int adv7180_subscribe_event(struct v4l2_subdev *sd,
				   struct v4l2_fh *fh,
				   struct v4l2_event_subscription *sub)
{
	printk("ADV7180 Status : Girdi 35\n");
	switch (sub->type) {
	case V4L2_EVENT_SOURCE_CHANGE:
		return v4l2_src_change_event_subdev_subscribe(sd, fh, sub);
	case V4L2_EVENT_CTRL:
		return v4l2_ctrl_subdev_subscribe_event(sd, fh, sub);
	default:
		return -EINVAL;
	}
}

static const struct v4l2_subdev_video_ops adv7180_video_ops = {
	.s_std = adv7180_s_std,
	.g_std = adv7180_g_std,
	.g_frame_interval = adv7180_g_frame_interval,
	.querystd = adv7180_querystd,
	.g_input_status = adv7180_g_input_status,
	.s_routing = adv7180_s_routing,
	.g_pixelaspect = adv7180_g_pixelaspect,
	.g_tvnorms = adv7180_g_tvnorms,
	.s_stream = adv7180_s_stream,
};

static const struct v4l2_subdev_core_ops adv7180_core_ops = {
	.s_power = adv7180_s_power,
	.subscribe_event = adv7180_subscribe_event,
	.unsubscribe_event = v4l2_event_subdev_unsubscribe,
};

static const struct v4l2_subdev_pad_ops adv7180_pad_ops = {
	.init_cfg = adv7180_init_cfg,
	.enum_mbus_code = adv7180_enum_mbus_code,
	.set_fmt = adv7180_set_pad_format,
	.get_fmt = adv7180_get_pad_format,
	.get_mbus_config = adv7180_get_mbus_config,
};

static const struct v4l2_subdev_sensor_ops adv7180_sensor_ops = {
	.g_skip_frames = adv7180_get_skip_frames,
};

static const struct v4l2_subdev_ops adv7180_ops = {
	.core = &adv7180_core_ops,
	.video = &adv7180_video_ops,
	.pad = &adv7180_pad_ops,
	.sensor = &adv7180_sensor_ops,
};


//AZIZ
static int adv7180_link_setup(struct media_entity *entity,
struct media_pad const *local,
struct media_pad const *remote, u32 flags) 
{
	printk("ADV7180 Status : Girdi 36\n");
	return 0;
}

static const struct media_entity_operations adv7180_entity_ops = {
	.link_setup = adv7180_link_setup,
};
//AZIZ

static irqreturn_t adv7180_irq(int irq, void *devid)
{
	printk("ADV7180 Status : Girdi 37\n");
	struct adv7180_state *state = devid;
	u8 isr3;

	mutex_lock(&state->mutex);
	isr3 = adv7180_read(state, ADV7180_REG_ISR3);
	/* clear */
	adv7180_write(state, ADV7180_REG_ICR3, isr3);

	if (isr3 & ADV7180_IRQ3_AD_CHANGE) {
		static const struct v4l2_event src_ch = {
			.type = V4L2_EVENT_SOURCE_CHANGE,
			.u.src_change.changes = V4L2_EVENT_SRC_CH_RESOLUTION,
		};

		v4l2_subdev_notify_event(&state->sd, &src_ch);
	}
	mutex_unlock(&state->mutex);

	return IRQ_HANDLED;
}

static int adv7180_init(struct adv7180_state *state)
{
	printk("ADV7180 Status : Girdi 38\n");
	int ret;

	/* ITU-R BT.656-4 compatible */
	ret = adv7180_write(state, ADV7180_REG_EXTENDED_OUTPUT_CONTROL,
			ADV7180_EXTENDED_OUTPUT_CONTROL_NTSCDIS);
	if (ret < 0)
		return ret;

	/* Manually set V bit end position in NTSC mode */
	return adv7180_write(state, ADV7180_REG_NTSC_V_BIT_END,
					ADV7180_NTSC_V_BIT_END_MANUAL_NVEND);
}

static int adv7180_set_std(struct adv7180_state *state, unsigned int std)
{
	printk("ADV7180 Status : Girdi 39\n");
	return adv7180_write(state, ADV7180_REG_INPUT_CONTROL,
		(std << 4) | state->input);
}

static int adv7180_select_input(struct adv7180_state *state, unsigned int input)
{
	printk("ADV7180 Status : Girdi 40\n");
	int ret;

	ret = adv7180_read(state, ADV7180_REG_INPUT_CONTROL);
	if (ret < 0)
		return ret;

	ret &= ~ADV7180_INPUT_CONTROL_INSEL_MASK;
	ret |= input;
	return adv7180_write(state, ADV7180_REG_INPUT_CONTROL, ret);
}

static int adv7182_init(struct adv7180_state *state)
{
	printk("ADV7180 Status : Girdi 41\n");
	if (state->chip_info->flags & ADV7180_FLAG_MIPI_CSI2)
		adv7180_write(state, ADV7180_REG_CSI_SLAVE_ADDR,
			ADV7180_DEFAULT_CSI_I2C_ADDR << 1);

	if (state->chip_info->flags & ADV7180_FLAG_I2P)
		adv7180_write(state, ADV7180_REG_VPP_SLAVE_ADDR,
			ADV7180_DEFAULT_VPP_I2C_ADDR << 1);

	if (state->chip_info->flags & ADV7180_FLAG_V2) {
		/* ADI recommended writes for improved video quality */
		adv7180_write(state, 0x0080, 0x51);
		adv7180_write(state, 0x0081, 0x51);
		adv7180_write(state, 0x0082, 0x68);
	}

	/* ADI required writes */
	if (state->chip_info->flags & ADV7180_FLAG_MIPI_CSI2) {
		adv7180_write(state, ADV7180_REG_OUTPUT_CONTROL, 0x4e);
		adv7180_write(state, ADV7180_REG_EXTENDED_OUTPUT_CONTROL, 0x57);
		adv7180_write(state, ADV7180_REG_CTRL_2, 0xc0);
	} else {
		if (state->chip_info->flags & ADV7180_FLAG_V2)
			adv7180_write(state,
				      ADV7180_REG_EXTENDED_OUTPUT_CONTROL,
				      0x17);
		else
			adv7180_write(state,
				      ADV7180_REG_EXTENDED_OUTPUT_CONTROL,
				      0x07);
		adv7180_write(state, ADV7180_REG_OUTPUT_CONTROL, 0x0c);
		adv7180_write(state, ADV7180_REG_CTRL_2, 0x40);
	}

	adv7180_write(state, 0x0013, 0x00);

	return 0;
}

static int adv7182_set_std(struct adv7180_state *state, unsigned int std)
{
	/* Failing to set the reserved bit can result in increased video noise */
	return adv7180_write(state, ADV7182_REG_INPUT_VIDSEL,
			     (std << 4) | ADV7182_REG_INPUT_RESERVED);
}

enum adv7182_input_type {
	ADV7182_INPUT_TYPE_CVBS,
	ADV7182_INPUT_TYPE_DIFF_CVBS,
	ADV7182_INPUT_TYPE_SVIDEO,
	ADV7182_INPUT_TYPE_YPBPR,
};

static enum adv7182_input_type adv7182_get_input_type(unsigned int input)
{
	switch (input) {
	case ADV7182_INPUT_CVBS_AIN1:
	case ADV7182_INPUT_CVBS_AIN2:
	case ADV7182_INPUT_CVBS_AIN3:
	case ADV7182_INPUT_CVBS_AIN4:
	case ADV7182_INPUT_CVBS_AIN5:
	case ADV7182_INPUT_CVBS_AIN6:
	case ADV7182_INPUT_CVBS_AIN7:
	case ADV7182_INPUT_CVBS_AIN8:
		return ADV7182_INPUT_TYPE_CVBS;
	case ADV7182_INPUT_SVIDEO_AIN1_AIN2:
	case ADV7182_INPUT_SVIDEO_AIN3_AIN4:
	case ADV7182_INPUT_SVIDEO_AIN5_AIN6:
	case ADV7182_INPUT_SVIDEO_AIN7_AIN8:
		return ADV7182_INPUT_TYPE_SVIDEO;
	case ADV7182_INPUT_YPRPB_AIN1_AIN2_AIN3:
	case ADV7182_INPUT_YPRPB_AIN4_AIN5_AIN6:
		return ADV7182_INPUT_TYPE_YPBPR;
	case ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2:
	case ADV7182_INPUT_DIFF_CVBS_AIN3_AIN4:
	case ADV7182_INPUT_DIFF_CVBS_AIN5_AIN6:
	case ADV7182_INPUT_DIFF_CVBS_AIN7_AIN8:
		return ADV7182_INPUT_TYPE_DIFF_CVBS;
	default: /* Will never happen */
		return 0;
	}
}

/* ADI recommended writes to registers 0x52, 0x53, 0x54 */
static unsigned int adv7182_lbias_settings[][3] = {
	[ADV7182_INPUT_TYPE_CVBS] = { 0xCB, 0x4E, 0x80 },
	[ADV7182_INPUT_TYPE_DIFF_CVBS] = { 0xC0, 0x4E, 0x80 },
	[ADV7182_INPUT_TYPE_SVIDEO] = { 0x0B, 0xCE, 0x80 },
	[ADV7182_INPUT_TYPE_YPBPR] = { 0x0B, 0x4E, 0xC0 },
};

static unsigned int adv7280_lbias_settings[][3] = {
	[ADV7182_INPUT_TYPE_CVBS] = { 0xCD, 0x4E, 0x80 },
	[ADV7182_INPUT_TYPE_DIFF_CVBS] = { 0xC0, 0x4E, 0x80 },
	[ADV7182_INPUT_TYPE_SVIDEO] = { 0x0B, 0xCE, 0x80 },
	[ADV7182_INPUT_TYPE_YPBPR] = { 0x0B, 0x4E, 0xC0 },
};

static int adv7182_select_input(struct adv7180_state *state, unsigned int input)
{
	printk("ADV7180 Status : Girdi 43\n");
	enum adv7182_input_type input_type;
	unsigned int *lbias;
	unsigned int i;
	int ret;

	ret = adv7180_write(state, ADV7180_REG_INPUT_CONTROL, input);
	if (ret)
		return ret;

	/* Reset clamp circuitry - ADI recommended writes */
	adv7180_write(state, ADV7180_REG_RST_CLAMP, 0x00);
	adv7180_write(state, ADV7180_REG_RST_CLAMP, 0xff);

	input_type = adv7182_get_input_type(input);

	switch (input_type) {
	case ADV7182_INPUT_TYPE_CVBS:
	case ADV7182_INPUT_TYPE_DIFF_CVBS:
		/* ADI recommends to use the SH1 filter */
		adv7180_write(state, ADV7180_REG_SHAP_FILTER_CTL_1, 0x41);
		break;
	default:
		adv7180_write(state, ADV7180_REG_SHAP_FILTER_CTL_1, 0x01);
		break;
	}

	if (state->chip_info->flags & ADV7180_FLAG_V2)
		lbias = adv7280_lbias_settings[input_type];
	else
		lbias = adv7182_lbias_settings[input_type];

	for (i = 0; i < ARRAY_SIZE(adv7182_lbias_settings[0]); i++)
		adv7180_write(state, ADV7180_REG_CVBS_TRIM + i, lbias[i]);

	if (input_type == ADV7182_INPUT_TYPE_DIFF_CVBS) {
		/* ADI required writes to make differential CVBS work */
		adv7180_write(state, ADV7180_REG_RES_CIR, 0xa8);
		adv7180_write(state, ADV7180_REG_CLAMP_ADJ, 0x90);
		adv7180_write(state, ADV7180_REG_DIFF_MODE, 0xb0);
		adv7180_write(state, ADV7180_REG_AGC_ADJ1, 0x08);
		adv7180_write(state, ADV7180_REG_AGC_ADJ2, 0xa0);
	} else {
		adv7180_write(state, ADV7180_REG_RES_CIR, 0xf0);
		adv7180_write(state, ADV7180_REG_CLAMP_ADJ, 0xd0);
		adv7180_write(state, ADV7180_REG_DIFF_MODE, 0x10);
		adv7180_write(state, ADV7180_REG_AGC_ADJ1, 0x9c);
		adv7180_write(state, ADV7180_REG_AGC_ADJ2, 0x00);
	}

	return 0;
}

static const struct adv7180_chip_info adv7180_info = {
	.flags = ADV7180_FLAG_RESET_POWERED,
	/* We cannot discriminate between LQFP and 40-pin LFCSP, so accept
	 * all inputs and let the card driver take care of validation
	 */
	.valid_input_mask = BIT(ADV7180_INPUT_CVBS_AIN1) |
		BIT(ADV7180_INPUT_CVBS_AIN2) |
		BIT(ADV7180_INPUT_CVBS_AIN3) |
		BIT(ADV7180_INPUT_CVBS_AIN4) |
		BIT(ADV7180_INPUT_CVBS_AIN5) |
		BIT(ADV7180_INPUT_CVBS_AIN6) |
		BIT(ADV7180_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7180_INPUT_SVIDEO_AIN3_AIN4) |
		BIT(ADV7180_INPUT_SVIDEO_AIN5_AIN6) |
		BIT(ADV7180_INPUT_YPRPB_AIN1_AIN2_AIN3) |
		BIT(ADV7180_INPUT_YPRPB_AIN4_AIN5_AIN6),
	.init = adv7180_init,
	.set_std = adv7180_set_std,
	.select_input = adv7180_select_input,
};

static const struct adv7180_chip_info adv7182_info = {
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN3) |
		BIT(ADV7182_INPUT_CVBS_AIN4) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN3_AIN4) |
		BIT(ADV7182_INPUT_YPRPB_AIN1_AIN2_AIN3) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN3_AIN4),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static const struct adv7180_chip_info adv7280_info = {
	.flags = ADV7180_FLAG_V2 | ADV7180_FLAG_I2P,
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN3) |
		BIT(ADV7182_INPUT_CVBS_AIN4) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN3_AIN4) |
		BIT(ADV7182_INPUT_YPRPB_AIN1_AIN2_AIN3),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static const struct adv7180_chip_info adv7280_m_info = {
	.flags = ADV7180_FLAG_V2 | ADV7180_FLAG_MIPI_CSI2 | ADV7180_FLAG_I2P,
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN3) |
		BIT(ADV7182_INPUT_CVBS_AIN4) |
		BIT(ADV7182_INPUT_CVBS_AIN5) |
		BIT(ADV7182_INPUT_CVBS_AIN6) |
		BIT(ADV7182_INPUT_CVBS_AIN7) |
		BIT(ADV7182_INPUT_CVBS_AIN8) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN3_AIN4) |
		BIT(ADV7182_INPUT_SVIDEO_AIN5_AIN6) |
		BIT(ADV7182_INPUT_SVIDEO_AIN7_AIN8) |
		BIT(ADV7182_INPUT_YPRPB_AIN1_AIN2_AIN3) |
		BIT(ADV7182_INPUT_YPRPB_AIN4_AIN5_AIN6),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static const struct adv7180_chip_info adv7281_info = {
	.flags = ADV7180_FLAG_V2 | ADV7180_FLAG_MIPI_CSI2,
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN7) |
		BIT(ADV7182_INPUT_CVBS_AIN8) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN7_AIN8) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN7_AIN8),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static const struct adv7180_chip_info adv7281_m_info = {
	.flags = ADV7180_FLAG_V2 | ADV7180_FLAG_MIPI_CSI2,
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN3) |
		BIT(ADV7182_INPUT_CVBS_AIN4) |
		BIT(ADV7182_INPUT_CVBS_AIN7) |
		BIT(ADV7182_INPUT_CVBS_AIN8) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN3_AIN4) |
		BIT(ADV7182_INPUT_SVIDEO_AIN7_AIN8) |
		BIT(ADV7182_INPUT_YPRPB_AIN1_AIN2_AIN3) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN3_AIN4) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN7_AIN8),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static const struct adv7180_chip_info adv7281_ma_info = {
	.flags = ADV7180_FLAG_V2 | ADV7180_FLAG_MIPI_CSI2,
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN3) |
		BIT(ADV7182_INPUT_CVBS_AIN4) |
		BIT(ADV7182_INPUT_CVBS_AIN5) |
		BIT(ADV7182_INPUT_CVBS_AIN6) |
		BIT(ADV7182_INPUT_CVBS_AIN7) |
		BIT(ADV7182_INPUT_CVBS_AIN8) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN3_AIN4) |
		BIT(ADV7182_INPUT_SVIDEO_AIN5_AIN6) |
		BIT(ADV7182_INPUT_SVIDEO_AIN7_AIN8) |
		BIT(ADV7182_INPUT_YPRPB_AIN1_AIN2_AIN3) |
		BIT(ADV7182_INPUT_YPRPB_AIN4_AIN5_AIN6) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN3_AIN4) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN5_AIN6) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN7_AIN8),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static const struct adv7180_chip_info adv7282_info = {
	.flags = ADV7180_FLAG_V2 | ADV7180_FLAG_I2P,
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN7) |
		BIT(ADV7182_INPUT_CVBS_AIN8) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN7_AIN8) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN7_AIN8),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static const struct adv7180_chip_info adv7282_m_info = {
	.flags = ADV7180_FLAG_V2 | ADV7180_FLAG_MIPI_CSI2 | ADV7180_FLAG_I2P,
	.valid_input_mask = BIT(ADV7182_INPUT_CVBS_AIN1) |
		BIT(ADV7182_INPUT_CVBS_AIN2) |
		BIT(ADV7182_INPUT_CVBS_AIN3) |
		BIT(ADV7182_INPUT_CVBS_AIN4) |
		BIT(ADV7182_INPUT_CVBS_AIN7) |
		BIT(ADV7182_INPUT_CVBS_AIN8) |
		BIT(ADV7182_INPUT_SVIDEO_AIN1_AIN2) |
		BIT(ADV7182_INPUT_SVIDEO_AIN3_AIN4) |
		BIT(ADV7182_INPUT_SVIDEO_AIN7_AIN8) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN1_AIN2) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN3_AIN4) |
		BIT(ADV7182_INPUT_DIFF_CVBS_AIN7_AIN8),
	.init = adv7182_init,
	.set_std = adv7182_set_std,
	.select_input = adv7182_select_input,
};

static int init_device(struct adv7180_state *state)
{
	printk("ADV7180 Status : Girdi 44\n");
	int ret;

	mutex_lock(&state->mutex);

	adv7180_set_power_pin(state, true);

	adv7180_write(state, ADV7180_REG_PWR_MAN, ADV7180_PWR_MAN_RES);
	usleep_range(5000, 10000);

	ret = state->chip_info->init(state);
	if (ret)
		goto out_unlock;

	ret = adv7180_program_std(state);
	if (ret)
		goto out_unlock;

	adv7180_set_field_mode(state);

	/* register for interrupts */
	if (state->irq > 0) {
		/* config the Interrupt pin to be active low */
		ret = adv7180_write(state, ADV7180_REG_ICONF1,
						ADV7180_ICONF1_ACTIVE_LOW |
						ADV7180_ICONF1_PSYNC_ONLY);
		if (ret < 0)
			goto out_unlock;

		ret = adv7180_write(state, ADV7180_REG_IMR1, 0);
		if (ret < 0)
			goto out_unlock;

		ret = adv7180_write(state, ADV7180_REG_IMR2, 0);
		if (ret < 0)
			goto out_unlock;

		/* enable AD change interrupts interrupts */
		ret = adv7180_write(state, ADV7180_REG_IMR3,
						ADV7180_IRQ3_AD_CHANGE);
		if (ret < 0)
			goto out_unlock;

		ret = adv7180_write(state, ADV7180_REG_IMR4, 0);
		if (ret < 0)
			goto out_unlock;
	}

out_unlock:
	mutex_unlock(&state->mutex);

	return ret;
}

static int adv7180_probe(struct i2c_client *client,
			 const struct i2c_device_id *id)
{
	printk("ADV7180 Status : Girdi 45\n");
	struct adv7180_state *state;
	struct v4l2_subdev *sd;
	int ret;

	/* Check if the adapter supports the needed features */
	if (!i2c_check_functionality(client->adapter, I2C_FUNC_SMBUS_BYTE_DATA))
		return -EIO;

	state = devm_kzalloc(&client->dev, sizeof(*state), GFP_KERNEL);
	if (state == NULL)
		return -ENOMEM;

	state->client = client;
	state->field = V4L2_FIELD_ALTERNATE;
	state->chip_info = (struct adv7180_chip_info *)id->driver_data;

	state->pwdn_gpio = devm_gpiod_get_optional(&client->dev, "powerdown",
						   GPIOD_OUT_HIGH);
	if (IS_ERR(state->pwdn_gpio)) {
		ret = PTR_ERR(state->pwdn_gpio);
		v4l_err(client, "request for power pin failed: %d\n", ret);
		return ret;
	}

	if (state->chip_info->flags & ADV7180_FLAG_MIPI_CSI2) {
		state->csi_client = i2c_new_dummy_device(client->adapter,
				ADV7180_DEFAULT_CSI_I2C_ADDR);
		if (IS_ERR(state->csi_client))
			return PTR_ERR(state->csi_client);
	}

	if (state->chip_info->flags & ADV7180_FLAG_I2P) {
		state->vpp_client = i2c_new_dummy_device(client->adapter,
				ADV7180_DEFAULT_VPP_I2C_ADDR);
		if (IS_ERR(state->vpp_client)) {
			ret = PTR_ERR(state->vpp_client);
			goto err_unregister_csi_client;
		}
	}

	state->irq = client->irq;
	mutex_init(&state->mutex);
	state->curr_norm = V4L2_STD_PAL; //NTSC
	if (state->chip_info->flags & ADV7180_FLAG_RESET_POWERED)
		state->powered = true;
	else
		state->powered = false;
	state->input = 0;
	sd = &state->sd;
	v4l2_i2c_subdev_init(sd, client, &adv7180_ops);
	sd->flags |= V4L2_SUBDEV_FL_HAS_DEVNODE | V4L2_SUBDEV_FL_HAS_EVENTS;

	ret = adv7180_init_controls(state);
	if (ret)
		goto err_unregister_vpp_client;

	state->pad.flags = MEDIA_PAD_FL_SOURCE;
	sd->entity.function = MEDIA_ENT_F_ATV_DECODER;
	//AZIZ
	sd->entity.ops = &adv7180_entity_ops;
	//AZIZ
	ret = media_entity_pads_init(&sd->entity, 1, &state->pad);
	if (ret)
		goto err_free_ctrl;

	ret = init_device(state);
	if (ret)
		goto err_media_entity_cleanup;

	if (state->irq) {
		ret = request_threaded_irq(client->irq, NULL, adv7180_irq,
					   IRQF_ONESHOT | IRQF_TRIGGER_FALLING,
					   KBUILD_MODNAME, state);
		if (ret)
			goto err_media_entity_cleanup;
	}

	ret = v4l2_async_register_subdev(sd);
	if (ret)
		goto err_free_irq;

	mutex_lock(&state->mutex);
	ret = adv7180_read(state, ADV7180_REG_IDENT);
	mutex_unlock(&state->mutex);
	if (ret < 0)
		goto err_v4l2_async_unregister;

	v4l_info(client, "chip id 0x%x found @ 0x%02x (%s)\n",
		 ret, client->addr, client->adapter->name);

	return 0;

err_v4l2_async_unregister:
	v4l2_async_unregister_subdev(sd);
err_free_irq:
	if (state->irq > 0)
		free_irq(client->irq, state);
err_media_entity_cleanup:
	media_entity_cleanup(&sd->entity);
err_free_ctrl:
	adv7180_exit_controls(state);
err_unregister_vpp_client:
	i2c_unregister_device(state->vpp_client);
err_unregister_csi_client:
	i2c_unregister_device(state->csi_client);
	mutex_destroy(&state->mutex);
	return ret;
}

static int adv7180_remove(struct i2c_client *client)
{
	printk("ADV7180 Status : Girdi 46\n");
	struct v4l2_subdev *sd = i2c_get_clientdata(client);
	struct adv7180_state *state = to_state(sd);

	v4l2_async_unregister_subdev(sd);

	if (state->irq > 0)
		free_irq(client->irq, state);

	media_entity_cleanup(&sd->entity);
	adv7180_exit_controls(state);

	i2c_unregister_device(state->vpp_client);
	i2c_unregister_device(state->csi_client);

	adv7180_set_reset_pin(state, true);
	adv7180_set_power_pin(state, false);

	mutex_destroy(&state->mutex);

	return 0;
}

static const struct i2c_device_id adv7180_id[] = {
	{ "adv7180", (kernel_ulong_t)&adv7180_info },
	{ "adv7180cp", (kernel_ulong_t)&adv7180_info },
	{ "adv7180st", (kernel_ulong_t)&adv7180_info },
	{ "adv7182", (kernel_ulong_t)&adv7182_info },
	{ "adv7280", (kernel_ulong_t)&adv7280_info },
	{ "adv7280-m", (kernel_ulong_t)&adv7280_m_info },
	{ "adv7281", (kernel_ulong_t)&adv7281_info },
	{ "adv7281-m", (kernel_ulong_t)&adv7281_m_info },
	{ "adv7281-ma", (kernel_ulong_t)&adv7281_ma_info },
	{ "adv7282", (kernel_ulong_t)&adv7282_info },
	{ "adv7282-m", (kernel_ulong_t)&adv7282_m_info },
	{},
};
MODULE_DEVICE_TABLE(i2c, adv7180_id);

#ifdef CONFIG_PM_SLEEP
static int adv7180_suspend(struct device *dev)
{
	printk("ADV7180 Status : Girdi 47\n");
	struct i2c_client *client = to_i2c_client(dev);
	struct v4l2_subdev *sd = i2c_get_clientdata(client);
	struct adv7180_state *state = to_state(sd);

	return adv7180_set_power(state, false);
}

static int adv7180_resume(struct device *dev)
{
	printk("ADV7180 Status : Girdi 48\n");
	struct i2c_client *client = to_i2c_client(dev);
	struct v4l2_subdev *sd = i2c_get_clientdata(client);
	struct adv7180_state *state = to_state(sd);
	int ret;

	ret = init_device(state);
	if (ret < 0)
		return ret;

	ret = adv7180_set_power(state, state->powered);
	if (ret)
		return ret;

	return 0;
}

static SIMPLE_DEV_PM_OPS(adv7180_pm_ops, adv7180_suspend, adv7180_resume);
#define ADV7180_PM_OPS (&adv7180_pm_ops)

#else
#define ADV7180_PM_OPS NULL
#endif

#ifdef CONFIG_OF
static const struct of_device_id adv7180_of_id[] = {
	{ .compatible = "adi,adv7180", },
	{ .compatible = "adi,adv7180cp", },
	{ .compatible = "adi,adv7180st", },
	{ .compatible = "adi,adv7182", },
	{ .compatible = "adi,adv7280", },
	{ .compatible = "adi,adv7280-m", },
	{ .compatible = "adi,adv7281", },
	{ .compatible = "adi,adv7281-m", },
	{ .compatible = "adi,adv7281-ma", },
	{ .compatible = "adi,adv7282", },
	{ .compatible = "adi,adv7282-m", },
	{ },
};

MODULE_DEVICE_TABLE(of, adv7180_of_id);
#endif

static struct i2c_driver adv7180_driver = {
	.driver = {
		   .name = KBUILD_MODNAME,
		   .pm = ADV7180_PM_OPS,
		   .of_match_table = of_match_ptr(adv7180_of_id),
		   },
	.probe = adv7180_probe,
	.remove = adv7180_remove,
	.id_table = adv7180_id,
};

module_i2c_driver(adv7180_driver);

MODULE_DESCRIPTION("Analog Devices ADV7180 video decoder driver");
MODULE_AUTHOR("Mocean Laboratories");
MODULE_LICENSE("GPL v2");

"""" imx8mp-evk.dts """"

adv7280@21{
                compatible = "adi,adv7280-m";
                reg = <0x21>;
		status ="okay";
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_adv7180>;

		powerdown-gpios = <&gpio5 9 GPIO_ACTIVE_LOW>;
		//irq-gpios = <&gpio5 8 GPIO_ACTIVE_LOW>; 
		interrupt-parent = <&gpio5>;
		interrupts = <8 IRQ_TYPE_LEVEL_LOW>;
		reset-gpios = <&gpio5 7 GPIO_ACTIVE_LOW>;		

		//gpios = <&gpio5 9 GPIO_ACTIVE_LOW>,<&gpio5 7 GPIO_ACTIVE_LOW>;
		//DOVDD-supply = <&reg_3p3v>; 
		//AVDD-supply = <&reg_3p3v>; 
		//DVDD-supply = <&reg_3p3v>; 
		//PVDD-supply = <&reg_3p3v>;

		assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
		assigned-clock-rates = <24000000>;

		csi_id = <0>;
		cvbs = <1>;	
		clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		clock-names = "csi_mclk";
		mclk = <24000000>;
		mclk_source = <0>;
		
		//mipi_csi;
		//mipi_camera = <1>;
		//enable-active-low;
		
		

		port {
			adv7280m_out: endpoint {
			remote-endpoint = <&mipi0_sensor_ep>;
			clock-lanes = <0>;
			data-lanes = <1>;
			//max-pixel-frequency = /bits/ 64 <266000000>;
			//max-pixel-frequency = /bits/ 64 <500000000>;		
			
				
			};
		};


        };
        
        
        
        &mipi_csi_0 {
	
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";
	clock_frequency = <24000000>;
	port@0 {
		reg = <0>;
		mipi0_sensor_ep: endpoint {
			remote-endpoint = <&adv7280m_out>;
			data-lanes = <1>;
			csis-hs-settle = <13>;
			csis-clk-settle = <2>;
			csis-wclk;
		};
	};
};

"""" Terminal Output of ADV """"

 dmesg | grep -i adv
[    0.141808] Advanced Linux Sound Architecture Driver Initialized.
[    2.144588] ADV7180 Status : Girdi 45
[    2.148437] ADV7180 Status : Girdi 22
[    2.152131] ADV7180 Status : Girdi 21
[    2.155802] ADV7180 Status : Girdi 10
[    2.159469] ADV7180 Status : Girdi 1
[    2.163044] ADV7180 Status : Girdi 2
[    2.167740] ADV7180 Status : Girdi 21
[    2.171402] ADV7180 Status : Girdi 10
[    2.175082] ADV7180 Status : Girdi 1
[    2.178685] ADV7180 Status : Girdi 2
[    2.184275] ADV7180 Status : Girdi 21
[    2.187951] ADV7180 Status : Girdi 10
[    2.191619] ADV7180 Status : Girdi 1
[    2.195193] ADV7180 Status : Girdi 2
[    2.201056] ADV7180 Status : Girdi 1
[    2.204651] ADV7180 Status : Girdi 2
[    2.209907] ADV7180 Status : Girdi 21
[    2.213591] ADV7180 Status : Girdi 10
[    2.217259] ADV7180 Status : Girdi 1
[    2.220840] ADV7180 Status : Girdi 2
[    2.225534] ADV7180 Status : Girdi 21
[    2.229206] ADV7180 Status : Girdi 10
[    2.234231] ADV7180 Status : Girdi 1
[    2.237815] ADV7180 Status : Girdi 2
[    2.244759] ADV7180 Status : Girdi 1
[    2.248344] ADV7180 Status : Girdi 2
[    2.254221] ADV7180 Status : Girdi 44
[    2.257894] ADV7180 Status : Girdi 18
[    2.273413] ADV7180 Status : Girdi 1
[    2.277005] ADV7180 Status : Girdi 2
[    2.291450] ADV7180 Status : Girdi 41
[    2.295113] ADV7180 Status : Girdi 1
[    2.298695] ADV7180 Status : Girdi 2
[    2.303962] ADV7180 Status : Girdi 1
[    2.307547] ADV7180 Status : Girdi 2
[    2.313422] ADV7180 Status : Girdi 1
[    2.317009] ADV7180 Status : Girdi 2
[    2.322577] ADV7180 Status : Girdi 1
[    2.326163] ADV7180 Status : Girdi 2
[    2.331120] ADV7180 Status : Girdi 1
[    2.334707] ADV7180 Status : Girdi 2
[    2.339970] ADV7180 Status : Girdi 1
[    2.343554] ADV7180 Status : Girdi 2
[    2.349432] ADV7180 Status : Girdi 1
[    2.353019] ADV7180 Status : Girdi 2
[    2.358586] ADV7180 Status : Girdi 1
[    2.362173] ADV7180 Status : Girdi 2
[    2.367128] ADV7180 Status : Girdi 1
[    2.370713] ADV7180 Status : Girdi 2
[    2.375982] ADV7180 Status : Girdi 14
[    2.379654] ADV7180 Status : Girdi 7
[    2.383229] ADV7180 Status : Girdi 5
[    2.386814] ADV7180 Status : Girdi 1
[    2.390394] ADV7180 Status : Girdi 2
[    2.396276] ADV7180 Status : Girdi 26
[    2.399950] ADV7180 Status : Girdi 4
[    2.405245] ADV7180 Status : Girdi 4
[    2.410187] ADV7180 Status : Girdi 4
[    2.415133] ADV7180 Status : Girdi 4
[    2.420687] ADV7180 Status : Girdi 4
[    2.426548] ADV7180 Status : Girdi 4
[    2.432102] ADV7180 Status : Girdi 4
[    2.437961] ADV7180 Status : Girdi 4
[    2.443577] ADV7180 Status : Girdi 6
[    2.449433] ADV7180 Status : Girdi 6
[    2.454409] ADV7180 Status : Girdi 6
[    2.460725] ADV7180 Status : Girdi 1
[    2.464310] ADV7180 Status : Girdi 2
[    2.469268] ADV7180 Status : Girdi 1
[    2.472852] ADV7180 Status : Girdi 2
[    2.477539] ADV7180 Status : Girdi 1
[    2.481124] ADV7180 Status : Girdi 2
[    2.486084] ADV7180 Status : Girdi 1
[    2.489668] ADV7180 Status : Girdi 2
[    2.494629] ADV7180 Status : Girdi 1
[    2.498213] ADV7180 Status : Girdi 2
[    2.505615] ADV7180 Status : Girdi 1
[    2.509211] ADV7180 Status : Girdi 3
[    2.514286] adv7180 1-0021: chip id 0x43 found @ 0x21 (30a30000.i2c)
[    3.535510] systemd[1]: System time before build time, advancing clock.
[    6.392248] mx8-img-md: Registered sensor subdevice: adv7180 1-0021 (1)
[    6.429061] ADV7180 Status : Girdi 36
[    6.437222] mx8-img-md: created link [adv7180 1-0021] => [mxc-mipi-csi2.0]
[    6.897947] ADV7180 Status : Girdi 27
[    6.897962] ADV7180 Status : Girdi 10
[    6.897965] ADV7180 Status : Girdi 25
[    6.897968] ADV7180 Status : Girdi 10
[    6.899158] ADV7180 Status : Girdi 29
[    6.899168] ADV7180 Status : Girdi 28
[    6.899171] ADV7180 Status : Girdi 10
[    6.899173] ADV7180 Status : Girdi 25
[    6.899175] ADV7180 Status : Girdi 10

"""" Gstreamer Output """"

gst-launch-1.0 v4l2src device=/dev/video3 ! vidw,width=720,height=144 ! queue ! fpsdisplaysink sync=false
[  170.955754] ADV7180 Status : Girdi 29
[  170.959424] ADV7180 Status : Girdi 28
[  170.963180] ADV7180 Status : Girdi 10
[  170.966863] ADV7180 Status : Girdi 25
[  170.970668] ADV7180 Status : Girdi 10
[  170.989613] ADV7180 Status : Girdi 27
[  170.993299] ADV7180 Status : Girdi 10
[  170.996980] ADV7180 Status : Girdi 25
[  171.000658] ADV7180 Status : Girdi 10
Setting pipeline to PAUSED ...
[  171.056697] ADV7180 Status : Girdi 27
[  171.060463] ADV7180 Status : Girdi 10
[  171.064163] ADV7180 Status : Girdi 25
[  171.067869] ADV7180 Status : Girdi 10
Pipeline is live and does not need PREROLL ...
Pipeline is PRER[  171.075671] ADV7180 Status : Girdi 17
OLLED ...
Setting pipeline to PL[  171.081738] ADV7180 Status : Girdi 10
AYING ...
New clock: GstSystemCl[  171.090055] ADV7180 Status : Girdi 20
ock
[  171.094790] ADV7180 Status : Girdi 10
[  171.098877] ADV7180 Status : Girdi 19
[  171.103068] ADV7180 Status : Girdi 1
[  171.106662] ADV7180 Status : Girdi 2
[  171.110750] ADV7180 Status : Girdi 4
[  171.114833] ADV7180 Status : Girdi 4
[  171.118918] ADV7180 Status : Girdi 4
[  171.123010] ADV7180 Status : Girdi 4
[  171.127087] ADV7180 Status : Girdi 4
[  171.131163] ADV7180 Status : Girdi 4
[  171.135257] ADV7180 Status : Girdi 28
[  171.138937] ADV7180 Status : Girdi 10
[  171.142613] ADV7180 Status : Girdi 25
[  171.146302] ADV7180 Status : Girdi 10
[  171.149982] ADV7180 Status : Girdi 27
[  171.153660] ADV7180 Status : Girdi 10
[  171.157349] ADV7180 Status : Girdi 25
[  171.161025] ADV7180 Status : Girdi 10
[  171.169709] bypass csc
[  171.172077] input fmt YUV4
[  171.174781] output fmt YUYV
[  171.487786] ADV7180 Status : Girdi 34
[  171.491472] ADV7180 Status : Girdi 10
[  171.495133] ADV7180 Status : Girdi 34 ENABLE RET IF

We have been struggling this for about 2 months now. We have tried pretty much all the recommended solutions on the internet, but none of them works. Any help would be greatly appreciated. No error message or anything else is shown, but we still don't get any video frames or captures from the camera.  Thanks for your help.

Parents
  • Hi,

      Please ensure with below things,

    1) Make sure whether ADV7280-M is programmed correctly with ADI recommended I2C writes,
    2) Could you ensure that during power-up: the reset pin is held low for at least 5ms after the 3.3V, 1.8V and powerdown lines go high. After the reset pin goes high, wait for at least 5ms before starting I2C communication.
    3) After programming the ADV7280-M could you please read the User Map register 0x0F. This should have the value 0x00.
    4) Can you ensure that there is no contention on the lines. i.e. that the backend processor could be trying to pull the line low as the ADV7280-M tries to output a MIPI clock.
    5) The backend processor is not configured correctly and it is pulling the clock lane low. Could you double check that the backend processor is configured correctly with latest software.
    Expert written an applications note describing the main issues interfacing the ADV728x with a MIPI receiver. Please refer the link here: : https://www.analog.com/media/en/technical-documentation/application-notes/AN-1337.pdf
    And also please check that the reset and power-down pins are controlled in the manner described in the datasheet "optimal power-up sequence" section.
    Also please check freescale forum ADV7181 on IMX6Q board | Freescale Community
    Note: As part of the MIPI specification the MIPI receiver needs to terminate the signals correctly. The termination required changes depending on the MIPI mode (e.g. high speed, low power mode etc). The receiver needs to detect the mode of operation and dynamically set its termination accordingly.
    Note that the Clock signals will only appear correctly when properly terminated.Until proper termination is achieved then you will not be able to decode video data from the MIPI CSI-2 signals output by the ADV7280-M.

    ADI linux drivers can be found at  Linux Drivers [Analog Devices Wiki]
    The Linux driver for the ADV7280 branch in the Linux kernel git repository on the ADI github account.

    https://github.com/analogdevicesinc/linux/tree/adv7280

    https://github.com/analogdevicesinc/linux/blob/adv7280/drivers/media/i2c/adv7180.c

    This driver support parts for both ADV718x and ADV728x family.
    Also ADV7282-M driver is part of the upstream Linux kernel distribution and can be found at http://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/media/i2c/adv7180.c

    Thanks,

    Poornima

Reply
  • Hi,

      Please ensure with below things,

    1) Make sure whether ADV7280-M is programmed correctly with ADI recommended I2C writes,
    2) Could you ensure that during power-up: the reset pin is held low for at least 5ms after the 3.3V, 1.8V and powerdown lines go high. After the reset pin goes high, wait for at least 5ms before starting I2C communication.
    3) After programming the ADV7280-M could you please read the User Map register 0x0F. This should have the value 0x00.
    4) Can you ensure that there is no contention on the lines. i.e. that the backend processor could be trying to pull the line low as the ADV7280-M tries to output a MIPI clock.
    5) The backend processor is not configured correctly and it is pulling the clock lane low. Could you double check that the backend processor is configured correctly with latest software.
    Expert written an applications note describing the main issues interfacing the ADV728x with a MIPI receiver. Please refer the link here: : https://www.analog.com/media/en/technical-documentation/application-notes/AN-1337.pdf
    And also please check that the reset and power-down pins are controlled in the manner described in the datasheet "optimal power-up sequence" section.
    Also please check freescale forum ADV7181 on IMX6Q board | Freescale Community
    Note: As part of the MIPI specification the MIPI receiver needs to terminate the signals correctly. The termination required changes depending on the MIPI mode (e.g. high speed, low power mode etc). The receiver needs to detect the mode of operation and dynamically set its termination accordingly.
    Note that the Clock signals will only appear correctly when properly terminated.Until proper termination is achieved then you will not be able to decode video data from the MIPI CSI-2 signals output by the ADV7280-M.

    ADI linux drivers can be found at  Linux Drivers [Analog Devices Wiki]
    The Linux driver for the ADV7280 branch in the Linux kernel git repository on the ADI github account.

    https://github.com/analogdevicesinc/linux/tree/adv7280

    https://github.com/analogdevicesinc/linux/blob/adv7280/drivers/media/i2c/adv7180.c

    This driver support parts for both ADV718x and ADV728x family.
    Also ADV7282-M driver is part of the upstream Linux kernel distribution and can be found at http://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/media/i2c/adv7180.c

    Thanks,

    Poornima

Children
No Data