Post Go back to editing

[ADV7480] About laptop audio output

Thread Summary

The user is troubleshooting an issue where audio is not output from a Windows 10 laptop to a monitor equipped with the ADV7480 HDMI receiver. The final answer suggests that the EDID supports only LPCM audio and recommends toggling the HPA line to force the PC to re-read the EDID. The sequence to toggle HPA should be executed from the HPD=H state and involves setting specific register values. The user should also verify the audio stream format being played from the laptop.
AI Generated Content
Category: Software

Hi,

We are evaluating the ADV780 product.

I am checking the video/audio output by connecting the HDMI output of a Windows 10 laptop (Dynabook R73)

to a monitor equipped with ADV7480.

The video from the PC is output, but the audio from the PC is not output.

(PC audio driver itself does not recognize)

What could be the cause?

For monitors without ADV7480, PC audio is output.

Best regards.

Parents Reply Children
  • Hi Tatsuya San,

            It seems your corresponding EDID would support only LPCM audio.

            Please let us know, the audio stream that you are playing from the laptop.

            Also Please note sometimes PC has failed to get the correct EDID, So toggle the HPA line to force the PC to re-read the EDID and follow either below two sequence,

           This must be done after the EDID is loaded.

    1) Set HPA_MAN_VALUE_A = 1 ; sets bit high

    2) HPA_TRISTATE_A = 0 ;  make HPA pin an output

    3) set HPA_MAN_VALUE = 0 ; Pulls HPA pin low

    4) wait 100ms ; just delay a bit

    5) set HPA_TRISTATE = 1 ; makes HPA pin an input

    6) External pull up resistor will create the rising edge on the HPD  causing the PC to re-read the EDID

    Or

    1) HPA_MAN_VALUE_X =1

    2) HPA_A pin active =0

    3)  HPA_MAN_VALUE_A =0, sets HPA low

    4)  load up the EDID

    5) HPA_MAN_VALUE_A =1, sets HPA high, forces source to reload EDID

       

    Thanks,

    Poornima

  • Hi,

    Sorry for the late thank you.

    Thank you for your reply.

    I have additional questions.

    Q1) Can the above sequence be executed from the HPD=H state?

    Q2) In the above sequence, is the following correct register setting procedure

           for the ADV7480 device?

          1) Set HPA_MAN_VALUE_A = 1 ; sets bit high     

          2) HPA_TRISTATE_A = 0 ; make HPA pin an output

          3) set HPA_MAN_VALUE = 0 ; Pulls HPA pin low

          4) wait 100ms ; just delay a bit

          5) set HPA_TRISTATE = 1 ; makes HPA pin an input     

        ↓

          1) HDMI Rx-MAP(0x68) Register Addr(0xF8) Data (0x01)

          2) HDMI Rx-MAP(0x68) Register Addr(0xF9) Data (0x00)

          3) HDMI Rx-MAP(0x68) Register Addr(0xF8) Data (0x00)

          4) 100ms wait

          5) HDMI Rx-MAP(0x68) Register Addr(0xF9) Data (0x01)

     Or
          1) HPA_MAN_VALUE_X=1

          2) HPA_A pin active =0

          3) HPA_MAN_VALUE_A =0, sets HPA low

          4) load up the EDID

          5) HPA_MAN_VALUE_A =1, sets HPA high, forces source to reload EDID

                 ↓

          1) HDMI Rx-MAP(0x68) Register Addr(0x6C) Data (0x01)

          2) HDMI Rx-MAP(0x68) Register Addr(0xF9) Data (0x00)

          3) HDMI Rx-MAP(0x68) Register Addr(0xF8) Data (0x00)

          4) ??

          5) HDMI Rx-MAP(0x68) Register Addr(0xF8) Data (0x01)

          How can we control "4)"?

    Best regards.

  • Hi Tatsuya San,

    Please find the below comments,

     Q1) Can the above sequence be executed from the HPD=H state?

    YES, the sequence should be executed from HPD High state.

    Please note When the sink toggles the HPA line low then high, It tells the source to read the EDID data.  Normally with source will not read the EDID until it sees a low to high transition( By spec, the low to high HPD transition should cause the source to read the EDID). 

    Q2) How can we control "4)"?

    Please configure the below EDID in your script.

    And this CEA write would indicate the CEA tag is present "6C 80 02" .

    64 74 00 ; Disable the Internal EDID for all ports

    6C 00 00 ;

    6C 01 FF ;

    6C 02 FF ;

    6C 03 FF ;

    6C 04 FF ;

    6C 05 FF ;

    6C 06 FF ;

    6C 07 00 ;

    6C 08 06 ;

    6C 09 8F ;

    6C 0A 07 ;

    6C 0B 11 ;

    6C 0C 01 ;

    6C 0D 00 ;

    6C 0E 00 ;

    6C 0F 00 ;

    6C 10 17 ;

    6C 11 11 ;

    6C 12 01 ;

    6C 13 03 ;

    6C 14 80 ;

    6C 15 0C ;

    6C 16 09 ;

    6C 17 78 ;

    6C 18 0A ;

    6C 19 1E ;

    6C 1A AC ;

    6C 1B 98 ;

    6C 1C 59 ;

    6C 1D 56 ;

    6C 1E 85 ;

    6C 1F 28 ;

    6C 20 29 ;

    6C 21 52 ;

    6C 22 57 ;

    6C 23 00 ;

    6C 24 00 ;

    6C 25 00 ;

    6C 26 01 ;

    6C 27 01 ;

    6C 28 01 ;

    6C 29 01 ;

    6C 2A 01 ;

    6C 2B 01 ;

    6C 2C 01 ;

    6C 2D 01 ;

    6C 2E 01 ;

    6C 2F 01 ;

    6C 30 01 ;

    6C 31 01 ;

    6C 32 01 ;

    6C 33 01 ;

    6C 34 01 ;

    6C 35 01 ;

    6C 36 8C ;

    6C 37 0A ;

    6C 38 D0 ;

    6C 39 8A ;

    6C 3A 20 ;

    6C 3B E0 ;

    6C 3C 2D ;

    6C 3D 10 ;

    6C 3E 10 ;

    6C 3F 3E ;

    6C 40 96 ;

    6C 41 00 ;

    6C 42 81 ;

    6C 43 60 ;

    6C 44 00 ;

    6C 45 00 ;

    6C 46 00 ;

    6C 47 18 ;

    6C 48 01 ;

    6C 49 1D ;

    6C 4A 80 ;

    6C 4B 18 ;

    6C 4C 71 ;

    6C 4D 1C ;

    6C 4E 16 ;

    6C 4F 20 ;

    6C 50 58 ;

    6C 51 2C ;

    6C 52 25 ;

    6C 53 00 ;

    6C 54 81 ;

    6C 55 49 ;

    6C 56 00 ;

    6C 57 00 ;

    6C 58 00 ;

    6C 59 9E ;

    6C 5A 00 ;

    6C 5B 00 ;

    6C 5C 00 ;

    6C 5D FC ;

    6C 5E 00 ;

    6C 5F 56 ;

    6C 60 41 ;

    6C 61 2D ;

    6C 62 31 ;

    6C 63 38 ;

    6C 64 30 ;

    6C 65 39 ;

    6C 66 41 ;

    6C 67 0A ;

    6C 68 20 ;

    6C 69 20 ;

    6C 6A 20 ;

    6C 6B 20 ;

    6C 6C 00 ;

    6C 6D 00 ;

    6C 6E 00 ;

    6C 6F FD ;

    6C 70 00 ;

    6C 71 17 ;

    6C 72 3D ;

    6C 73 0D ;

    6C 74 2E ;

    6C 75 11 ;

    6C 76 00 ;

    6C 77 0A ;

    6C 78 20 ;

    6C 79 20 ;

    6C 7A 20 ;

    6C 7B 20 ;

    6C 7C 20 ;

    6C 7D 20 ;

    6C 7E 01 ;

    6C 7F 1C ;

    6C 80 02 ;

    6C 81 03 ;

    6C 82 3D ;

    6C 83 71 ;

    6C 84 4D ;

    6C 85 82 ;

    6C 86 05 ;

    6C 87 04 ;

    6C 88 01 ;

    6C 89 10 ;

    6C 8A 11 ;

    6C 8B 14 ;

    6C 8C 13 ;

    6C 8D 1F ;

    6C 8E 06 ;

    6C 8F 15 ;

    6C 90 03 ;

    6C 91 12 ;

    6C 92 3E ;

    6C 93 0F ;

    6C 94 7F ;

    6C 95 07 ;

    6C 96 17 ;

    6C 97 1F ;

    6C 98 38 ;

    6C 99 1F ;

    6C 9A 07 ;

    6C 9B 30 ;

    6C 9C 2F ;

    6C 9D 07 ;

    6C 9E 72 ;

    6C 9F 3F ;

    6C A0 7F ;

    6C A1 72 ;

    6C A2 4F ;

    6C A3 7F ;

    6C A4 00 ;

    6C A5 57 ;

    6C A6 7F ;

    6C A7 00 ;

    6C A8 5F ;

    6C A9 7F ;

    6C AA 01 ;

    6C AB 37 ;

    6C AC 7F ;

    6C AD 72 ;

    6C AE 67 ;

    6C AF 7F ;

    6C B0 00 ;

    6C B1 83 ;

    6C B2 4F ;

    6C B3 00 ;

    6C B4 00 ;

    6C B5 67 ;

    6C B6 03 ;

    6C B7 0C ;

    6C B8 00 ;

    6C B9 10 ;

    6C BA 00 ;

    6C BB B8 ;

    6C BC 2D ;

    6C BD 01 ;

    6C BE 1D ;

    6C BF 00 ;

    6C C0 72 ;

    6C C1 51 ;

    6C C2 D0 ;

    6C C3 1E ;

    6C C4 20 ;

    6C C5 6E ;

    6C C6 28 ;

    6C C7 55 ;

    6C C8 00 ;

    6C C9 81 ;

    6C CA 49 ;

    6C CB 00 ;

    6C CC 00 ;

    6C CD 00 ;

    6C CE 1E ;

    6C CF D6 ;

    6C D0 09 ;

    6C D1 80 ;

    6C D2 A0 ;

    6C D3 20 ;

    6C D4 E0 ;

    6C D5 2D ;

    6C D6 10 ;

    6C D7 10 ;

    6C D8 60 ;

    6C D9 A2 ;

    6C DA 00 ;

    6C DB 81 ;

    6C DC 60 ;

    6C DD 00 ;

    6C DE 08 ;

    6C DF 08 ;

    6C E0 18 ;

    6C E1 8C ;

    6C E2 0A ;

    6C E3 D0 ;

    6C E4 90 ;

    6C E5 20 ;

    6C E6 40 ;

    6C E7 31 ;

    6C E8 20 ;

    6C E9 0C ;

    6C EA 40 ;

    6C EB 55 ;

    6C EC 00 ;

    6C ED 81 ;

    6C EE 60 ;

    6C EF 00 ;

    6C F0 00 ;

    6C F1 00 ;

    6C F2 18 ;

    6C F3 00 ;

    6C F4 00 ;

    6C F5 00 ;

    6C F6 00 ;

    6C F7 00 ;

    6C F8 00 ;

    6C F9 00 ;

    6C FA 00 ;

    6C FB 00 ;

    6C FC 00 ;

    6C FD 00 ;

    6C FE 00 ;

    6C FF 46 ;

    64 71 00 ; Set the Most Significant Bit of the SPA location to 0

    64 52 20 ; Set the SPA for port B

    64 53 00 ; Set the SPA for port B.

    64 70 B9 ; Set the Least Significant Byte of the SPA location

    64 74 03 ; Enable the Internal EDID for ports

    End

    Please refer (+) How can I use ADV7611 with an internal EDID - Q&A - Video - EngineerZone (analog.com)

    Thanks,

    Poornima

  • Hi,

    Thank you for your reply.

    I would like to ask a question regarding the answer to Q1 above.

    Is it correct that the Hot Plug Detect (HPD) transition always starts from H,

    HPD=H → HPD=L → HPD=H?

    Best regards.

  • Hi Tatsuya San,

             HPD=H → HPD=L → HPD=H ?

                Yes, the below suggested sequence is given by expert so it should be H -> L -> H

    1) HPA_MAN_VALUE_X =1

    2) HPA_A pin active =0

    3)  HPA_MAN_VALUE_A =0, sets HPA low

    4)  load up the EDID

    5) HPA_MAN_VALUE_A =1, sets HPA high, forces source to reload EDID

    Thanks,

    Poornima

  • Hi,

    Thank you for your reply.

    Sorry for asking so many questions.

    Before and after the HDMI device is connected,

    does the HPD sequence look like the following?

    ①Before connecting an HDMI device: HPD = L

    ②After connecting HDMI equipment: 

     1) HPD=H

        2) HPD = L

        3) 100ms wait

        4) HPD=H

        In this case, how long should HPD=H be maintained in 1)?

    Best regards.

  • Hi Tatsuya San,

          Please find the below comments,

     ① Before connecting an HDMI device: HPD = L

           Generally the Sink device will supply a voltage on an HPD pin to signal to the video source device that it is connected So the video source device monitors the voltage on the HPD pin and then initiates EDID requests as it senses incoming voltage.

         If HDMI device is disconnected then the HPD would be in LOW State (The absences of a voltage on the HPD pin indicates disconnection).

    ② After connecting HDMI equipment: 

         In this case, how long should HPD=H be maintained in 1) ?

          There is no specific time duration that we need to maintained for the case "1. HPD=H" .

         Please note But "After HPD become low, We need to wait 100ms".

    Thanks,

    Poornima