Hi,
I have a question regrading ADV7611/19 chips. I have a device which does alter the input tmds clock to adv7611/19 , when is trying to genlock. Sometimes I am getting image shifting during the genlock process. I noticed that during initial steps of genlock process DC_FIFO_LOCKED goes low and after high. I noticed a huge improvement in my case when in the DPLL address register 0xc3 to 0x80 and 0x3F to 0x03. Initial value for this register was 0x"00". Video resolution tested :1920x1080x30Hz(pixel clock = 74.25 Mhz) and 1920x1080x60Hz(pixel clock = 148.5 Mhz). I was thinking that the issue with image shifting is caused by video fifo underflow/overflow condition and I noticed that DPLL is disable for pixel clock greater than 170 Mhz. In the recommended register setting document I manage to find the above register settings.
Question :
1. What are those register ? I am not able to find any description in the datasheet.
2. Is it safe to have those register settings for all modes ? What are the implication of setting those register for those values for all modes ?
Thank you.