Post Go back to editing

ADV7800_1080p_10bit Resolution Support

Dear Sir

We study ADV7800 to use 1080p or less than resolution.

We checked the datasheet.

We understand that ADV7800 can support 1080p59.94/60Hz.

But we have some question about ADV7800 performance at 1080p resolution.

1. Depth 10bit support.

There are description that ADV7800 support 8bit at "BSL 150MHz". 

Can ADV7800 support 10bit depth color at 1080P50/59.94/60Hz?

 

2. Support Output Dot Clock

We would like to use the format 1080i/50Hz/59.94Hz and 1080p50/59.94Hz.

These format clock is as follows.

1080/59.94i:74.175MHz

1080/50i:74.25MHz

1080/59.94p:148.35MHz

 1080/50p:148.5MHz

Can ADV7800 support to output these Clock by internal   PLL?

BR Kida