Hi team
I am planning to use an ADV8005 Serial Video RX core and two TX cores.
So, could you please tell me if I can use the ADV8005 in the following way?
A) HDMI signal 2160p30fps (297MHz) input is split into two and HDMI output 4K30fps (297MHz).
B) Similarly, split the 1080p60Hz (148.5MHz) input into two and HDMI output 1080p60Hz (148.5MHz).
C) Convert one of the two HDMI outputs in configuration B to a DVI signal.
D) Convert the opposite of C to a DVI signal.
E) Convert both outputs to DVI signal.
Also, I am thinking that DDR implementation is not necessary when making the above operation, is this correct?
Thank you.
Maru