Post Go back to editing

About AP1_OUT of ADV7625

Hi.

Please tell me about ADV7625.

I set the AP1_OUT port pins individually using the tristate_ap1_out_x [7:0] control register.

I'd like to use the AP1_OUT4 port, but the port couldn't communicate as I2S data.

The AP1_OUT port 0 and 1 were working as I2S data and I could measure their waveform.

Could you help me?

Best Regards

Morry

Parents
  • Hi,

      'AP1_OUT4' should output I2S data , Please make sure whether you are in I2S mode.

       

    Also make sure this corresponding bit - TRISTATE_AP1_OUT_X[4] = Tristate AP1_OUT[4] pin should be '0' in register TRISTATE_AP1_OUT_X[7:0] (0x9D).

    Thanks,

    Poornima

  • Dear Poornima

    Hi.

    Thank you for your answer.

    I checked out I2S mode for AP1_OUT4 port but I didn't confirm the waveform as I2s data.

    I understand that Tristate AP1_OUT[4] pin should be '0' in register.

    Which device address is 00 or EC?

    I executed in the following steps.

    ①used script file (ADV7625-26-27_Ver1.0)

    ②selected HDMI Splitter Mode 

    ③set Tristate AP1_OUT_X

    ④set I2S out mode

    Best Regards

    Morry

  • Hi,

      In Eval board i have not get any chance to verify but in Melody boards we are using ADV7625 part .

      In Melody boards, We have verified 'MCPCM to Compressed streams' using ADV7625 chip. So I am sure our ADV7625 part can support 4xI2S.

      Please make sure, Whether you are pumping multichannel stream ?

      Also make sure whether you have the enabled the register as "Audio from HDMI Rx1" (i.e if  source is connected to RX1)

    Thanks,

    Poornima

  • Dear Poornima.

     

    Hi.

    It's no problem about the register as "Audio from HDMI Rx1".

    How do you think about signal mapping of the AP1_OUT output port?

    Do you think it's related?

    Thanks, 

    Best Regards

    Morry

  • Hi,

      How do you think about signal mapping of the AP1_OUT output port ?

        Please let us know, what does signal mapping sense ?

    Thanks,

    Poornima

  • Dear Poornima

    Hi.

    The default mapping for I2S is as follows.

    Do you think how it's going to turn out If the audio mapping for I2S is changed as follows?

    Please tell me.

    Thanks,

    Best Regards

    Morry

  • Hi,

    YES, below is the default mapping when i2s_spdif_map_rot=00 & i2s_spdif_map_inv =0.

    i2s_spdif_map_inv =1, it will invert the arrangements when i2s_spdif_map_rot=00 & i2s_spdif_map_inv =1.

    i2s_spdif_map_rot[1:0] - This control is used to select the arrangement of the I2S/SPDIF interface on the corresponding APx_OUT audio output port pins and the arrangement of the I2S/SPDIF interface on the audio output port pins is determined by "I2S_SPDIF_MAP_ROT".

     For example "I2S3 on AP1 or I2S0 on AP1" So depending on that you will get the channel output. 

     I2S0/SPDIF0 I2S audio (Channel 1, Channel 2)/SPDIF0

     I2S1/SPDIF1 I2S audio (Channel 3, Channel 4)/SPDIF1

     I2S2/SPDIF2 I2S audio (Channel 5, Channel 6)/SPDIF2

     I2S3/SPDIF3 I2S audio (Channel 7, Channel 8)/SPDIF3

        AP1 - Front L/R

        AP2 - Sub/Cen

        AP3 - Rear L/R

        AP4 - Surround Back L/R

     Please note "i2soutmode[1:0]and i2sbitwidth[4:0]" controls are used to configure the I2S output interface for audio extraction.

    Thanks,

    Poornima

  • Dear Poornima

     

    Hi.

    Sorry, but I've clicked complete by my mistake.

    By the way, I changed I2S audio mapping before but I couldn't confirm the waveform for 

    I2S data from AP1_OUT4.

    What do you have any answers?

     

    Thanks, 

    Best Regards

    Morry

  • Hi,

     As i already mentioned,  We have used ADV7625 part in Eval Melody5/6/7/8

     ADV7625 part has four I2S pins and this has been connected to DSP processor for achieving the 8 channel output of PCM,HBR etc.

     But I don't know, why this is not working from your end.

    Thanks,

    Poornima

  • Dear

    Poornima

    Hi.

    Could you tell me the register that you use if it's possible ?

    Thanks,

    Best Regards

    Morry

  • Hi,

      As stated, Will use above register for enabling the extraction other than that there is no much complication of using the register for enabling the extraction.  Please let us know, Is it Possible for you to tape-out the I2S pins ?

      In your driver, Have you implemented any commands for enabling the extraction. Please ensure whether you are giving the commands in right way.

      

      Have you reviewed your schematic with our reference one 7356.EVAL-ADV7625-SMZ_rev0p1_schems_20150811.pdf

    Thanks,

    Poornima

  • Dear Poornima

    Hi.

    I use a script file (4101.ADV7625-26-27_Ver1.0.txt) and enable the extraction so I haven't implemented any commands.

    I have reviewed my schematic with your reference one.

    I think it is no problem.

    What do you mean "tape-out the I2S pins" ?

    Thanks,

    Best Regards

    Morry

Reply Children