Post Go back to editing

About AP1_OUT of ADV7625

Thread Summary

The user is troubleshooting I2S data output on AP1_OUT4 of the ADV7625 HDMI Splitter/Evaluator board. The final answer suggests configuring the HDMI_Rx1_Map address register (68 6D 40) to swap I2S pins. It also confirms that the ADV7625 supports 4xI2S and 8-channel audio extraction, and advises checking the source for multichannel PCM input and the schematic for proper pin connections.
AI Generated Content

Hi.

Please tell me about ADV7625.

I set the AP1_OUT port pins individually using the tristate_ap1_out_x [7:0] control register.

I'd like to use the AP1_OUT4 port, but the port couldn't communicate as I2S data.

The AP1_OUT port 0 and 1 were working as I2S data and I could measure their waveform.

Could you help me?

Best Regards

Morry

Parents Reply
  • Hi,

    YES, below is the default mapping when i2s_spdif_map_rot=00 & i2s_spdif_map_inv =0.

    i2s_spdif_map_inv =1, it will invert the arrangements when i2s_spdif_map_rot=00 & i2s_spdif_map_inv =1.

    i2s_spdif_map_rot[1:0] - This control is used to select the arrangement of the I2S/SPDIF interface on the corresponding APx_OUT audio output port pins and the arrangement of the I2S/SPDIF interface on the audio output port pins is determined by "I2S_SPDIF_MAP_ROT".

     For example "I2S3 on AP1 or I2S0 on AP1" So depending on that you will get the channel output. 

     I2S0/SPDIF0 I2S audio (Channel 1, Channel 2)/SPDIF0

     I2S1/SPDIF1 I2S audio (Channel 3, Channel 4)/SPDIF1

     I2S2/SPDIF2 I2S audio (Channel 5, Channel 6)/SPDIF2

     I2S3/SPDIF3 I2S audio (Channel 7, Channel 8)/SPDIF3

        AP1 - Front L/R

        AP2 - Sub/Cen

        AP3 - Rear L/R

        AP4 - Surround Back L/R

     Please note "i2soutmode[1:0]and i2sbitwidth[4:0]" controls are used to configure the I2S output interface for audio extraction.

    Thanks,

    Poornima

Children