Hi,
My customer will use ADV7613 for their project.
He has three questions about ADV7613.
Question 1:
The customer's HDMI interface timing(DE mode) is below.
Can ADV7613 support this HDMI interface timing?
This customer’s clock rate (64.5MHz – 80MHz) is within the data sheet clock rate.
So I think ADV7613 can support it.
Is this right?
Question 2:
If your answer of question 1 is yes, could you tell us how we should set registers?
We can get the script file "ADV7613-VER.1.1c.txt" as below:
ez.analog.com/.../6763.ADV7613_5F00_2.zip
The script includes two cases, which one of them is "TMDS CLK Less Than or Equal to 27MHz" and the other one is "TMDS CLK Greater Than 27MHz".
The customer’s clock rate is 64.5MHz – 80MHz in the customer's timing parameter I mentioned on question 1.
Can we use the script "##02 Full Scripts - HDMI Input_LVDS Output script TMDS CLK Greater Than 27MHz##"?
If we have to add some additional register settings for the customer's HDMI interface timing, please let us know.
Question 3:
There are following description about LVDS (oLDI) mapping on the ADV7613 Reference Manual “ADV7613-UG-907.pdf “.
On page 5,
On page 162,
Customer wants to know whether the "VESA mapping" is the "Alternative mapping".
It seems that the "VESA mapping" means the "Alternative mapping".
Is this right?
Thank you!
Best regards.
Tamu