Post Go back to editing

ADV7610 Eval board Software unavailable from ftp.analog.com

Thread Summary

The user encountered issues retrieving directory listings from the ADV7610 Eval Kit FTP server using FileZilla. The solution was to change the encryption setting in FileZilla's Site Manager from 'Use explicit FTP over TLS if available' to 'Only use plain FTP (insecure)'. This workaround resolved the connection timeout issue.
AI Generated Content

When I follow the printed instructions in the ADV7610 Eval Kit, I cannot get the Software from ftp.analog.com.

I get the following in Filezilla:


Status: Resolving address of ftp.analog.com
Status: Connecting to 137.71.25.119:21...
Status: Connection established, waiting for welcome message...
Status: Initializing TLS...
Status: Verifying certificate...
Status: TLS connection established.
Status: Logged in
Status: Retrieving directory listing...
Command: PWD
Response: 257 "/users/adv7610" is current directory
Command: TYPE I
Response: 200 Transfer mode set to BINARY
Command: PASV
Response: 227 Entering Passive Mode (137,71,25,119,212,46).
Command: MLSD
Error: Connection timed out after 20 seconds of inactivity
Error: Failed to retrieve directory listing