Hi,
I have a question about details of I2P (interlace to progressive) conversion of ADV7282A-M.
The expert answered on following thread as follows:
https://ez.analog.com/video/f/q-a/9323/adv7280-deinterlacing-question/7255#7255
>The deinterlacer in the ADV7280, ADV7280-M, ADV7282, ADV7282-M all work on a line doubling rather than on a frame buffering technique.
>This gives the advantage of reduced delay on the output. Also large external memory is not needed.
>The line doubling technique uses a propriety analog devices algorithm.
>It interpolates between two lines (e.g. lines 1 and 3 on an odd frame) to generate the an additional line (e.g. line 2).
>A smoothing filter is also applied to reduce the effect of low angle noise (i.e. jaggies).
Question:
Please tell me more details of the I2P interpolation.
About your comment "It interpolates between two lines (e.g. lines 1 and 3 on an odd frame) to generate the an additional line (e.g. line 2). ",
=> Does it mean linear interpolation? (Does it mean that line2 is interpolated by linear?)
Is it the way to generate line 2 from average of line 1 and line 3?
Thank you!
Best regards.
Tamu