Post Go back to editing

ADV7403 register configuration for STANAG 3350 CLASS B/C Video Signals

Hi,


I have the following requirements for ADV7403:


I/P Video - STANAG 3350 with Sync On Green as Input to the Chip.

1)720x576i @ 50/25Hz(Class B)video resolution, Interlaced video input,RGB(STANAG Class B)
2)720x480i @ 60/30Hz(Class C)video resolution, Interlaced video input,RGB(STANAG Class C)

O/P Video - 16bit YCbCr 4:2:2 as output from the chip.

Hardware Connections:
We have custom hardware with ADV7403 chip whose input channel configuration for RGsB is given below

Ain1 - G and SOG
Ain2 - B
Ain3 - R

Could you please provide the Script for the above configurations?

Also could you please let me know the values to be set for PRIM_MODE, INSEL, SDM_SEL, and VID_STD for the above configurations?

I want to know how to configure ADV7403 to accept RGsB at Ain1, Ain2, and Ain3? What should be the channel settings for the same?

Waiting for a quick response since it is very critical for us to proceed further.

Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.