KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADV7403
Production
The ADV7403 is a high quality, single chip, multiformat video decoder and graphics digitizer. This multiformat decoder supports the conversion of PAL,...
Datasheet
ADV7403 on Analog.com
Hi,
I have the following requirements for ADV7403:
I/P Video - STANAG 3350 with Sync On Green as Input to the Chip.
1)720x576i @ 50/25Hz(Class B)video resolution, Interlaced video input,RGB(STANAG Class B)
2)720x480i @ 60/30Hz(Class C)video resolution, Interlaced video input,RGB(STANAG Class C)
O/P Video - 16bit YCbCr 4:2:2 as output from the chip.
Hardware Connections:
We have custom hardware with ADV7403 chip whose input channel configuration for RGsB is given below
Ain1 - G and SOG
Ain2 - B
Ain3 - R
Could you please provide the Script for the above configurations?
Also could you please let me know the values to be set for PRIM_MODE, INSEL, SDM_SEL, and VID_STD for the above configurations?
I want to know how to configure ADV7403 to accept RGsB at Ain1, Ain2, and Ain3? What should be the channel settings for the same?
Waiting for a quick response since it is very critical for us to proceed further.
Thank you.
Hi,
Please refer this configuration script " ##SCART RGB## "(:SCART RGB IN In Thru CP YPrPb 2X1 8Bit 422 Out through Encoder) in that don't use CVBS connection in the AIN pin and follow the remaining configuration w.r.t reference script
SOG register related configuration are provided in ADV7403 manual & adjust the sync slicer to use SOG.
Also use registers 0xC3 & 0XC4 for configuring the AIN1,AIN2,AIN3 and crosscheck this configuration(ADC SWITCH) in Page 277.
Thanks,
Poornima
Hi,
Thank you for your response.
I want to understand, If I use Ain1, Ain2, and Ain3 using C3 and C4 registers, how ADV7403 understands that Ain1 is G, Ain2 is B and Ain3 is R? With the script given, is it possible that the Chip will recognize Ain1 as G, Ain2 as B and Ain3 as R? Is there any specific settings to be done in order to give RGB properly to the chip?
Thank you.
Hello,
Wanted to know what is the 8-bit DDR mode LLC frequency in CP mode?
Thanks & Regards,
Arpitha
Hi,
DDR mode nothing but the pixel output port can be configured in an 8-/10-/12-bit 4:2:2 YCrCb upto a clock rate of 75Mhz (i.e In DDR mode we can support maximum clock rate upto 75MHz.
Please note DDR mode doesn't change the overall performance of the part-- DDR mode maximum would be half the SDR mode maximum. It's really no different than SDR mode-- just half the pixel clock rate since you are getting pixels on each edge instead of every other edge.

Note: DDR mode, a new data value is presented on the positive and the negative edge of the
LLC (line-locked clock) and, hence double the amount of data is transferred.
Thanks,
Poornima
Hello,
Wanted to know what is the DDR mode maximum and SDR mode maximum?
Thanks,
Arpitha
Hi,
ADV7403 pixel clock can run at 140MHZ, but more than that,it will not support
For example if you are in DDR mode the LLC is 1/2 the pixel clock rate i.e If the pixel clock = 140MHz then DDR clock =70MHz
And If you are running 140MHz then you must be in SDR mode not DDR mode. SDR has one pixel per rising edge while DDR has one pixel per rising edge and one pixel per falling edge.
Thanks,
Poornima
Hello,
Thank you for the response.
As it is for ADV7403, it should same for ADV7181C, correct ?
DDR mode maximum and SDR mode maximum means the maximum clock supported by the chip in SDR and DDR mode
So for 8-bit of pixel data, if SDR mode the pixel clock is 27MHz then in DDR mode it is 13.5MHz
Thanks,
Arpitha
Hi,
As it is for ADV7403, it should same for ADV7181C, correct ?
YES, but pixel clock(LLC) will vary between ADV7403 & ADV7181C.
So for 8-bit of pixel data, if SDR mode the pixel clock is 27MHz then in DDR mode it is 13.5MHz
YES.
Thanks,
Poornima
Hello
Understood. Thank you
But according to our observation with respect to the ADV7181C chipset, when we configure the 0xC9 register to DDR mode and probe the LLC clock it shows 27MHz only, where as it should have been13.5MHz,
Can you suggest why is this observation?
Thanks,
Arpitha
Hi,
Please let us know, whether you have assign the DDR bus pin as per table 51.

Thanks,
Poornima
Hello,
The data bus pin are given from P12 to P19 for 8-bit DDR mode
Attached is the capture of one of the data signal with respect to the LLC clock
Thanks,
Arpitha
Hi,
Please let us know your format (resolution) ?
Thanks,
Poornima
Hi,
Please let us know your format (resolution) ?
Thanks,
Poornima
Hello,
Resolution is 720*575 @25i (STANAG RGB 3350B)
Thanks,
Arpitha
Hi,
Please let us know your pixel clock and also your oversampling mode(4x or 2x).
Meanwhile let me check with expert also.
Thanks,
Poornima