ADV7403
Production
The ADV7403 is a high quality, single chip, multiformat video decoder and graphics digitizer. This multiformat decoder supports the conversion of PAL,...
Datasheet
ADV7403 on Analog.com
Hi,
I have the following requirements for ADV7403:
I/P Video - STANAG 3350 with Sync On Green as Input to the Chip.
1)720x576i @ 50/25Hz(Class B)video resolution, Interlaced video input,RGB(STANAG Class B)
2)720x480i @ 60/30Hz(Class C)video resolution, Interlaced video input,RGB(STANAG Class C)
O/P Video - 16bit YCbCr 4:2:2 as output from the chip.
Hardware Connections:
We have custom hardware with ADV7403 chip whose input channel configuration for RGsB is given below
Ain1 - G and SOG
Ain2 - B
Ain3 - R
Could you please provide the Script for the above configurations?
Also could you please let me know the values to be set for PRIM_MODE, INSEL, SDM_SEL, and VID_STD for the above configurations?
I want to know how to configure ADV7403 to accept RGsB at Ain1, Ain2, and Ain3? What should be the channel settings for the same?
Waiting for a quick response since it is very critical for us to proceed further.
Thank you.
Hi,
Please refer this configuration script " ##SCART RGB## "(:SCART RGB IN In Thru CP YPrPb 2X1 8Bit 422 Out through Encoder) in that don't use CVBS connection in the AIN pin and follow the remaining configuration w.r.t reference script
SOG register related configuration are provided in ADV7403 manual & adjust the sync slicer to use SOG.
Also use registers 0xC3 & 0XC4 for configuring the AIN1,AIN2,AIN3 and crosscheck this configuration(ADC SWITCH) in Page 277.
Thanks,
Poornima
Hi,
Thank you for your response.
I want to understand, If I use Ain1, Ain2, and Ain3 using C3 and C4 registers, how ADV7403 understands that Ain1 is G, Ain2 is B and Ain3 is R? With the script given, is it possible that the Chip will recognize Ain1 as G, Ain2 as B and Ain3 as R? Is there any specific settings to be done in order to give RGB properly to the chip?
Thank you.
Hi,
(1) "the number of pixels between SAV and EAV should have been 720, where as here it is 1440"
Is there any other register need to be taken care for this ?
Generally we will use the 'PRIM_MODE and VID_STD' registers are setting the free run mode & leave these configuration.
(3) In case of STANAG input :- I am able to get the output 8-bit YCrCb 4:2:2 in Component processor with DDR mode, but my requirement is to work with SDR mode, so I wanted to know whether this is possible or not?
For 8bit 422 SDR mode, Please make sure with below things,
42 6B 83 ; 422 8bit out
42 C9 00 ; SDR mode
42 52 00 ; Colour Space Conversion from RGB->YCrCb
As per CPOP_SEL[0:3] register configuration,if it is 83 then it will be like 16bit output, So for 8 bit output we need to configure the pixel port in below pin assignment.
8-bit out YPrPb=P19-P12/P2-P9.
16-bit out Y= P19-P12
PrPb = P2-P9.
Thanks,
Poornima
Hello,
I tried with this following configuration:-
For 8bit 422 SDR mode,
42 6B 83 ; 422 8bit out
42 C9 00 ; SDR mode
42 52 00 ; Color Space Conversion from RGB->YCrCb
8-bit out:- YPrPb =P19-P12
But ,not able to get the output in the SDR mode
I suspect because of the DDR mode the wordings are not clear because with the initial configuration where i used to get black and white output the output video was clear, only color issue was faced
Any suggestion, where any ADI settings has to be followed for the registers where the output from the decoder is 8-bit YCrCb 422 in SDR mode when the input is STANAG.
Thanks & Regards,
Arpitha
Hi,
We basically have no scripts or support for STANAG 3350 although if you search the forums you will see several threads with suggestions for custom formats. We don't test the format or have any way to test it so what you can find on the forum is all we have to offer for STANAG 3350.
Please note according to specification,we can configure the SDR output in below ways ,
Composite and S-Video pixel data output modes:
- 8-/10-bit ITU-R BT.656 4:2:2 YCrCb with embedded time codes and/or HS, VS
and FIELD.
- 16-/20-bit YCrCb with embedded time codes and/or HS, VS and FIELD.
Component pixel data output modes:
- Single data rate (SDR) 8-/10-bit 4:2:2 YCrCb for 525i and 625i
- SDR 16-/20-bit 4:2:2 YCrCb for all standards
- Double data rate (DDR) 8-/10-bit 4:2:2 YCrCb
- DDR 12-bit 4:4:4 RGB
Thanks,
Poornima
Hello,
Thank you for the support
Following are the observation when done changes with the script:-
(1)When used the script recommended by ADI (from ADV7181C_RGB_SOG.pdf) tried to debug the 8-bit data from the decoder by capturing it in the FPGA with the help of debug probes inside the FPGA, observation was the data is sent from the decoder in SDR mode (in BT.656 format) where, the 0xC9 register was configured to 0x0C (DDR mode)
What is the 8-bit DDR mode LLC frequency?
(2)When the 0xC9 register is configured to 0x00 (SDR mode), the 8-bit data is not sent in BT.656 format
(3)We checked the CP AV control register and CP default color force register and the default color registers to get at-least the free run output, tried with forcing the default color to be blue but at the output we get a combination of all three colors(red, blue and green)
Can you suggest what can be cross checked either register setting or which part of schematic to get proper output
Thanks & Regards,
Arpitha
Hi,
As stated above, SDR 8-/10-bit ITU-R BT.656 4:2:2 YCrCb is only possible when the ADV7181C input is Composite and S-Video.
For blue color output, Please configure the 0xBF(CP DEF COL) register as "0x02".
Thanks,
Poornima
Hello,
Wanted to know what is the 8-bit DDR mode LLC frequency in CP mode?
Thanks & Regards,
Arpitha
Hi,
DDR mode nothing but the pixel output port can be configured in an 8-/10-/12-bit 4:2:2 YCrCb upto a clock rate of 75Mhz (i.e In DDR mode we can support maximum clock rate upto 75MHz.
Please note DDR mode doesn't change the overall performance of the part-- DDR mode maximum would be half the SDR mode maximum. It's really no different than SDR mode-- just half the pixel clock rate since you are getting pixels on each edge instead of every other edge.

Note: DDR mode, a new data value is presented on the positive and the negative edge of the
LLC (line-locked clock) and, hence double the amount of data is transferred.
Thanks,
Poornima
Hello,
Wanted to know what is the DDR mode maximum and SDR mode maximum?
Thanks,
Arpitha
Hi,
ADV7403 pixel clock can run at 140MHZ, but more than that,it will not support
For example if you are in DDR mode the LLC is 1/2 the pixel clock rate i.e If the pixel clock = 140MHz then DDR clock =70MHz
And If you are running 140MHz then you must be in SDR mode not DDR mode. SDR has one pixel per rising edge while DDR has one pixel per rising edge and one pixel per falling edge.
Thanks,
Poornima
Hello,
Thank you for the response.
As it is for ADV7403, it should same for ADV7181C, correct ?
DDR mode maximum and SDR mode maximum means the maximum clock supported by the chip in SDR and DDR mode
So for 8-bit of pixel data, if SDR mode the pixel clock is 27MHz then in DDR mode it is 13.5MHz
Thanks,
Arpitha
Hello,
Thank you for the response.
As it is for ADV7403, it should same for ADV7181C, correct ?
DDR mode maximum and SDR mode maximum means the maximum clock supported by the chip in SDR and DDR mode
So for 8-bit of pixel data, if SDR mode the pixel clock is 27MHz then in DDR mode it is 13.5MHz
Thanks,
Arpitha
Hi,
As it is for ADV7403, it should same for ADV7181C, correct ?
YES, but pixel clock(LLC) will vary between ADV7403 & ADV7181C.
So for 8-bit of pixel data, if SDR mode the pixel clock is 27MHz then in DDR mode it is 13.5MHz
YES.
Thanks,
Poornima
Hello
Understood. Thank you
But according to our observation with respect to the ADV7181C chipset, when we configure the 0xC9 register to DDR mode and probe the LLC clock it shows 27MHz only, where as it should have been13.5MHz,
Can you suggest why is this observation?
Thanks,
Arpitha
Hi,
Please let us know, whether you have assign the DDR bus pin as per table 51.

Thanks,
Poornima
Hello,
The data bus pin are given from P12 to P19 for 8-bit DDR mode
Attached is the capture of one of the data signal with respect to the LLC clock
Thanks,
Arpitha
Hi,
Please let us know your format (resolution) ?
Thanks,
Poornima
Hello,
Resolution is 720*575 @25i (STANAG RGB 3350B)
Thanks,
Arpitha
Hi,
Please let us know your pixel clock and also your oversampling mode(4x or 2x).
Meanwhile let me check with expert also.
Thanks,
Poornima