Post Go back to editing

ADV7403 register configuration for STANAG 3350 CLASS B/C Video Signals

Hi,


I have the following requirements for ADV7403:


I/P Video - STANAG 3350 with Sync On Green as Input to the Chip.

1)720x576i @ 50/25Hz(Class B)video resolution, Interlaced video input,RGB(STANAG Class B)
2)720x480i @ 60/30Hz(Class C)video resolution, Interlaced video input,RGB(STANAG Class C)

O/P Video - 16bit YCbCr 4:2:2 as output from the chip.

Hardware Connections:
We have custom hardware with ADV7403 chip whose input channel configuration for RGsB is given below

Ain1 - G and SOG
Ain2 - B
Ain3 - R

Could you please provide the Script for the above configurations?

Also could you please let me know the values to be set for PRIM_MODE, INSEL, SDM_SEL, and VID_STD for the above configurations?

I want to know how to configure ADV7403 to accept RGsB at Ain1, Ain2, and Ain3? What should be the channel settings for the same?

Waiting for a quick response since it is very critical for us to proceed further.

Thank you.

Parents
  • Hi,

      Please refer this configuration script  " ##SCART RGB## "(:SCART RGB IN In Thru CP YPrPb 2X1  8Bit 422 Out through Encoder)  in that don't use CVBS connection in the AIN pin and follow the remaining configuration w.r.t reference script

     SOG register related configuration are provided in ADV7403 manual & adjust the sync slicer to use SOG.

     Also use registers 0xC3 & 0XC4 for configuring the AIN1,AIN2,AIN3 and crosscheck this configuration(ADC SWITCH) in Page 277.

    Thanks,

    Poornima

  • Hi,

    Thank you for your response.

    I want to understand, If I use Ain1, Ain2, and Ain3 using C3 and C4 registers, how ADV7403 understands that Ain1 is G, Ain2 is B and Ain3 is R? With the script given, is it possible that the Chip will recognize Ain1 as G, Ain2 as B and Ain3 as R? Is there any specific settings to be done in order to give RGB properly to the chip?

    Thank you.

  • Hi,

     Please let us know, Have you configured the below registers without doing any register configuration.

        Format - 720*576 @625i

    42 05 00 ; Prim_Mode =000b for SD-M
    42 06 0B ; VID_STD=1011 for SD  4x1 625i
    42 1D 47 ; Enable 28MHz Crystal
    42 3A 11 ; Set Latch Clock 01b, Power Down ADC3
    42 3B 81 ; Enable internal Bias
    42 3C 52 ; PLL_QPUMP to 010b
    42 C4 85 ; Manual Muxing - ADC2=AIN5(R)
    42 C3 46 ; Manual Muxing - ADC0=AIN6(G), ADC1=AIN4(B)
    42 52 00 ; Colour Space Conversion from RGB->YCrCb
    42 53 00 ; CSC
    42 54 12 ; CSC
    42 55 90 ; CSC
    42 56 38 ; CSC
    42 57 69 ; CSC
    42 58 48 ; CSC
    42 59 08 ; CSC
    42 5A 00 ; CSC
    42 5B 75 ; CSC
    42 5C 21 ; CSC
    42 5D 00 ; CSC
    42 5E 1A ; CSC
    42 5F B8 ; CSC
    42 60 08 ; CSC
    42 61 00 ; CSC
    42 62 20 ; CSC
    42 63 03 ; CSC
    42 64 D7 ; CSC
    42 65 19 ; CSC
    42 66 48 ; CSC last
    42 67 13 ; DPP Filters
    42 6B C3 ; Select 422 8 bit YPrPb out from CP
    42 73 CF ; Enable Manual Gain and set CH_A gain
    42 74 A3 ; Set CH_A and CH_B Gain - 0FAh
    42 75 E8 ; Set CH_B and CH_C Gain
    42 76 FA ; Set CH_C Gain
    42 7B 06 ; clears the bits CP_DUP_AV and AV_Blank_EN
    42 85 19 ; Turn off SSPD and force SOY. For Eval Board.
    42 86 1B ; Enable stdi_line_count_mode
    42 8F 77 ; FR_LL to 1820 & Enable 28.63MHz LLC
    42 90 1C ; FR_LL to 1820
    42 BF 06 ; Blue Screen Free Run Colour
    42 C0 40 ; default color
    42 C1 F0 ; default color
    42 C2 80 ; Default color
    42 C5 01 ; CP_CLAMP_AVG_FACTOR[1-0] = 00b
    42 C9 0C ; Enable DDR Mode
    42 F3 07 ; Enable Anti Alias Filters on ADC 0,1,2
    42 0E 80 ; ADI Recommended Setting
    42 52 46 ; ADI Recommended Setting
    42 54 00 ; ADI Recommended Setting
    42 F6 3B ; ADI Recommended Setting
    42 0E 00 ; ADI Recommended Setting

    Thanks,

    Poornima

  • Hello,

    Thank you for the script

    Following are the observations:-

    Test case 1:-

    When I configured all the register with same value mentioned in the above script ,except the 0xC9 to 0x00 (because we need it in SDR mode)

    Here the status is CP is in free running mode

    Test case 2:-

    When I configure all the registers as mentioned above I get a colored output (far better then before but not a cleared one), but in this case the chip is configured to DDR mode, where as we need it in SDR mode

    Please find the attached image of the screen output which has to be blue test pattern when no input is connected, but it shows shades of blue and green

    Thanks & Regards,

    Arpitha

  • Hello,

    One observation is with the script shared , the number of pixels between SAV and EAV should have been 720, where as here it is 1440 

    But according to the register configuration of primary mode and video standard, it has to be 720 pixels

    Primary mode :- 0x05 :- 0x00 (SD-M)

    Video Standard :- 0x06 :- 0x0B ( CP processor 720*576 @625i)

    Is there any other register need to be taken care for this

    Thanks & Regards,

    Arpitha

  • Hi,

      Please let us know your Rx & Tx chip in your board.

       Let me clarify few things from your end.

      Please let me know, you are not even getting the freerun output properly?

    If So,Please refer ADV7180 RSD document ADV7180_RSD.pdf  pg 10 section 3.3 for free run mode which is available at ADV7180 Design Support Files
    The writes below force the ADV7180 into free-run mode. The writes must be made in the order shown below and should be performed after an Analog Devices’ recommended script. User Map
           42 0C 37  Force Free-Run mode
           42 00 XX  Force Video Standard1
           42 0D YY  Set Color Output2
    -  Have you tried with general PAL/NTSC input instead of STANAG ?

    Thanks,

    Poornima

  • Hello,

    Thank you for the response

    The RX chip is ADV7181C and the TX chip is ADV7343

    In case of STANAG input and PAL output the free run output is like the one attached in the previous reply

    In case of PAL input and the PAL output , the free run output is attached below

    ...

    Thanks & Regards,

    Arpitha

  • Hi,

      Please note freerun nothing but "Receiver enters free run only when the TMDS clock is not detected or when the detected input format does not match the format indicated by the PRIM_MODE [3:0] and VID_STD [5:0] settings.
       For example, if input video is not present. It controls the default color insertion and causes the receiver to generate a default clock.

     If your facing issue with general PAL input & PAL output, then you need to crosscheck your schematic.

    Thanks,

    Poornima

  • Hello,

    Thank you for the quick response

    Will check and let you know regarding the free running mode

    Would like to know the following information:-

    (1) "the number of pixels between SAV and EAV should have been 720, where as here it is 1440"

    Is there any other register need to be taken care for this ?

    (2) In case of STANAG input, we can observe blur output and more blue color component in the output

    Is this because of CSC registers? or should i need to configure the offset registers for the three channels

    (3) In case of STANAG input :- I am able to get the output 8-bit YCrCb 4:2:2 in Component processor with DDR mode, but my requirement is to work with SDR mode, so I wanted to know whether this is possible or not?

    Thanks & Regards,

    Arpitha

  • Hi,

    (1) "the number of pixels between SAV and EAV should have been 720, where as here it is 1440"

    Is there any other register need to be taken care for this ?

       Generally we will use the 'PRIM_MODE and VID_STD' registers are setting the free run mode & leave these configuration.

    (3) In case of STANAG input :- I am able to get the output 8-bit YCrCb 4:2:2 in Component processor with DDR mode, but my requirement is to work with SDR mode, so I wanted to know whether this is possible or not?

    For 8bit 422 SDR mode, Please make sure with below things,
            42 6B 83 ; 422 8bit out
            42 C9 00 ; SDR mode
            42 52 00 ; Colour Space Conversion from RGB->YCrCb
    As per CPOP_SEL[0:3] register configuration,if it is 83 then it will be like 16bit output, So for 8 bit output we need to configure the pixel port in below pin assignment.

       8-bit  out       YPrPb=P19-P12/P2-P9.
      16-bit out       Y= P19-P12
                              PrPb = P2-P9.

    Thanks,

    Poornima

  • Hello,

    I tried with this following configuration:-

    For 8bit 422 SDR mode,
            42 6B 83 ; 422 8bit out
            42 C9 00 ; SDR mode
            42 52 00 ; Color Space Conversion from RGB->YCrCb

     8-bit  out:- YPrPb =P19-P12

    But ,not able to get the output in the SDR mode

    I suspect because of the DDR mode the wordings are not clear because with the initial configuration where i used to get black and white output the output video was clear, only color issue was faced

    Any suggestion, where any ADI settings has to be followed for the registers where the output from the decoder is 8-bit YCrCb 422 in SDR mode when the input is STANAG.

    Thanks & Regards,

    Arpitha

  • Hi,

      We basically have no scripts or support for STANAG 3350 although if you search the forums you will see several threads with suggestions for custom formats. We don't test the format or have any way to test it so what you can find on the forum is all we have to offer for STANAG 3350.

     Please note according to specification,we can configure the SDR output in below ways ,

    Composite and S-Video pixel data output modes:
       - 8-/10-bit ITU-R BT.656 4:2:2 YCrCb with embedded time codes and/or HS, VS
    and FIELD.
      - 16-/20-bit YCrCb with embedded time codes and/or HS, VS and FIELD.

    Component pixel data output modes:
    - Single data rate (SDR) 8-/10-bit 4:2:2 YCrCb for 525i and 625i
    - SDR 16-/20-bit 4:2:2 YCrCb for all standards
    - Double data rate (DDR) 8-/10-bit 4:2:2 YCrCb
    - DDR 12-bit 4:4:4 RGB

    Thanks,

    Poornima

Reply
  • Hi,

      We basically have no scripts or support for STANAG 3350 although if you search the forums you will see several threads with suggestions for custom formats. We don't test the format or have any way to test it so what you can find on the forum is all we have to offer for STANAG 3350.

     Please note according to specification,we can configure the SDR output in below ways ,

    Composite and S-Video pixel data output modes:
       - 8-/10-bit ITU-R BT.656 4:2:2 YCrCb with embedded time codes and/or HS, VS
    and FIELD.
      - 16-/20-bit YCrCb with embedded time codes and/or HS, VS and FIELD.

    Component pixel data output modes:
    - Single data rate (SDR) 8-/10-bit 4:2:2 YCrCb for 525i and 625i
    - SDR 16-/20-bit 4:2:2 YCrCb for all standards
    - Double data rate (DDR) 8-/10-bit 4:2:2 YCrCb
    - DDR 12-bit 4:4:4 RGB

    Thanks,

    Poornima

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.