KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADV7403
Production
The ADV7403 is a high quality, single chip, multiformat video decoder and graphics digitizer. This multiformat decoder supports the conversion of PAL,...
Datasheet
ADV7403 on Analog.com
Hi,
I have the following requirements for ADV7403:
I/P Video - STANAG 3350 with Sync On Green as Input to the Chip.
1)720x576i @ 50/25Hz(Class B)video resolution, Interlaced video input,RGB(STANAG Class B)
2)720x480i @ 60/30Hz(Class C)video resolution, Interlaced video input,RGB(STANAG Class C)
O/P Video - 16bit YCbCr 4:2:2 as output from the chip.
Hardware Connections:
We have custom hardware with ADV7403 chip whose input channel configuration for RGsB is given below
Ain1 - G and SOG
Ain2 - B
Ain3 - R
Could you please provide the Script for the above configurations?
Also could you please let me know the values to be set for PRIM_MODE, INSEL, SDM_SEL, and VID_STD for the above configurations?
I want to know how to configure ADV7403 to accept RGsB at Ain1, Ain2, and Ain3? What should be the channel settings for the same?
Waiting for a quick response since it is very critical for us to proceed further.
Thank you.
Hi,
Please refer this configuration script " ##SCART RGB## "(:SCART RGB IN In Thru CP YPrPb 2X1 8Bit 422 Out through Encoder) in that don't use CVBS connection in the AIN pin and follow the remaining configuration w.r.t reference script
SOG register related configuration are provided in ADV7403 manual & adjust the sync slicer to use SOG.
Also use registers 0xC3 & 0XC4 for configuring the AIN1,AIN2,AIN3 and crosscheck this configuration(ADC SWITCH) in Page 277.
Thanks,
Poornima
Hi,
Thank you for your response.
I want to understand, If I use Ain1, Ain2, and Ain3 using C3 and C4 registers, how ADV7403 understands that Ain1 is G, Ain2 is B and Ain3 is R? With the script given, is it possible that the Chip will recognize Ain1 as G, Ain2 as B and Ain3 as R? Is there any specific settings to be done in order to give RGB properly to the chip?
Thank you.
Hi,
Please configure the CSC registers as like below configuration,
0x52 0x00 Conversion from RGB -> YPbPr
0x53 0x00 CSC Start
0x54 0x07 CSC Register
0x55 0x0C CSC Register
0x56 0x99 CSC Register
0x57 0xA9 CSC Register
0x58 0x71 CSC Register
0x59 0x08 CSC Register
0x5A 0x00 CSC Register
0x5B 0x20 CSC Register
0x5C 0xA7 CSC Register
0x5D 0xA9 CSC Register
0x5E 0x1A CSC Register
0x5F 0x8F CSC Register
0x60 0x08 CSC Register
0x61 0x00 CSC Register
0x62 0x7A CSC Register
0x63 0xE1 CSC Register
0x64 0x05 CSC Register
0x65 0x39 CSC Register
0x66 0x1F CSC last
0x73 0xD0 Enable Manual Gain and set CH_A gain
0x74 0x04 Set CH_A and CH_B Gain
0x75 0x01 Set CH_B and CH_C Gain
0x76 0x00 Set CH_C Gain
Thanks,
Poornima
Hello Poornima,
Thank you for your reply.
Tried configuring the given CSC register settings along with other registers mentioned in the previous mail, but the colours are not proper as in the below image.

There is colour swapping as you can see in the above image.
Thank you.
Hi,
Please try configuring the 0X74 ,0X75 ,0X76 ,0X77 ,0X78,0X79 , 0X7A registers as once & it seems you have been configured these registers as twice.
Also try to swap the Cr,Cb by using register "SWPC Swap Pixel Cr/Cb (SDP), Address 0x27[7]" & let us know.

Thanks,
Poornima
Hello,
Can I use the same CSC configuration for ADV7181C
Thanks,
Arpitha
Hi,
Yes, you can use the CSC configuration register which we shared above and just swap the pixel by using "SWPC Swap Pixel Cr/Cb (SDP), Address 0x27[7]"
Thanks,
Poornima
Hello,
I tried with the same configuration by swapping the pixel as well ,but in my case, the input is STANAG (ADV7181C) and output is PAL/STANAG resolution from (ADV7343 IC)
When PAL input and PAL output implementation is done, the output is as expected
When STANAG input and PAL/STANAG output implementation is done ,the output video observed is black and white.
One more observation is , when the register 0x54 is configured to value 0x07 or 0x12, there is no output observed
Could you please let me know what other registers has to be taken care in case of Stanag input
Thanks & Regards,
Arpitha
Hi,
Please make sure with STANAG3350 input like, "whether STANAG3350 video is supplied as a component RGB signal & then according to that configure the PRIM_MODE[3:0] (0x05) & VID_STD[3:0] (0x06) registers.
42 05 01 ; PRIM_MODE = 001b COMP - "using component input, we can send either YPbPr or analog RGB".
Also it require by changing the PLL settings (or clamping) to sample all pixels & refer below snap for PLL recommended settings.
http://www.analog.com/static/imported-files/application_notes/AN-0978.pdf

Thanks,
Poornima
Hello
Thank you for your response
The STANAG input to the decoder is through the following signals:-
Ain4 - B
Ain5 - R
Ain6 - G
STANAG 3350B resolution:- 720*575 @25i
Output format from the decoder :- 8bit YCrCb 422 in BT.656 format
8-bit out :- YCrCb :- P19-P12 pins are connected
According to the input , I have configured the ADC switch registers and the PLL settings as described in the AN-0978 pdf
Output image:- Black and white with patches of pink, green and blue colors and it varies
Issues:-
(1) When the primary mode register is configured to PRIM_MODE = 001b, the output is blank with green-pink color at the bottom of the display
(2) When the VID_STD register set is configured, no output display is observed
As mentioned in the manual "The CP circuitry is activated under the control of PRIM_MODE[3:0] and VID_STD[3:0]" but i am not able to configure these two registers,
I have attached the registers configured for ADV7181C IC, Could you please check those register configuration and let us know which register has to be changed or to be added
{0x42, 0X00, 0X09},//YPrPb component
{0x42,0x01,0xC8},//video selection
{0x42,0x02,0x04},//reserved
{0x42, 0x3C, 0x5B},//sog AND pll(>22)
{0x42, 0X04, 0X45},//extended op control
{0x42, 0X1D, 0X47},//Enable 28MHz Crystal
{0x42, 0X27, 0X98},//Swap Cr & Cb & YC Delay Correction
{0x42, 0X6B, 0XC3},// 422 8bit out and DE and field selection
{0x42, 0XC9, 0X00},// SDR mode
{0x42, 0X31, 0X02},//Clears NEWAV_MODE, SAV/EAV to suit ADV video encoders
{0x42, 0X3A, 0X10},//set latch clock settings to 001b
{0x42, 0X3B, 0X81},//Enable internal Bias
{0x42, 0X86, 0X0B},//[4]:- Swap Cr and Cb
{0x42, 0XC3, 0X56},//ADC 0 and ADc 1
{0x42, 0XC4, 0XB5},//ADC3
{0x42, 0XF3, 0X07},// Enable Anti Alias Filters on ADC 0,1,2
{0x42, 0XF9, 0X03},//VS Mode Control
{0x42, 0X0E, 0X80},//ADI Recommended Setting
{0x42, 0X52, 0X00},
{0x42, 0X53, 0X00},
{0x42, 0X54, 0X00},
{0x42, 0X55, 0x0C},
{0x42, 0X56, 0X99},
{0x42, 0X57, 0X69},
{0x42, 0X58, 0X71},
{0x42, 0X59, 0X08},
{0x42, 0X5A, 0X00},
{0x42, 0X5B, 0X20},
{0x42, 0X5C, 0XA7},
{0x42, 0X5D, 0XA9},
{0x42, 0X5E, 0X1A},
{0x42, 0X5F, 0X8F},
{0x42, 0X60, 0X08},
{0x42, 0X61, 0X00},
{0x42, 0X62, 0X7A},
{0x42, 0X63, 0XE1},
{0x42, 0X64, 0X05},
{0x42, 0X65, 0X19},//0x39
{0x42, 0X66, 0X1F},
{0x42, 0X67, 0X13},
{0x42, 0X68, 0X01},
{0x42, 0X73, 0XD0},//Enable Manual Gain and set CH_A gain
{0x42, 0X74, 0X04},//Set CH_A and CH_B Gain
{0x42, 0X75, 0X01},//Set CH_B and CH_C Gain
{0x42, 0X76, 0X00},//Set CH_C Gain
{0x42, 0x77, 0xFF},
{0x42, 0x78, 0xFF},
{0x42, 0x79, 0xFF},
{0x42, 0x7A, 0xFF},
{0x42, 0X0B, 0X00},//ADV7181C Hue register
{0x42, 0X08, 0X80},//ADV7181C contrast register
{0x42, 0X0A, 0X80},//ADV7181C Brightness Adjust
{0x42, 0x84, 0x0C},//No Filtering
{0x42, 0x85, 0x18},//Autodetect mode for sync source
{0x42, 0x87, 0xE6},//CP TLLC CONTROL 1//20
{0x42, 0x88, 0xC0},//CP TLLC CONTROL 2//for 27MHz (PLL divisor is 1728)
{0x42, 0x89, 0x08},//inversion of Cb and Cr in SDp mode
{0x42, 0x8A, 0x10},//VCO range
{0x42, 0x8F, 0x02},// Set FR_LL = 720
{0x42, 0X90, 0XD0},// Set FR_LL = 720
{0x42, 0X7F, 0XFF},//brightness
{0x42, 0X91, 0X50},//DPP_CP_64
{0x42, 0X0E, 0X00},//ADI Recommended Setting
{0x42, 0X0E, 0X00},//ADI Recommended Setting
Thanks & Regards,
Arpitha
Hello,
When we tapped the 8-bit output signal from the decoder, what we observed is irrespective of any color test pattern input to the decoder, the values of Y,Cb,Cr will be in the range of white ,black, grey color values
which is the reason why we get the black and white output, which indicates CSC is not enabled in the decoder
Request you to go through the configuration script attached in the above reply and please let us know soon if there is any mistake in the configuration
Thanks & Regards
Arpitha
Hi,
Please refer below comments,
1.Please remove INSEL configuration(i.e 0x00) register. The settings of INSEL and the manual input muxing registers (ADC0/1/2/3_SW) are contradict to each other, so when ADC0/1/2/3_sw settings are used we can ignore the INSEL configuration.
Please configure AIN 4,5,6 as like below
42 C3 46 ; ADC1 to Ain4, ADC0 to Ain6,
42 C4 B5 ; ADC2 to Ain5
or
42 C3 56 ; ADC1 to Ain5, ADC0 to Ain6,
42 C4 B4 ; ADC2 to Ain4
2. Please configure the CSC register as like below
42 52 00 ; Colour Space Conversion from RGB->YCrCb
42 53 00 ; CSC
42 54 12 ; CSC
42 55 90 ; CSC
42 56 38 ; CSC
42 57 69 ; CSC
42 58 48 ; CSC
42 59 08 ; CSC
42 5A 00 ; CSC
42 5B 75 ; CSC
42 5C 21 ; CSC
42 5D 00 ; CSC
42 5E 1A ; CSC
42 5F B8 ; CSC
42 60 08 ; CSC
42 61 00 ; CSC
42 62 20 ; CSC
42 63 03 ; CSC
42 64 D7 ; CSC
42 65 19 ; CSC
42 66 48 ; CSC last
42 67 13 ; DPP Filters
3. Please configure the PRIM_MODE and VID_STD to the nearest available standard to correctly configure the internal parameters of the CP core to decode the specific SD/HD/GR and Interlace/Progressive standard.
4. Please remove below configuration.
{0x42, 0X0B, 0X00},//ADV7181C Hue register
{0x42, 0X08, 0X80},//ADV7181C contrast register
{0x42, 0X0A, 0X80},//ADV7181C Brightness
Thanks,
Poornima
Hi,
Please refer below comments,
1.Please remove INSEL configuration(i.e 0x00) register. The settings of INSEL and the manual input muxing registers (ADC0/1/2/3_SW) are contradict to each other, so when ADC0/1/2/3_sw settings are used we can ignore the INSEL configuration.
Please configure AIN 4,5,6 as like below
42 C3 46 ; ADC1 to Ain4, ADC0 to Ain6,
42 C4 B5 ; ADC2 to Ain5
or
42 C3 56 ; ADC1 to Ain5, ADC0 to Ain6,
42 C4 B4 ; ADC2 to Ain4
2. Please configure the CSC register as like below
42 52 00 ; Colour Space Conversion from RGB->YCrCb
42 53 00 ; CSC
42 54 12 ; CSC
42 55 90 ; CSC
42 56 38 ; CSC
42 57 69 ; CSC
42 58 48 ; CSC
42 59 08 ; CSC
42 5A 00 ; CSC
42 5B 75 ; CSC
42 5C 21 ; CSC
42 5D 00 ; CSC
42 5E 1A ; CSC
42 5F B8 ; CSC
42 60 08 ; CSC
42 61 00 ; CSC
42 62 20 ; CSC
42 63 03 ; CSC
42 64 D7 ; CSC
42 65 19 ; CSC
42 66 48 ; CSC last
42 67 13 ; DPP Filters
3. Please configure the PRIM_MODE and VID_STD to the nearest available standard to correctly configure the internal parameters of the CP core to decode the specific SD/HD/GR and Interlace/Progressive standard.
4. Please remove below configuration.
{0x42, 0X0B, 0X00},//ADV7181C Hue register
{0x42, 0X08, 0X80},//ADV7181C contrast register
{0x42, 0X0A, 0X80},//ADV7181C Brightness
Thanks,
Poornima
Hello,
Thank you for the response.
I followed the comments shared by you.
observation is:-
Green test pattern is observed in the display (when 0x05 = 0x01 and 0x06 = 0x02/0x00)
when the registers are updated the Status register 0x12 is read, the value is 0xC0, which indicates CP free running is enabled,
In our case the STANAG input is 720 * 575 @25i RGB so according to the manual we need to configure the 0x05= 0x02, which fails to work
Updated register configuration is attached, could you please check it once again whether the required registers are configured or is there any sequence of the register configuration to be followed ,like is there any sequence mismatch in the registers configured.
Thanks & Regards,
Arpitha
{0x42,0x01,0xC8},//video selection
{0x42,0x02,0x04},//reserved
{0x42,0X04,0X45},//extended op control
{0x42,0x05,0x01},//YPrPb component
{0x42,0x06,0x02},//YPrPb component
{0x42,0x0C,0x36},
{0x42,0x0D,0x7C},
{0x42, 0X1D, 0X47},//Enable 28MHz Crystal
{0x42, 0X27, 0X98},//Swap Cr & Cb & YC Delay Correction
{0x42, 0X31, 0X02},//Clears NEWAV_MODE, SAV/EAV to suit ADV video encoders
{0x42, 0X3A, 0X10},//set latch clock settings to 001b
{0x42, 0X3B, 0X81},//Enable internal Bias
{0x42, 0x3C, 0x5B},//sog AND pll(>22)
{0x42, 0XF3, 0X07},// Enable Anti Alias Filters on ADC 0,1,2
{0x42, 0XF9, 0X03},//VS Mode Control
{0x42, 0X0E, 0X80},//ADI Recommended Setting
{0x42, 0X52, 0X00},
{0x42, 0X53, 0X00},
{0x42, 0X54, 0X12},
{0x42, 0X55, 0x90},
{0x42, 0X56, 0X38},
{0x42, 0X57, 0X69},
{0x42, 0X58, 0X48},
{0x42, 0X59, 0X08},
{0x42, 0X5A, 0X00},
{0x42, 0X5B, 0X75},
{0x42, 0X5C, 0X21},
{0x42, 0X5D, 0X00},
{0x42, 0X5E, 0X1A},
{0x42, 0X60, 0X08},
{0x42, 0X61, 0X00},
{0x42, 0X62, 0X20},
{0x42, 0X63, 0X03},
{0x42, 0X64, 0XD7},
{0x42, 0X65, 0X19},//0x39
{0x42, 0X66, 0X48},
{0x42, 0X67, 0X13},//DPP Filters
{0x42, 0X68, 0X01},//automatic selection od DOO_FILT
{0x42, 0X69, 0XA0},//
{0x42, 0X6B, 0XC3},// 422 8bit out and DE and field selection
{0x42, 0X73, 0XD0},//Enable Manual Gain and set CH_A gain
{0x42, 0X74, 0X04},//Set CH_A and CH_B Gain
{0x42, 0X75, 0X01},//Set CH_B and CH_C Gain
{0x42, 0X76, 0X00},//Set CH_C Gain
{0x42, 0x77, 0x00},
{0x42, 0x78, 0x08},
{0x42, 0x79, 0xAE},
{0x42, 0x7A, 0x0F},
{0x42, 0x84, 0x0C},//No Filtering
{0x42, 0x85, 0x18},//Autodetect mode for sync source
{0x42, 0X86, 0X0B},//[4]:- Swap Cr and Cb
{0x42, 0x87, 0xE6},//CP TLLC CONTROL 1//20
{0x42, 0x88, 0xC0},//CP TLLC CONTROL 2//for 27MHz (PLL divisor is 1728)
{0x42, 0x89, 0x08},//inversion of Cb and Cr in SDp mode
{0x42, 0x8A, 0x10},//VCO range
{0x42, 0x8F, 0x02},// Set FR_LL = 720
{0x42, 0X90, 0XD0},// Set FR_LL = 720
{0x42, 0X7F, 0XFF},//brightness
{0x42, 0X91, 0X50},//DPP_CP_64
{0x42, 0X0E, 0X00},//ADI Recommended Setting
{0x42, 0xBE, 0xE0},
{0x42, 0XC3, 0X56},
{0x42, 0XC4, 0XB4},//ADC3
{0x42, 0XC9, 0X00},// SDR modeHello,
I configured the primary mode and video standard registers, according to the value specified in the ADV7181Cmanual,
Primary mode :- 0x05 :- 0x00 (SD-M)
Video Standard :- 0x06 :- 0x0B ( CP processor 720*576 @625i)
Observation is whenever the video standard is configured, the status is CP free running mode ( verified by reading 0x12 register i.e. 0x12 = 0xC0)
When the LLC clock is probed it is 27MHz,
Request you to please let me know soon is there any registers need to be taken care or is there any mismatch in the I2C sequence
Thanks & Regards,
Arpitha
Hello,
I changed some of the register set configuration, and with the script attached here, The valid signal is detected and the status is 0x80 when 0x12 register is read
Output observation is overlay of green and pink color.
Is this overlay because of some CSC registers or is it because of the settings on primary mode and video standard?
{0x42, 0x01, 0xC8},//video selection
{0x42, 0x02, 0x04},//reserved
{0x42, 0X04, 0X45},//extended op control
{0x42, 0x05, 0x01},//YPrPb component
{0x42, 0x06, 0x01},//YPrPb component//1440
{0x42, 0x13, 0x04},
{0x42, 0x0C, 0x36},
{0x42, 0X0E, 0X00},
{0x42, 0X1D, 0X47},//Enable 28MHz Crystal
{0x42, 0X27, 0X58},//Swap Cr & Cb & YC Delay Correction
{0x42, 0X31, 0X02},//Clears NEWAV_MODE, SAV/EAV to suit ADV video encoders
{0x42, 0X3A, 0X11},//set latch clock settings to 001b
{0x42, 0X3B, 0X85},//Enable internal Bias//81
{0x42, 0x3C, 0x5B},//sog AND pll(>22)
{0x42, 0XC3, 0X56},
{0x42, 0XC4, 0XB4},//ADC3
{0x42, 0XF3, 0X07},// Enable Anti Alias Filters on ADC 0,1,2
{0x42, 0XF9, 0X03},//VS Mode Control
{0x42, 0X52, 0X00},
{0x42, 0X53, 0X00},
{0x42, 0X54, 0X12},
{0x42, 0X55, 0x90},
{0x42, 0X56, 0X38},
{0x42, 0X57, 0X69},
{0x42, 0X58, 0X48},
{0x42, 0X59, 0X08},
{0x42, 0X5A, 0X00},
{0x42, 0X5B, 0X75},
{0x42, 0X5C, 0X21},
{0x42, 0X5D, 0X00},
{0x42, 0X5E, 0X1A},
{0x42, 0x5F, 0xB8},//
{0x42, 0X60, 0X08},
{0x42, 0X61, 0X00},
{0x42, 0X62, 0X20},
{0x42, 0X63, 0X03},
{0x42, 0X64, 0XD7},
{0x42, 0X65, 0X19},//0x39
{0x42, 0X66, 0X48},
{0x42, 0X67, 0X13},//DPP Filters
{0x42, 0X68, 0X01},//automatic selection od DOO_FILT
{0x42, 0X69, 0X00},//
{0x42, 0X6A, 0X00},
{0x42, 0X6B, 0XC3},// 422 8bit out and DE and field selection
{0x42, 0X73, 0XD0},//Enable Manual Gain and set CH_A gain
{0x42, 0X74, 0X04},//Set CH_A and CH_B Gain
{0x42, 0X75, 0X01},//Set CH_B and CH_C Gain
{0x42, 0X76, 0X00},//Set CH_C Gain
{0x42, 0x77, 0x02},
{0x42, 0x78, 0x08},
{0x42, 0x79, 0x02},
{0x42, 0x7A, 0x00},
{0x42, 0X7B, 0X1F},
{0x42, 0X7D, 0X8C},
{0x42, 0X7E, 0X8C},
{0x42, 0X7F, 0XFF},//brightness
{0x42, 0X86, 0X0B},//[4]:- Swap Cr and Cb
{0x42, 0XF3, 0X07},// Enable Anti Alias Filters on ADC 0,1,2
{0x42, 0XF4, 0X3F},
{0x42, 0XF9, 0X03},//VS Mode Control
{0x42, 0XF4, 0X1D},
{0x42, 0x89, 0x08},//inversion of Cb and Cr in SDp mode
{0x42, 0x8A, 0x10},//VCO range
{0x42, 0x8F, 0x00},// Set FR_LL = 720
{0x42, 0X90, 0X00},// Set FR_LL = 720
Thanks & Regards
Arpitha
Hi,
Please let us know, Have you configured the below registers without doing any register configuration.
Format - 720*576 @625i
42 05 00 ; Prim_Mode =000b for SD-M
42 06 0B ; VID_STD=1011 for SD 4x1 625i
42 1D 47 ; Enable 28MHz Crystal
42 3A 11 ; Set Latch Clock 01b, Power Down ADC3
42 3B 81 ; Enable internal Bias
42 3C 52 ; PLL_QPUMP to 010b
42 C4 85 ; Manual Muxing - ADC2=AIN5(R)
42 C3 46 ; Manual Muxing - ADC0=AIN6(G), ADC1=AIN4(B)
42 52 00 ; Colour Space Conversion from RGB->YCrCb
42 53 00 ; CSC
42 54 12 ; CSC
42 55 90 ; CSC
42 56 38 ; CSC
42 57 69 ; CSC
42 58 48 ; CSC
42 59 08 ; CSC
42 5A 00 ; CSC
42 5B 75 ; CSC
42 5C 21 ; CSC
42 5D 00 ; CSC
42 5E 1A ; CSC
42 5F B8 ; CSC
42 60 08 ; CSC
42 61 00 ; CSC
42 62 20 ; CSC
42 63 03 ; CSC
42 64 D7 ; CSC
42 65 19 ; CSC
42 66 48 ; CSC last
42 67 13 ; DPP Filters
42 6B C3 ; Select 422 8 bit YPrPb out from CP
42 73 CF ; Enable Manual Gain and set CH_A gain
42 74 A3 ; Set CH_A and CH_B Gain - 0FAh
42 75 E8 ; Set CH_B and CH_C Gain
42 76 FA ; Set CH_C Gain
42 7B 06 ; clears the bits CP_DUP_AV and AV_Blank_EN
42 85 19 ; Turn off SSPD and force SOY. For Eval Board.
42 86 1B ; Enable stdi_line_count_mode
42 8F 77 ; FR_LL to 1820 & Enable 28.63MHz LLC
42 90 1C ; FR_LL to 1820
42 BF 06 ; Blue Screen Free Run Colour
42 C0 40 ; default color
42 C1 F0 ; default color
42 C2 80 ; Default color
42 C5 01 ; CP_CLAMP_AVG_FACTOR[1-0] = 00b
42 C9 0C ; Enable DDR Mode
42 F3 07 ; Enable Anti Alias Filters on ADC 0,1,2
42 0E 80 ; ADI Recommended Setting
42 52 46 ; ADI Recommended Setting
42 54 00 ; ADI Recommended Setting
42 F6 3B ; ADI Recommended Setting
42 0E 00 ; ADI Recommended Setting
Thanks,
Poornima
Hello,
Thank you for the script
Following are the observations:-
Test case 1:-
When I configured all the register with same value mentioned in the above script ,except the 0xC9 to 0x00 (because we need it in SDR mode)
Here the status is CP is in free running mode
Test case 2:-
When I configure all the registers as mentioned above I get a colored output (far better then before but not a cleared one), but in this case the chip is configured to DDR mode, where as we need it in SDR mode
Please find the attached image of the screen output which has to be blue test pattern when no input is connected, but it shows shades of blue and green
Thanks & Regards,
Arpitha
Hello,
One observation is with the script shared , the number of pixels between SAV and EAV should have been 720, where as here it is 1440
But according to the register configuration of primary mode and video standard, it has to be 720 pixels
Primary mode :- 0x05 :- 0x00 (SD-M)
Video Standard :- 0x06 :- 0x0B ( CP processor 720*576 @625i)
Is there any other register need to be taken care for this
Thanks & Regards,
Arpitha
Hi,
Please let us know your Rx & Tx chip in your board.
Let me clarify few things from your end.
Please let me know, you are not even getting the freerun output properly?
If So,Please refer ADV7180 RSD document ADV7180_RSD.pdf pg 10 section 3.3 for free run mode which is available at ADV7180 Design Support Files
The writes below force the ADV7180 into free-run mode. The writes must be made in the order shown below and should be performed after an Analog Devices’ recommended script. User Map
42 0C 37 Force Free-Run mode
42 00 XX Force Video Standard1
42 0D YY Set Color Output2
- Have you tried with general PAL/NTSC input instead of STANAG ?
Thanks,
Poornima
Hello,
Thank you for the response
The RX chip is ADV7181C and the TX chip is ADV7343
In case of STANAG input and PAL output the free run output is like the one attached in the previous reply
In case of PAL input and the PAL output , the free run output is attached below
...
Thanks & Regards,
Arpitha
Hi,
Please note freerun nothing but "Receiver enters free run only when the TMDS clock is not detected or when the detected input format does not match the format indicated by the PRIM_MODE [3:0] and VID_STD [5:0] settings.
For example, if input video is not present. It controls the default color insertion and causes the receiver to generate a default clock.
If your facing issue with general PAL input & PAL output, then you need to crosscheck your schematic.
Thanks,
Poornima
Hello,
Thank you for the quick response
Will check and let you know regarding the free running mode
Would like to know the following information:-
(1) "the number of pixels between SAV and EAV should have been 720, where as here it is 1440"
Is there any other register need to be taken care for this ?
(2) In case of STANAG input, we can observe blur output and more blue color component in the output
Is this because of CSC registers? or should i need to configure the offset registers for the three channels
(3) In case of STANAG input :- I am able to get the output 8-bit YCrCb 4:2:2 in Component processor with DDR mode, but my requirement is to work with SDR mode, so I wanted to know whether this is possible or not?
Thanks & Regards,
Arpitha