Post Go back to editing

EVAL-ADV7341EBZ Kit Usage Only Encoder

Hi,

I want to use ADV7343 in my design, I saw EVAL-ADV7341EBZ kit for ADV734X series.

Firstly ADV7343 8-bit but demo board encoder is 10-bit for this reason can I use EVAL-ADV7341EBZ for 8-bit input mode.

Second I want to feed encoder with my digital data (for example from FPGA), Can I disable two decoder on demo board and use pin header for feeding DAC?

Thank for reply.

Best Regard.

Parents Reply
  • Hi,

       Can you please check with FAE(Sales Person) about ADV7343 demo kit.

       Its also possible to validate the ADV7343 using internal test pattern generation & some customers have used these color bars as a test pattern to test their system design. Please refer Page81 in ADV7343 datasheet

       Please make sure with below things for internal test pattern generation,
           SD Test Pattern- 27Mhz clock signal must be applied to the CLKIN pin.
           ED Test Pattern- 27Mhz clock signal must be applied to the CLKIN pin.
           HD Test Pattern- 74.25MHz clock signal must be applied to the CLKIN pin.

    Thanks,

    Poornima

Children