Hello,
I am using ADV7401 for decoding CVBS Input. I am facing an issue with NTSC and PAL Video outputs from the Chip. I was able to measure the Number of Pixels and Number of Lines of output coming out of the ADV7401 Chip.
In case of NTSC, I am getting 720 pixels and 253 lines instead of 240. The output is shifted downwards on the monitor.
In case of PAL , I am getting 720 pixels and 288 lines. Here the output is moving up and down slightly.
Here are the Register Configuration of ADV7401,
Slave Address, Reg Address, Data - This is the format used below
{ 0x42, 0x0F, 0x80 }, //soft reset
{ 0x42, 0x01, 0xC8 }, //Square Pixel is disabled
{ 0x42, 0x00, 0x0E }, // CVBS Ain10
{ 0x42, 0x03, 0x0C }, // 8 Bit Mode
{ 0x42, 0x17, 0x41 }, // select SH1
{ 0x42, 0x1D, 0x47 }, // Enable 28MHz Crystal
{ 0x42, 0x31, 0x02 }, // Clears NEWAV_MODE, SAV/EAV to suit ADV video encoders
{ 0x42, 0x3A, 0x10 }, // Set Latch Clock & Power UP ADC 1 & ADC2 & ADC3& ADC4
{ 0x42, 0x3B, 0x80 }, // Enable External Bias
{ 0x42, 0x3D, 0xA2 }, // MWE Enable Manual Window, Colour Kill Threshold to 2
{ 0x42, 0x3E, 0x6A }, // BLM optimisation
{ 0x42, 0x3F, 0xA0 }, // BGB
{ 0x42, 0x67, 0x01 }, // Format 422
{ 0x42, 0x73, 0xD0 }, // Manual Gain Channels A,B,C
{ 0x42, 0x74, 0x04 }, // Manual Gain Channels A,B,C
{ 0x42, 0x75, 0x01 }, // Manual Gain Channels A,B,C
{ 0x42, 0x76, 0x00 }, // Manual Gain Channels A,B,C
{ 0x42, 0x77, 0x04 }, // Manual Offsets A to 64d & B,C to 512
{ 0x42, 0x78, 0x08 }, // Manual Offsets A to 64d & B,C to 512
{ 0x42, 0x79, 0x02 }, // Manual Offsets A to 64d & B,C to 512
{ 0x42, 0x7A, 0x00 }, // Manual Offsets A to 64d & B,C to 512
{ 0x42, 0x86, 0x0B }, // Enable stdi_line_count_mode
{ 0x42, 0xC5, 0x00 }, // Clamp Mode 0 for FB hc based
{ 0x42, 0xED, 0x12 }, // FB_CAP_RES,Enable Dynamic Fast Blank Mode
{ 0x42, 0xF3, 0x0F }, // Enable Anti Alias Filter on all ADCs
{ 0x42, 0x0E, 0x80 }, // ADI Recommended Setting
{ 0x42, 0x49, 0x01 }, // ADI Recommended Setting
{ 0x42, 0x52, 0x46 }, // ADI Recommended Setting
{ 0x42, 0x54, 0x00 }, // ADI Recommended Setting
{ 0x42, 0x7F, 0xFF }, // ADI Recommended Setting
{ 0x42, 0x81, 0x30 }, // ADI Recommended Setting
{ 0x42, 0x90, 0xC9 }, // ADI Recommended Setting
{ 0x42, 0x91, 0x40 }, // ADI Recommended Setting
{ 0x42, 0x92, 0x3C }, // ADI Recommended Setting
{ 0x42, 0x93, 0xCA }, // ADI Recommended Setting
{ 0x42, 0x94, 0xD5 }, // ADI Recommended Setting
{ 0x42, 0xB6, 0x08 }, // ADI Recommended Setting
{ 0x42, 0xC0, 0x9A }, // ADI Recommended Setting
{ 0x42, 0xCF, 0x50 }, // ADI Recommended Setting
{ 0x42, 0xD0, 0x4E }, // ADI Recommended Setting
{ 0x42, 0xD1, 0xB9 }, // ADI Recommended Setting
{ 0x42, 0xD6, 0xDD }, // ADI Recommended Setting
{ 0x42, 0xD7, 0xE2 }, // ADI Recommended Setting
{ 0x42, 0xE5, 0x51 }, // ADI Recommended Setting
{ 0x42, 0x0E, 0x00 }, // ADI Recommended Setting
{ 0x42, 0x0C, 0xE2 }, // changing input color
{ 0x42, 0x0D, 0x88 } // changing input color
CVBS AIN-10 – NTSC/PAL 16-bit 422 Output
These values are written to the decoder using I2C.
I want to know whether the issue is caused by these register settings or we have any other register values to be set to solve this issue.